GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Forum Gimzo 2 custom On/Off button?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 51 replies
  • Answers 2 answers
  • Subscribers 14 subscribers
  • Views 9476 views
  • Users 0 members are here
Related

Gimzo 2 custom On/Off button?

e14 Contributor
e14 Contributor over 11 years ago

Ideally I'd want to modify the BIOS to autostart without pressing any button. But if nobody ends up knowing how to do that, I'd like to at least have a custom proper button on my device's case for turning the Gizmo on. I've read one of the pin pairs can be used, but which ones?

 

mCPawjq.png

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago +1 suggested
    Hi Mark, The information is in this thread: http://www.element14.com/community/community/designcenter/single-board-computers/gizmo2/blog/2015/07/30/gizmo2--flash-bios-to-autostart-on-power-up . In summary…
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor +1
    Hi Mark, Enrico is suggesting try it with a resistor, see if it works for you. If you observe some behavior that is undesirable (e.g. having to hold the button pressed for a long time) then it can be considered…
Parents
  • fvan
    0 fvan over 11 years ago

    Check out this post where I added an external power and reset button: http://www.element14.com/community/community/designcenter/single-board-computers/gizmo2/blog/2015/01/28/gizmo2-adding-external-pwr-and-rst-buttons

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to fvan

    Oh wow, so much great tutorials I'm having hard time finding image

     

    So you didn't use a resistor?

    Is there any requirement for what button can be used. All I know is buttons have a maximum current rating, this shows how little my electronics knowledge is. But it's going to be fun programming the Gizmo after I get this figured out.

     

    PS. Is that a 3d printed enclosure? That's another hobby of mine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to balearicdynamics

    Yes, it seems I need a 5v relay shield for Arduino to use a relay.

    Arduino+relay is getting complicated option itself.

    Maybe it will be easier to jut use the transistor with the arduino after all.

    It's just two thing I don't get: how would I find out the ground side of the button of the projector? Voltmeter and checking if it shows positive or negative voltage?

    If the projector and arduino have a common ground, isn't it dangerous if one uses more current then the other can handle? (Arduino has 5 buttons connected and controls a servo motor). Or is connecting more stuff to GND not dangerous.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor
    how would I find out the ground side of the button of the projector?


    Just check with the voltmeter and see where is the negative it's the GND. On Gizmo2 schematics are distributed for free and are very helpful to find also where ground pins are on the board connectors.


    No matter about GND, all ground should be connected. voltage does not interfere at all, if you connect things correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to balearicdynamics

    I know about Gizmo, the video projectors ground is not known thats why I asked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    I supposed, so you should check with a voltmeter the negative should be GND

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to balearicdynamics

    Will do and report back.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    Ok.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to balearicdynamics

    Oh forgot this. The GND from the Arduino is 5V, from projector its 12V. Is that an issue?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    Mark gnd is gnd. Is voltage that is different. It is expected - don't offend - that you know at least the badis of electricity. Viltage are fifferen wirrs. Gnd is common and is gnd for all. If you put 12 over 5 you burn something. Afyer your tests use diodes for return current protection

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to balearicdynamics

    I understand, no offence taken. However, most of this is electronics, not electricity. You now mentioned diodes for return current protection, I didn't know about them. So if GND taking 12V and 5V wasn't a problem for the respective devices that wouldn't be needed, right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    It is the worth to use diodes, in my opinion

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    It is the worth to use diodes, in my opinion