BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone: Getting Started
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oneleggedredcow
  • Date Created: 14 May 2013 7:33 PM Date Created
  • Views 2278 views
  • Likes 0 likes
  • Comments 2 comments
  • codexstart
  • BeagleBone
  • bb_black
Related
Recommended

BeagleBone: Getting Started

oneleggedredcow
oneleggedredcow
14 May 2013

Installing Software

Connecting to the BeagleBone board is pretty easy, here’s the quick run down of how to do it:

 

1) Download and install the driver:

 

32 bit

64 bit

 

2) Download and install putty:

 

PuTTY

 

Connecting

Now that you have all of the necessary software installed, you need to figure connect to the board. To do this, open device manager. I always forget where it is, so I think the easiest way to get to it is just to search for it:

 

Start -> Search Text Box : “Device Manager”

 

Once in the device manager, expand the “Ports (COM & LPT)” section.  This is where the BeagleBone will show up once it is plugged in.

 

Now plug in the BeagleBone. The “Ports (COM & LPT)” section should update and the BeagleBone board should show up there.  For me it was difficult figuring out which one it was, so I had to watch the list pretty closely.

 

The important part is what COM port it was assigned.  Once you know this open up PuTTY and:

 

Change the “Connection Type” to “Serial”

Set the “Serial Line” to COM<X> where <X> is the number that you found in the Device Manager.

Set the “Speed” to 115200

Click “Open”

 

image

 

I don’t know why, but mine comes up blank and I have to hit enter before it does anything.  Once I hit enter, it prompts me for a “beaglebone login”, which is “root”.

 

image

 

At this point you should be up and running with your BeagleBone.

Ethernet

Now that we are connected to the BeagleBone through the USB connection, we want to be able to connect to it through Ethernet.  To do this, we first need to figure out its IP Address, which can be obtained through the command:

 

Ifconfig -a

 

image

 

Then take the eth0 IP address and type that into Firefox or Chrome.  That should land you on a BeagleBoard 101 page.

 

image

 

Blink an LED

Create a circuit like the one shown here:

 

image

 

Now that we have the circuit built, we need to run a program that blinks the LED.  Fortunately, an example comes built in with the BeagleBone board.  To access it, fire up Cloud9, which is their built in Integrated Development Environment (IDE).  To do this, go to <IP_Address>:3000 in your browser:

 

image

 

Once you have the browser up, double click blinkled.js.  This is a simple program that blinks an LED.  To run the program, just click the green play button at the top, next to the word “debug”.

Conclusion

Setting up the BeagleBone is really easy.  In a couple of minutes, we went from opening up the box to running a program that blinks an LED.  Not bad at all.

  • Sign in to reply
  • oneleggedredcow
    oneleggedredcow over 13 years ago in reply to ericwertz

    Thanks for the helpful comment!  That's good to know!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ericwertz
    ericwertz over 13 years ago

    "I don’t know why, but mine comes up blank and I have to hit enter before it does anything."

     

    By the time you open putty, the login prompt has already been output and you've missed it.  By hitting enter (a blank username), it re-issues the prompt.  If you open putty early enough, you'll likely catch the first prompt.  Anything that you type before enter is going to be taken as a username, and the first enter will send that and then ask for a password.

     

    On a generic two-wire serial connection, this is pretty much how it has to be -- login (or getty on classic u*ix) can't tell that you've connected and issue you a prompt at that time  Serial port logins have behaved this way for 40+ years.

     

    Getting a login prompt over the network (with telnet, ssh, etc.) relies on a totally different connection mechanism, and so doesn't have this behavior.

     

    Looks easy to get started -- thanks.