BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleY-AI Review - Part 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: aswinvenu
  • Date Created: 10 Sep 2024 3:48 PM Date Created
  • Views 5665 views
  • Likes 6 likes
  • Comments 6 comments
  • beagleyai
Related
Recommended

BeagleY-AI Review - Part 2

aswinvenu
aswinvenu
10 Sep 2024

Introduction


This is the continuation of my previous blog ( BeagleY-AI Review - Part 1 ). In this blog we will look into the AI/ML inference performance of BeagleY-AI. As I was working with this board for the past few weeks, I have learnt a lot about the platform and the board. I think It's definitely worth sharing. For those who wanted to get started with the BeagleY-AI board, I think this will help a lot.

The Architecture

image

The heart of Beagley-AI is Texas Instruments AM67A. This quad core ARM Cortex A53 processors can clock upto a maximum speed of 1400MHz. This is not a fancy looking processor compared to what we get in the latest Raspberry Pis. But the real difference comes into picture when you look into the co-processors.

  • 2x C7x DSPs. Each can produce 2TOPS
  • ARM Cortex R5F MCU for meeting any realtime requirements
  • 3D graphics processing unit
  • Video and Vision accelerators

So it's very clear that this processor was meant for performing AI/ML inference on edge. Let's dive deep into this use case in this blog.

Example given in the getting started guide

TensorFlow Lite Object Detection

This is a sample project given in the getting started guide. Very simple example which deploys coco-ssd-mobilenet pretrained model for object detection. The example make use of TensorFlow Lite APIs for inference on edge.

Note : The steps involved to get this running on the board is very well documented in the above given link. So I am not including it in this blog.

Let's look at the result what I got.

image

Interesting!! I am hardly getting 3 FPS performance. It's really bad!

In comparison, I ran the same example on my Raspberry Pi 5 (8GB variant) and I am getting  15 FPS! 5 times better performance on RPi5!


image

Hmmm... Something is really wrong. What can that be. With the dual DSP Co-processors which can produce 4TOPS, It's not producing a satisfactory result?? Answer to this question is in the way how TensorFlow Lite works.

AI/ML Inference on Edge

TensorFlow Lite is google's high performance runtime for AI models on edge devices. BeagleY-AI has two C7x DSP processors to boost the inference performance. But how does the TFLite runtime know there is such a co-processor present and how to access it ?

image 

LiteRT Delegates address this issue. Delegates enable hardware acceleration of TFLite models leveraging the underlying GPUs or DSPs. By default TFLite models are optimized for ARM Neon architecture. But CPUs are not optimized for performing large scale matrix multiplication or convolutions.

Read more on LiteRT Delegates here : https://ai.google.dev/edge/litert/performance/delegates

Now the question is from where do I get the delegates for C7x DSPs, So that I can accelerate the inference performance on edge.

TI's Edge AI

TIDL Texas Instruments Deep Learning product is the fundamental part of TI's Edge AI. This software product is used for acceleration of deep neural networks (DNN) in TI's Processors. It supports TI’s latest generation C7x DSP and TI's DNN accelerator (MMA).

image

TIDL not only supports TensorFlow Lite runtimes but also ONNX RunTime as well as TVM/Neo-AI RunTime. All of them uses heterogeneous execution on cortex-A** + C7x-MMA.

Heterogeneous execution enables the following benefits.

  • OSRT as the top level inference for user applications
  • Offloading subgraphs to C7x/MMA for accelerated execution with TIDL
  • Runs optimized code on ARM core for layers that are not supported by TIDL

Getting started with TIDL

This is a two parted installation.

1) On the host PC (x86) - [ model compilation and artifacts generation]

2) On the target BeagleY-AI [ inference ]

Before we install TIDL tools, we need to install the processor SDK for working with AM67 series processors. This includes all the cross buildtools required to train compile and test the models given in TIDL.

Download the latest SDK from https://www.ti.com/tool/PROCESSOR-SDK-AM67

sudo apt-get install libyaml-cpp-dev libglib2.0-dev
wget https://dr-download.ti.com/software-development/software-development-kit-sdk/MD-f73Ky6d9aZ/10.00.08.06/ti-processor-sdk-linux-am67-sk-10_00_08_06-Linux-x86-Install.bin
chmod +x ti-processor-sdk-linux-j722s-evm-09_02_00_04-Linux-x86-Install.bin
./ti-processor-sdk-linux-j722s-evm-09_02_00_04-Linux-x86-Install.bin

imageimageimageimage

Once we have successfully installed the SDK we can clone the latest TIDL repo.

git clone https://github.com/TexasInstruments/edgeai-tidl-tools.git

Since we are using the latest SDK we don't need to checkout to the version TAG. We can continue with the master branch

cd edgeai-tidl-tools
export SOC=am67a
source ./setup.sh

export TIDL_TOOLS_PATH=$(pwd)/tidl_tools
export LD_LIBRARY_PATH=$LD_LIBRARY_PATH:$TIDL_TOOLS_PATH
export ARM64_GCC_PATH=$(pwd)/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu

Compile and validate on the host PC (x86)

mkdir build && cd build
cmake ../examples && make -j && cd ..
source ./scripts/run_python_examples.sh
python3 ./scripts/gen_test_report.py

imageimage

The build was successful and we can see the models and model_artifacts are successfully generated. Sample outputs are stored in output_images

imageimageimage

So far so good!

image

Now we have successfully generated the artifacts we can use them for inference on edge. These artifacts are optimized to perform the best out of am67a chipset. For example mobilenet tflite model trained on coco dataset is available in the model directory. The model_artifact contains all the metadata and configuration files.

These files needs to be copied to the TIDL directory of the our target board.

On the target beagleY-AI:

git clone https://github.com/TexasInstruments/edgeai-tidl-tools.git
cd edgeai-tidl-tools
export SOC=am67a
export TIDL_TOOLS_PATH=$(pwd)
# scp -r <pc>/edgeai-tidl-tools/model-artifacts/  <dev board>/edgeai-tidl-tool/
# scp -r <pc>/edgeai-tidl-tools/models/  <dev board>/edgeai-tidl-tool/
mkdir build && cd build
cmake ../examples && make -j && cd ..
python3 ./scripts/gen_test_report.py

Sad end!

Unfortunately the Debian OS doesn't meet the dependencies to run the TIDL Example models on edge. I spent the whole weekend and last two days, for getting it to work ( By manually installing the dependencies). At this point I have to let it rest for sometime. I will continue work on this in the coming days. More updates will be covered in Part3 of this review blog series. 

References:

  • https://docs.beagleboard.org/latest/boards/beagley/ai/demos/beagley-ai-object-detection-tutorial.html
  • https://github.com/TexasInstruments/edgeai-tidl-tools
  • https://www.ti.com/technologies/edge-ai.html
  • https://github.com/TexasInstruments/edgeai/blob/main/readme_sdk.md
  • Sign in to reply
Parents
  • saivarma
    saivarma 5 months ago

    can you help me sir please iam facing error 

    root@j722s-evm:/opt/edgeai-gst-apps# cd /opt/edgeai-gst-apps
    root@j722s-evm:/opt/edgeai-gst-apps# python3 apps_python/app_edgeai.py configs/waterbottle_yolox_nano.yaml
    libtidl_onnxrt_EP loaded 0x25842a00
    Final number of subgraphs created are : 2, - Offloaded Nodes - 268, Total Nodes - 277
    APP: Init ... !!!
    1730.191277 s: MEM: Init ... !!!
    1730.191572 s: MEM: Initialized DMA HEAP (fd=5) !!!
    1730.191818 s: MEM: Init ... Done !!!
    1730.191854 s: IPC: Init ... !!!
    1730.247920 s: IPC: Init ... Done !!!
    REMOTE_SERVICE: Init ... !!!
    REMOTE_SERVICE: Init ... Done !!!
    1730.262588 s: GTC Frequency = 200 MHz
    APP: Init ... Done !!!
    1730.273688 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR
    1730.273735 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING
    1730.273752 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO
    1730.275262 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-0
    1730.275588 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-1
    1730.275790 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-2
    1730.275924 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-3
    1730.275947 s: VX_ZONE_INFO: [tivxInitLocal:202] Initialization Done !!!
    1730.276007 s: VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO
    1730.290000 s: VX_ZONE_ERROR: [vxGetStatus:1250] Reference is NULL
    TIDL_RT_OVX: ERROR: Init TIDL failed
    Traceback (most recent call last):
    File "/opt/edgeai-gst-apps/apps_python/app_edgeai.py", line 67, in <module>
    main(sys.argv)
    File "/opt/edgeai-gst-apps/apps_python/app_edgeai.py", line 46, in main
    demo = EdgeAIDemo(config)
    ^^^^^^^^^^^^^^^^^^
    File "/opt/edgeai-gst-apps/apps_python/edge_ai_class.py", line 108, in __init__
    model_obj.create_runtime()
    File "/usr/lib/python3.12/site-packages/edgeai_dl_inferer.py", line 315, in create_runtime
    self.run_time = RunTime(self.artifacts,
    ^^^^^^^^^^^^^^^^^^^^^^^
    File "/usr/lib/python3.12/site-packages/edgeai_dl_inferer.py", line 170, in __init__
    self.interpreter = _onnxruntime.InferenceSession(
    ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
    File "/usr/lib/python3.12/site-packages/onnxruntime/capi/onnxruntime_inference_collection.py", line 387, in __init__
    self._create_inference_session(providers, provider_options, disabled_optimizers)
    File "/usr/lib/python3.12/site-packages/onnxruntime/capi/onnxruntime_inference_collection.py", line 439, in _create_inference_session
    sess.initialize_session(providers, provider_options, disabled_optimizers)
    onnxruntime.capi.onnxruntime_pybind11_state.Fail: [ONNXRuntimeError] : 1 : FAIL : Create state function failed. Return value:-1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • saivarma
    saivarma 5 months ago

    can you help me sir please iam facing error 

    root@j722s-evm:/opt/edgeai-gst-apps# cd /opt/edgeai-gst-apps
    root@j722s-evm:/opt/edgeai-gst-apps# python3 apps_python/app_edgeai.py configs/waterbottle_yolox_nano.yaml
    libtidl_onnxrt_EP loaded 0x25842a00
    Final number of subgraphs created are : 2, - Offloaded Nodes - 268, Total Nodes - 277
    APP: Init ... !!!
    1730.191277 s: MEM: Init ... !!!
    1730.191572 s: MEM: Initialized DMA HEAP (fd=5) !!!
    1730.191818 s: MEM: Init ... Done !!!
    1730.191854 s: IPC: Init ... !!!
    1730.247920 s: IPC: Init ... Done !!!
    REMOTE_SERVICE: Init ... !!!
    REMOTE_SERVICE: Init ... Done !!!
    1730.262588 s: GTC Frequency = 200 MHz
    APP: Init ... Done !!!
    1730.273688 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR
    1730.273735 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING
    1730.273752 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO
    1730.275262 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-0
    1730.275588 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-1
    1730.275790 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-2
    1730.275924 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:169] Added target MPU-3
    1730.275947 s: VX_ZONE_INFO: [tivxInitLocal:202] Initialization Done !!!
    1730.276007 s: VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO
    1730.290000 s: VX_ZONE_ERROR: [vxGetStatus:1250] Reference is NULL
    TIDL_RT_OVX: ERROR: Init TIDL failed
    Traceback (most recent call last):
    File "/opt/edgeai-gst-apps/apps_python/app_edgeai.py", line 67, in <module>
    main(sys.argv)
    File "/opt/edgeai-gst-apps/apps_python/app_edgeai.py", line 46, in main
    demo = EdgeAIDemo(config)
    ^^^^^^^^^^^^^^^^^^
    File "/opt/edgeai-gst-apps/apps_python/edge_ai_class.py", line 108, in __init__
    model_obj.create_runtime()
    File "/usr/lib/python3.12/site-packages/edgeai_dl_inferer.py", line 315, in create_runtime
    self.run_time = RunTime(self.artifacts,
    ^^^^^^^^^^^^^^^^^^^^^^^
    File "/usr/lib/python3.12/site-packages/edgeai_dl_inferer.py", line 170, in __init__
    self.interpreter = _onnxruntime.InferenceSession(
    ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
    File "/usr/lib/python3.12/site-packages/onnxruntime/capi/onnxruntime_inference_collection.py", line 387, in __init__
    self._create_inference_session(providers, provider_options, disabled_optimizers)
    File "/usr/lib/python3.12/site-packages/onnxruntime/capi/onnxruntime_inference_collection.py", line 439, in _create_inference_session
    sess.initialize_session(providers, provider_options, disabled_optimizers)
    onnxruntime.capi.onnxruntime_pybind11_state.Fail: [ONNXRuntimeError] : 1 : FAIL : Create state function failed. Return value:-1