BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BB AI cooling Addon board available
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 113 subscribers
  • Views 6683 views
  • Users 0 members are here
  • bbai
  • visionthing
  • bbb
  • element14presents
  • oshwa
  • mayermakes
Related

BB AI cooling Addon board available

mayermakes
mayermakes over 7 years ago

if you can't wait to get a fan-addon for the Beaglebone AI : here is the link to order the pcb right away: https://aisler.net/p/SWHBYGQV

it takes the recommended Fan and allows to control it with pwm from a Pin on the Beaglebone (compatible with AI, Black, Green, Blue and Industrial Beaglebones)

it also provides an easier to reach debug header(has to be soldered the other way round as in the picture(don't know how to flip it in Kicad3Dviewer) and a debug cutout for the BBAI
Here is the BOM:

 

 

Bill of Materials

 

Product NameManufacturerQuantityBuy KitBuy Kit
Through Hole Resistor, 10 kohm, MCMF0W4 Series, 125 mW, ± 1%, Axial Leaded, 200 VMULTICOMP1Buy NowBuy Now
MOSFET Transistor, N Channel, 47 A, 55 V, 0.022 ohm, 10 V, 4 VINFINEON1Buy NowBuy Now
F251R-05LLC - Axial Fan, 5 V, DC, 25 mm, 10 mm, 1.412 cu.ft/min, 0.04 m³/minNIDEC1Buy NowBuy Now
706 - Development Kit Accessory, Stacking Header Set, Female, For BeagleBone Proto CapeADAFRUIT1Buy NowBuy Now
M2.5 12 PRSTMC Z100 -  Machine Screw, M2.5, 12 mm, Steel, Bright Zinc, Pan Head PozidrivTR FASTENINGS1Buy NowBuy Now
Board-To-Board Connector, Vertical, 2.54 mm, 3 Contacts, Header, 2211S Series, Through Hole, 1 RowsMULTICOMP1Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 2 Contacts, Header, 2211S Series, Through Hole, 1 RowsMULTICOMP1Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 6 Contacts, Header, 2211S Series, Through Hole, 1 RowsMULTICOMP1Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 6 Contacts, Receptacle, BG095 Series, Through Hole, 1 RowsGCT1Buy NowBuy Now




This is also to be released alongside a future
element14 presents episode image, and I see the need for people to use it so please try out this prototype at your own risk.

 

The first 0 batch has not yet arrived in my workshop so I can't promise it works perfectly right now.

image

The fan can be mounted in several ways:

1. on top of this pcb utilizing the original heatsink:(RECOMMENDED VERSION)

                    addon boards on top of the BBAI-Cooler need to provide a cutout or longer header pins for correct airflow.

2. on the bottom of the pcb;

                     B: longer header pins : the heatsink can stay where it is, no other changes needed (RECOMMENDED VERSION)

 

The DC Fan is driven with the exact circuit 90% of 3d printers use with similar fans to control their speed. The Mosfet is overkill for the purpose but I haven't found a better fit that is available in tht yet.

Nevertheless there is of course a Risk at high pwm frequencies of burning out the internal cap or overwhelming the IC, so I suggest  limiting the use of PWM to a lower frequency or implement a Bang-Bang cycle for temp control in software instead of constant PID loops.
On the BBAI I suggest leaving the Fan on full on either in software or by setting the jumper to on.


 

Message was edited by: Clemens Mayer Added some clarifications from the comments.

 

Message was edited by: Clemens Mayer Added Schematic file

Attachments:
BBAI-Cooler.zip
  • Sign in to reply
  • Cancel

Top Replies

  • mayermakes
    mayermakes over 7 years ago in reply to mudz +3
    the headers shown in the rendering are already long legged ones. I ordered the Adafruit BB header kit, we will see if these are long enough.
  • gdstew
    gdstew over 7 years ago in reply to mayermakes +3
    " but troublesome for another add-on board " This has been a problem for me as well as now a cape (on top of the fan cape) needs long pins so that it will not restrict air flow to the fan. i would venture…
  • mayermakes
    mayermakes over 7 years ago +2
    I've been running the BBAI with the Fan mentioned in the post for about 1hour with a PRU load , a simple python script and a tidl example(image classification) executing. temperatures are stying low (can…
Parents
  • mayermakes
    mayermakes over 7 years ago

    I've been running the BBAI with the  Fan mentioned in the post for about 1hour with a PRU  load , a simple python script and a tidl example(image classification) executing. temperatures are stying low (can touch heatsink easily)

    Running latest kernel and firmware image.

    the Fan seems to be sufficient

     

     

    Edit: updated loads, temps unchanged low! very good result

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mayermakes
    mayermakes over 7 years ago

    I've been running the BBAI with the  Fan mentioned in the post for about 1hour with a PRU  load , a simple python script and a tidl example(image classification) executing. temperatures are stying low (can touch heatsink easily)

    Running latest kernel and firmware image.

    the Fan seems to be sufficient

     

     

    Edit: updated loads, temps unchanged low! very good result

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • johnrains
    johnrains over 6 years ago in reply to mayermakes

    Is the 5v sourced from the BBAI board or an external supply?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 6 years ago in reply to johnrains

    It is sourced from the bbai header pins, it runs as soon as power is connected.