BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Reading BeagleBone AI Temperatures
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 113 subscribers
  • Views 8745 views
  • Users 0 members are here
  • bbb
Related

Reading BeagleBone AI Temperatures

gdstew
gdstew over 7 years ago

I finally brought up my BeagleBone AI with a 25mm x 7mm fan firmly screwed into the heat sink using M2 or

M3 (they were salvaged so I don't know for sure) machine screws. It was a lot quieter than I was expecting

although I don't believe it is running at the advertised 10K RPM. Attempting to update the software with

apt-get upgrade (after doing apt-get update) died with the message "FATAL -> failed to fork" which turned out

to be a low memory problem. The Getting Started program from the desktop was running the cloud9 IDE in

the Chromium browser so I shut that down and did the upgrade again and it worked. I had no problems with

any of the other updates after that.

 

The next thing I did was go look for where the SoC temperatures could be read and I think I found them several

sub-directories deep in the /sys directory. I do wish that there was a standard directory to put these in as

everybody puts them in very different places in the /sys directory. There are 5 different thermal zones and

each one has a directory in the /sys/devices/virtual/thermal/ directory named thermal_zone0 -  thermal_zone4.

To display the temperature for thermal zone 0 use this command:

 

debian@beaglebone:~$ cat /sys/devices/virtual/thermal/thermal_zone0/temp

47000

debian@beaglebone:~$

 

The response, 47000 (your mileages WILL vary) is 47.0 deg. C.

 

At the time the AI was mostly idle with me on a terminal inside an LXDE window. The temperatures I was

reading were within a couple of degrees C across all the zones. There are many thermal management

configuration files in the thermal_zoneX directories and it would be great to get documentation on what/where

the thermal zones are as well as the thermal management settings used for them.

 

While the idle temperatures were OK for checking out and doing light work on the AI I'm going to have to

come up with some serious thermal solutions. A 40mm fan is the biggest you can get between the GPIO

headers and I don't know if that will be big enough when you start loading up several of the more interesting

cores.

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago +4
    I would have imagined all these BB-AI were the same, however very cautiously I too ran the sudo apt update and upgrade from the Loud9 IDE and it did work. No errors! I'm connected via Ethernet from a router…
  • 14rhb
    14rhb over 7 years ago +2
    Thanks gdstew This is just the information I'll need soon. In a few days I'm expecting my USB-C cable and then I'll be powering up my BB-AI for the first time - having followed the various threads I'm…
  • gdstew
    gdstew over 7 years ago +2
    I just attached a bash shell script I wrote to read one or all temperature zones on a BeagleBone AI. There is a bin directory in the debian users home directory directory and I copied the script from a…
Parents
  • gdstew
    gdstew over 7 years ago

    I just attached a bash shell script I wrote to read one or all temperature zones on a BeagleBone AI. There is a bin directory in the debian users home

    directory directory and I copied the script from a micro sd card to /home/debian/bin. The home/bin directory is not in the environment PATH variable

    so either have to add it to PATH, include the path with the file name when you execute it, or copy it somewhere already in PATH. I chose to copy it to

    /usr/local/bin using the command:

     

      debian@beaglebone:~$ sudo cp bin/ai_temp.sh /usr/local/bin

     

    In order for the debian user to execute the script the file permissions have to be changed to allow it with the command:

     

       debian@beaglebone:~$ sudo chmod o+x /usr/local/bin/ai_temp.sh

     

    After that:

     

    To see all temperature zones type ai_temp.sh from the command line,

     

    To see a specific zone temperature type ai_temp.sh X where X is the zone number from 0 - 4. If you type in an invalid zone number you will get an

    error message.

     

    This script does use bash specific commands, specifically the ones used to extract characters from the temperature returned by the cat command.

    It also makes a couple of assumptions about the number of digits in the temperature. The first is that there are no more that two digits to the left of

    the decimal point. This is probably a safe assumption since the script will probably not be running if the AI temperature is > 99 deg. C. The second is

    that there there are two digits to the left of the decimal point. This is a reasonable assumption because the AI is not going below 10 deg. C unless

    some type of extreme cooling is used.

     

    From testing the script it looks like zone 2 is the dual core ARM Cortex-A15. It is always the highest temperature by around 2 degrees C.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to gdstew

    Good Work you did there. Though, to be sure, you can always contact ti community, and get an official answer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mudz
    mudz over 7 years ago in reply to gdstew

    Good Work you did there. Though, to be sure, you can always contact ti community, and get an official answer.