BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Upgrading Kernel on BeagleBone Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 109 subscribers
  • Views 5799 views
  • Users 0 members are here
  • tftp_server
  • uboot
  • crosscompiler
  • kernel
  • BeagleBone Black
Related

Upgrading Kernel on BeagleBone Black

e14 Contributor
e14 Contributor over 10 years ago

Hi,

 

I'm trying to upgrade the kernel of a BeagleBone Black from '3.8.13-bone79' to '4.1.16-bone18'.

The build of the new kernel is done under a virtual machine of Ubuntu15 with 'arm-linux-gnueabihf' cross-compiler, and then kernel is downloaded to BeagleBone Black through tftp.

 

BeagleBone Black Configuration:

  • Hardware: BeagleBone Black 4GB rev.C
  • OS: Debian 4.6.3-14
  • Kernel (current): 3.8.13-bone79
  • Internet connection: USB ('USB0') & Ethernet ('eth0')
    • Download the zImage and dtb files is done through a tftp server over windows.

 

* All the steps followed are from this tutorial.

 

After build and download the kernel, and copy the modules to BeagleBone Black too, the device is rebooted and a terminal console is opened through serial port to access to uBoot.

Following again the above tutorial steps, it is time to load the kernel and reboot the device.

Here, it is when process fails with next message:

/etc/rc.local: 14: /etc/rc.local: cannot create /sys/devices/bone_capemgr1/slots: Directory nonexistent
[FAIL] startpar: service(s) returned failure: rc.local ... failed!

 

Does anyone have an idea bout why is this happening?

I would thank any hint to understand the root cause and how can I finally upgrade the kernel.

 

KR!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57 +1
    Hi, is is fixed. Finally, I have changed the BBB's kernel (3.8.13 -> 4.1.16). I had to modify one line into ' /etc/inittab ' file. Original: T0:23:respawn:/sbin/getty -L tty O 0 115200 vt102 Modified:…
  • clem57
    clem57 over 10 years ago

    My guess is the environment or directories was not built. Please capture  /etc/rc.local/ here.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    Please, find below the content of '/etc/rc.local':

     

         #!/bin/sh -e

         #

         # rc.local

         #

         # This script is executed at the end of each multiuser runlevel.

         # Make sure that the script will "exit 0" on success or any other

         # value on error.

         #

         # In order to enable or disable this script just change the execution

         # bits.

         #

         # By default this script does nothing.

        

         echo ttyO2_armhf.com > /sys/devices/bone_capemgr1/slots

         echo ttyO5_armhf.com > /sys/devices/bone_capemgr2/slots

        

         exit 0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    Just comment out two echo lines since by default it does nothing.image

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    Hi,

     

    I have just commented both lines, and the process goes well until console starts to show:

    "INIT: Id "T0" respawning too fast: disabled for 5 minutes"

     

    Then, the process enters into an infinite loop showing message every 5 minutes.

     

    What process is T0? And how can I solved this?

     

    KR!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    The "respawning too fast" message is telling you that your X-server (or xorg.conf file) is miss-configured, and the X-server is crashing when it tries to start and trying to restart too fast or too often.

     

     

    From the command line, look at /var/log/Xorg.0.log to see why the X-server crashed, and fix the problem.

     

    I believe you need to recheck the tutorial or restart the build? This is not a small issue.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    Hi,

     

    is is fixed.

    Finally, I have changed the BBB's kernel (3.8.13 -> 4.1.16).

     

    I had to modify one line into '/etc/inittab' file.

    • Original: T0:23:respawn:/sbin/getty -L ttyO0 115200 vt102
    • Modified: T0:23:respawn:/sbin/getty -L ttyS0 115200 vt102

     

    Then, after doing the whole process I have written my own tutorial with the steps that worked for me.

     

    KR!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    Glad you found the bad line, Do you know why the change?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago

    Please mark helpful comments that helped you Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57

    What I have found about is:

     

        By default, the console definition is based on ttySx, nor as for BeagleBone where it has been changed to ttyOx.

        Then, when changing the kernel, default values are loaded again.

        There must be take into account we are compiling a linux kernel, specific for BeagleBone, but a linux kernel in its core.

     

    That is what I have understood.

    Please, correct me if I am wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    Curious why the beaglebone guys changed that, but good to know. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>