BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Android lagging on Beaglebone Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 109 subscribers
  • Views 1031 views
  • Users 0 members are here
  • andriod
  • bbb
Related

Android lagging on Beaglebone Black

sush1993
sush1993 over 10 years ago

I have an android 4.4 kitkat loaded on my sd card (sdhc class 10), with a GUI loaded with different apps such as to monitor two sensor values and to control the GPIOs of the beaglebone black amongst many other apps, but my GUI keeps on lagging on the Touchscreen panel which is a dell (S2240T).

 

I have kept the clock speed at 1 GHZ of my BBB.

 

What do I do to avoid this lagging?

 

Thanks,

  • Sign in to reply
  • Cancel
Parents
  • volly
    0 volly over 10 years ago

    sush1993. I get it, that for the present time you are stuck with the BBB.

    Let me  address your reply in the reverse order.

    If a variety of sensors and a user operated interface is the focus of your application,

    then I would actually recommend the Raspberry Pi 3 which is firstly much cheaper than the BBB,

    and secondly, it supports a very rich variety of readily available sensors and other peripherals,

    thirdly, it very much enjoys a greater support community. And most importantly, in my experience,

    Android just works with the least amount of tweaking and hacking.

    OH!!!!! And Google AOSP  Repository is imminent

    I am not saying that there are no issues with the RaspiAnd, but it is way more supported than on the BBB.

    With that being said, let's move on to attempting to assist you with your current issues.

    Can I ask you to email me the full project technical/functional specs and prime objectives of

    what it is that you ultimately want out of all of this.

    I will commit to assisting with everything I know and my experiences with the BBB and Android.

    If that is okay with you, here is my email:

    yunusvollenhoven@gmail.com

     

    Regards.

    Yunus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jeffmemyself
    0 jeffmemyself over 9 years ago in reply to volly

    Hello, we have the same issue. Running Android on BBB, and in some cases our App is very slow, as when we load a new screen etc, it may lag 3-5 seconds. We have confirmed the processor is running at max (1GHz) and we have plently of RAM. We are also running on the sd card, and perhaps there is better performance if we flash to the emmc? What can we do to speed things up?

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jeffmemyself
    0 jeffmemyself over 9 years ago in reply to volly

    Hello, we have the same issue. Running Android on BBB, and in some cases our App is very slow, as when we load a new screen etc, it may lag 3-5 seconds. We have confirmed the processor is running at max (1GHz) and we have plently of RAM. We are also running on the sd card, and perhaps there is better performance if we flash to the emmc? What can we do to speed things up?

     

    Thanks!