BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone Black Rev C screens shuts off
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 111 subscribers
  • Views 1977 views
  • Users 0 members are here
  • rev c
  • beagle bone black
Related

Beaglebone Black Rev C screens shuts off

ruanknoetze
ruanknoetze over 9 years ago

I recently bought a new Beaglebone Black rev C and started playing around with it by using a standalone setup with HDMI, keyboard and mouse. After a few minutes the screens completely shuts off and does not want to start up again. I thought it might be a OS issue and re flashed my eMMC with an Angstom distribution. After start up it did the exact same thing. I even added code that disables the auto sleep mode of the screen but that does not work.

 

I know the BBB is getting input from my mouse and keyboard because one of the LEDs flashes when I type or click.

 

Has anyone ever experienced this and what can you recommend I do?

 

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago +2
    could it be a power issue? If the screen goes off when a usb hub, mouse and keyboard are plugged in its a possibility.
  • ruanknoetze
    ruanknoetze over 9 years ago +2 suggested
    Hi All I have flashed Debian 8.6 to another REVC and so far the screen has not turned off. I am also using a more stable power supply. So maybe it is a Angstom problem or a power supply problem. I will…
  • kleykenb
    kleykenb over 9 years ago +2
    Definately sounds like a power related issue. In my setup I've found that powering the BeagleBone via the microUSB port limits current to 500mA (which is the USB standard but not followed by everyone)…
Parents
  • koudelad
    0 koudelad over 9 years ago

    Hello,

     

    Your trouble is not listed as a known issue, so I would try the following:

    1) visually checking the board (all components placed according to design files, no misplaced components, scratches, integrity of connectors...). (I assume you don't own of know anyone with an x-ray to check the BGA soldering.)

    2) check temperature of the components to rule out overheating

    3) use another sufficient and stable power supply

    4) use less and / or different peripherals (or try a powered USB hub).

     

    If none of this works, I would request an RMA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ruanknoetze
    0 ruanknoetze over 9 years ago in reply to koudelad

    Hello

     

    Thank you very much for the reply. I checked all your recommendations. The only one that stands out is the peripherals. When I only connected the HDMI cable the BBB stayed on. When I restarted with the Keyboard and Mouse Connected to a USB Hub that is when the BBB screen shut off.

     

    An interesting observation though is when I connected that same peripherals and the same power supply to a BBB REVB with the 2GB eMMC the screen stayed on. It was running Debian though so I don't know if that is a factor. I have another REVC that I will reinstall Debian on and see if I have the same issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ruanknoetze
    0 ruanknoetze over 9 years ago in reply to koudelad

    Hello

     

    Thank you very much for the reply. I checked all your recommendations. The only one that stands out is the peripherals. When I only connected the HDMI cable the BBB stayed on. When I restarted with the Keyboard and Mouse Connected to a USB Hub that is when the BBB screen shut off.

     

    An interesting observation though is when I connected that same peripherals and the same power supply to a BBB REVB with the 2GB eMMC the screen stayed on. It was running Debian though so I don't know if that is a factor. I have another REVC that I will reinstall Debian on and see if I have the same issue.