BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone Black Rev C screens shuts off
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 111 subscribers
  • Views 1976 views
  • Users 0 members are here
  • rev c
  • beagle bone black
Related

Beaglebone Black Rev C screens shuts off

ruanknoetze
ruanknoetze over 9 years ago

I recently bought a new Beaglebone Black rev C and started playing around with it by using a standalone setup with HDMI, keyboard and mouse. After a few minutes the screens completely shuts off and does not want to start up again. I thought it might be a OS issue and re flashed my eMMC with an Angstom distribution. After start up it did the exact same thing. I even added code that disables the auto sleep mode of the screen but that does not work.

 

I know the BBB is getting input from my mouse and keyboard because one of the LEDs flashes when I type or click.

 

Has anyone ever experienced this and what can you recommend I do?

 

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago +2
    could it be a power issue? If the screen goes off when a usb hub, mouse and keyboard are plugged in its a possibility.
  • ruanknoetze
    ruanknoetze over 9 years ago +2 suggested
    Hi All I have flashed Debian 8.6 to another REVC and so far the screen has not turned off. I am also using a more stable power supply. So maybe it is a Angstom problem or a power supply problem. I will…
  • kleykenb
    kleykenb over 9 years ago +2
    Definately sounds like a power related issue. In my setup I've found that powering the BeagleBone via the microUSB port limits current to 500mA (which is the USB standard but not followed by everyone)…
Parents
  • volly
    0 volly over 9 years ago

    ruanknoetze.

    Please update us on the situation.

     

    Yunus.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • henryhnguyen2000
    0 henryhnguyen2000 over 9 years ago in reply to volly

    Hi All,

     

    I got one BealgleBone Black a few days ago and connected its HDMI port to the monitor through the VGA splitter. I flashed it with the debian IOT version. It came up and a few minutes later, it turned off. I wriggled the cable, then it came up again, and turned off again after a few minutes. I returned for another BeagleBone Black, and now I got the same thing.

    Note that I already had two BeagleBone Black Wireless boards, and both works all the time, no problem with HDMI. In theory, there is not much change between BeagleBone Black and the Wireless version. Has any body have a reliable working BeagleBone Black bougth recently?? If yes, let us know where you bought it.

     

    Regards,

    Henry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • henryhnguyen2000
    0 henryhnguyen2000 over 9 years ago in reply to volly

    Hi All,

     

    I got one BealgleBone Black a few days ago and connected its HDMI port to the monitor through the VGA splitter. I flashed it with the debian IOT version. It came up and a few minutes later, it turned off. I wriggled the cable, then it came up again, and turned off again after a few minutes. I returned for another BeagleBone Black, and now I got the same thing.

    Note that I already had two BeagleBone Black Wireless boards, and both works all the time, no problem with HDMI. In theory, there is not much change between BeagleBone Black and the Wireless version. Has any body have a reliable working BeagleBone Black bougth recently?? If yes, let us know where you bought it.

     

    Regards,

    Henry