BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone Black Internet issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 111 subscribers
  • Views 4919 views
  • Users 0 members are here
  • beagle bone black
  • internet connection
Related

Beaglebone Black Internet issue

gunjanvora
gunjanvora over 9 years ago

I have a Beaglebone Black board having following configuration :- Linux beaglebone 3.8.13-bone47, Debian GNU/Linux 7 (wheezy). The internet connection in this board is not working. Neither through USB now through Ethernet. Kindly help me to resolve this issue.

  • Sign in to reply
  • Cancel

Top Replies

  • ninjatrent
    ninjatrent over 8 years ago +1
    This video might be a better explanation. www.youtube.com/watch
  • jomoenginer
    jomoenginer over 8 years ago +1
    I think Gunjan is not getting the wired Ethernet or the USB IP to work on the Beaglebone Black so I believe it is not a Wi-Fi issue. @Gunjan - try running 'dmesg' on the Beagelbone to see if there are…
  • gsgill112
    gsgill112 over 8 years ago in reply to ninjatrent +1
    Do you have any help with enabling the DTO files for WLAN and BLE Module ? I have a Beagle Bone Black with WCC cape and I am having some issues with getting it working. //GS GILL
Parents
  • jomoenginer
    0 jomoenginer over 8 years ago

    I think Gunjan is not getting the wired  Ethernet or the USB IP to work on the Beaglebone Black so I believe it is not a Wi-Fi issue.

     

    @Gunjan - try running 'dmesg' on the Beagelbone to see if there are any messages that are related to the Ethernet port being down or the driver having issues.

    Also, as we mentioned previously, check 'ifconfig -a' to see if the Ethernet port is up or not.

     

    Have you tried rebooting the BBB or restart the network interface?

    You should be able to restart the network interface with:

     

    # sudo /etc/init.d/network restart

     

    Derek Molloy has pretty good instructions on how to set up the Ethernet ports on the Beaglebone Black so you might want to have a look at the following links.

    http://derekmolloy.ie/set-ip-address-to-be-static-on-the-beaglebone-black/

     

    http://derekmolloy.ie/beaglebone/getting-started-usb-network-adapter-on-the-beaglebone/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jomoenginer
    0 jomoenginer over 8 years ago

    I think Gunjan is not getting the wired  Ethernet or the USB IP to work on the Beaglebone Black so I believe it is not a Wi-Fi issue.

     

    @Gunjan - try running 'dmesg' on the Beagelbone to see if there are any messages that are related to the Ethernet port being down or the driver having issues.

    Also, as we mentioned previously, check 'ifconfig -a' to see if the Ethernet port is up or not.

     

    Have you tried rebooting the BBB or restart the network interface?

    You should be able to restart the network interface with:

     

    # sudo /etc/init.d/network restart

     

    Derek Molloy has pretty good instructions on how to set up the Ethernet ports on the Beaglebone Black so you might want to have a look at the following links.

    http://derekmolloy.ie/set-ip-address-to-be-static-on-the-beaglebone-black/

     

    http://derekmolloy.ie/beaglebone/getting-started-usb-network-adapter-on-the-beaglebone/