BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Need help with E14  Beaglebone  4.3  LCD  Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 23 replies
  • Answers 6 answers
  • Subscribers 109 subscribers
  • Views 6021 views
  • Users 0 members are here
  • lcd
  • beaglebone black lcd
  • lcd display
  • beagle bone black
  • 4.3" lcd
  • lcd screen
  • BeagleBone
  • beagle_bone
  • beagle_bone_black
  • beagleboneblackwireless
  • beaglebone_black_accessory
  • beagle_board
Related

Need help with E14  Beaglebone  4.3  LCD  Display

ninjatrent
ninjatrent over 9 years ago

I  am  having  trouble  flashing  the  Beaglebone  Black  Wireless eMMC  with  the  image  file  provided for  the  E14 Beaglebone  4.3  LCD  Display.

 

 

README - 4.3 LCD Display Cape for Beaglebone Black

 

4.3 LCD Display Cape for Beaglebone Board (White, Black, or Wireless)

 

 

I have  followed  the  instructions  for  flashing  the  eMMC but it's  not  working.

 

The  LED status lights  on the  BeagleBone  Black  W blink for  a  few seconds  and  go out. The  micro  SD status  light  remains  on constant after attempt  to  flash.

 

I can't figure  this  out. Beginning to  regret  the  purchase  of  this  Display.

The  first  one  arrived  damaged, had to  wait  for  a  replacement .

 

Now on day two  of  trying  to  get  this  display  to  work  with  the  Beaglebone  Black  W.

 

The image will boot from microSD and display will work.

 

I need to flash the eMMC with this image.

 

So far unsuccessful

 

It seems  the   image  is not   compatible  with  the  BBB Wireless.

 

When   checking   available   services  with   " connmanctl  technologies   ", ethernet   and gadget   were   listed   but   not   Bluetooth  and   wifi .image

 

This image   seems  to  be  only  compatible  with  the   Beaglebone  Black  and   not   the   Beaglebone  Black  Wireless .

 

Is there  any  one  who  might  be  able  to  assist  with  finding  a  solution  to  this  problem?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +3 suggested
    Hi Trent, Just by coincidence I was trying to put an image on the BBB Wireless a few nights ago. I don't have a display, so in my case I was using the images on the beagleboard website. Out of curiosity…
  • ninjatrent
    ninjatrent over 8 years ago +3 suggested
    The Debian 9.1 2017-08-31 4GB SD LXQT Desktop image available at Beagleboard is confirmed working properly with the Beaglebone LCD Display Cape. Wi-Fi and Bluetooth are detected. Chromium Desktop works…
  • alager
    alager over 9 years ago +2 suggested
    I don't have the wireless version, but I too had issues getting the image to transfer to the eMMC. What I finally found was that the image that has the bbcape43 support has the eMMC disabled. So in /boot…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Trent,

     

    Just by coincidence I was trying to put an image on the BBB Wireless a few nights ago. I don't have a display, so in my case I was using the images on the beagleboard website. Out of curiosity just now I checked and it appears to have a 'device tree' fragment file called BB-CAPE-DISP-CT4-00A0.dtbo, and this name appears in one of the comments here: README - 4.3 LCD Display Cape for Beaglebone Black   so I'm wondering if you might not need the specific image that is advertised for the cape, and instead the standard image could be used.

    To activate that device tree fragment, the command line (as root user) will be something like:

    echo BB-CAPE-DISP-CT4 > /sys/devices/platform/bone_capemgr/slots

    I don't know if anything more would be needed though. But it could be worth a try. You probably will also  need to use that command to disable the HDMI that Aaron mentions above too I guess.

    Also, incidentally, for the recent images, it would be worth just running from microSD and not eMMC, because they consume nearly the entire eMMC, not leaving much space for applications and updates. I found that out by accidentally filling up and the shell going crazy and having no bytes left to even delete files : )

    Also, things have changed for the past few releases, and now when you burn the image onto the SD card, it will no longer be readable on the PC, and it will seem as if the burn operation failed. But it will work.

    This really caught me out, because it isn't described anywhere that the image format has recently changed.

     

    Also some (nearly all) online documentation/blog posts about the device tree mention a path like /sys/devices/bone_capemgr/... but it looks like about a year ago, it changed, to /sys/devices/platform/bone_capemgr/.. which isn't great, since it means everyone's documentation is now incorrect : ( I wish they'd kept a link to the old path in the newer images : (

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago

    Hi Trent,

     

    Just by coincidence I was trying to put an image on the BBB Wireless a few nights ago. I don't have a display, so in my case I was using the images on the beagleboard website. Out of curiosity just now I checked and it appears to have a 'device tree' fragment file called BB-CAPE-DISP-CT4-00A0.dtbo, and this name appears in one of the comments here: README - 4.3 LCD Display Cape for Beaglebone Black   so I'm wondering if you might not need the specific image that is advertised for the cape, and instead the standard image could be used.

    To activate that device tree fragment, the command line (as root user) will be something like:

    echo BB-CAPE-DISP-CT4 > /sys/devices/platform/bone_capemgr/slots

    I don't know if anything more would be needed though. But it could be worth a try. You probably will also  need to use that command to disable the HDMI that Aaron mentions above too I guess.

    Also, incidentally, for the recent images, it would be worth just running from microSD and not eMMC, because they consume nearly the entire eMMC, not leaving much space for applications and updates. I found that out by accidentally filling up and the shell going crazy and having no bytes left to even delete files : )

    Also, things have changed for the past few releases, and now when you burn the image onto the SD card, it will no longer be readable on the PC, and it will seem as if the burn operation failed. But it will work.

    This really caught me out, because it isn't described anywhere that the image format has recently changed.

     

    Also some (nearly all) online documentation/blog posts about the device tree mention a path like /sys/devices/bone_capemgr/... but it looks like about a year ago, it changed, to /sys/devices/platform/bone_capemgr/.. which isn't great, since it means everyone's documentation is now incorrect : ( I wish they'd kept a link to the old path in the newer images : (

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to shabaz

    Hey Shabaz,

     

    I have yet to try the official  images from beagleboard.

     

    Going to make some time to test this weekend.

     

    It would be awesome to get the iot image to work with the display. I prefer working with terminal over desktop.

     

    Thanks for the suggestion, with hope I will post good results soon.

     

    Thanks again