BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BeagleBone Blue Quadcopter Drone - Need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 108 subscribers
  • Views 3234 views
  • Users 0 members are here
  • debian
  • single board computers
  • octavo
  • brushless motors
  • brushless dc motors
  • ardupilot
  • flight control systems
  • beaglebone blue projects
  • rc
  • beaglebone wireless
  • beaglebone black projects
  • Single Board Computer
  • rc plane
  • beaglebone blue drone
  • beaglebone_blue
  • rc car
  • electronic speed controller
  • robotics
  • beaglebone blue
  • flight controls
  • hobby electronics
  • linux debian
  • robot
  • beagleboard.org
  • drone
  • hobbyist
  • battery
  • BeagleBone
  • robotics cape
  • brushless motor
  • beaglebone drone
  • pocket beagle
  • beagleboard
  • texas instruments
  • beaglebone black wireless
  • quadcopter
  • beaglebone quadcopter
  • beagleboneblackwireless
  • robotics controller
  • ti
  • linux
Related

BeagleBone Blue Quadcopter Drone - Need help

ninjatrent
ninjatrent over 8 years ago

Hello Everyone,

 

I would like to use the BeagleBone Blue as the flight controller of my quadcopter drone and run ardupilotblue.

https://github.com/mirkix/ardupilotblue

image

 

The Brushless Motor Speed Control that I am using is the Racestar 20A 4in1 ESC mentioned in this parts list.

https://www.hackster.io/jkridner/beaglebone-blue-220mm-quadcopter-9801d8

image

 

 

I've been following guidance of these links and this tutorial but I've run into a few issues with construction.

     https://github.com/imfatant/test

 

First question, Is this Propeller Layout correct in this photo?

The orange props are the front/nose of the drone and black props at the rear.

image

The orange props have leading edge facing inwards and with the black props the trailing edge is facing inwards to the body.

My terminology and setup might be completely incorrect. For safety reasons the first test will be performed without the propellers attached.

 

 

 

image

In which direction should the ESC be oriented on the the chassis?

 

And Is the label side of ESC board meant to face upwards with the plug facing front of the drone?

image

Also, Which pins from the esc should be connected to the BeagleBone Blue?

image

I would like to mount the ESC to the bottom of the drone as shown in the photo below.

image

I'm unsure if the ESC should be facing label side upward and which direction the control wiring plug should be facing in orientation to the front of the drone.

The Lipo Battery will be located in the center of frame.

image

There will be a small First Person View Camera and transmitter in the nose with 5V power supplied from the BB Blue.

The BeagleBone Blue will be secured to the top deck with the onboard IMU chip at dead center.

 

I am waiting for the FPV Cam/Transmitter and Ublox M8N GPS to arrive tomorrow.

When complete this BB Blue Drone will be running ArduPilotBlue and will be carrying a GoPro Hero 5 Session on flights.

 

Thanks for your time reading this post and for any help.

 

Trent

ninjatrent

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 8 years ago in reply to ninjatrent +2
    They seem to be working now.
  • Fred27
    Fred27 over 8 years ago +2 suggested
    The props look like they match the setup in the Quad X Diagram to me. They will be providing lift when rotating in the direction shown in that diagram. The orientation of the ESC shouldn't matter. The…
  • shabaz
    shabaz over 8 years ago +2 verified
    Hi Trent, Quite surprising how elsewhere on the Internet this project doesn't have a single overall solution diagram or wiring diagram, or a single photo showing such detail. It looks like the original…
Parents
  • Fred27
    0 Fred27 over 8 years ago

    The props look like they match the setup in the Quad X Diagram to me. They will be providing lift when rotating in the direction shown in that diagram.

     

    The orientation of the ESC shouldn't matter. The IMU on the other hand does need to be orientated correctly.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Fred27
    0 Fred27 over 8 years ago

    The props look like they match the setup in the Quad X Diagram to me. They will be providing lift when rotating in the direction shown in that diagram.

     

    The orientation of the ESC shouldn't matter. The IMU on the other hand does need to be orientated correctly.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to Fred27

    The order of the motor wires on the esc are different from the order in the Quad X diagram above.

     

    Are the wires on ESC labeled "s1, s2, s3, s4" the signal wires for each motor and are these connected to the Servo signal wires on the BB Blue?

     

    If so, would I need to connect signal wires from esc in the same order as shown in the quad x diagram?

     

    As one might conclude, I've never built a drone. Plenty of flight time.