BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Accessing GPIO and PWM on BeagleBone AI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 36 replies
  • Answers 21 answers
  • Subscribers 110 subscribers
  • Views 10138 views
  • Users 0 members are here
  • beaglebone ai
Related

Accessing GPIO and PWM on BeagleBone AI

Sean_Miller
Sean_Miller over 7 years ago

I'm running through the BeagleBone examples for the AI, but the ones that attempt to read or write to pins throw errors in both Python and bonescript.

 

Here is the output from analoginout.js:

 

Hit ^C to stop

info: No pinmux for P9_14

fs.js:733

  var r = binding.read(fd, buffer, offset, length, position);

                 ^

Error: ETIMEDOUT: connection timed out, read

    at Error (native)

    at Object.fs.readSync (fs.js:733:19)

    at tryReadSync (fs.js:488:20)

    at Object.fs.readFileSync (fs.js:528:19)

    at Object.readAIN (/usr/local/lib/node_modules/bonescript/src/hw_mainline.js:287:30)

    at Object.f.analogRead (/usr/local/lib/node_modules/bonescript/src/index.js:330:19)

    at Timeout.loop [as _onTimeout] (/var/lib/cloud9/BeagleBone/AI/analogInOut.js:23:19)

    at ontimeout (timers.js:386:11)

    at tryOnTimeout (timers.js:250:5)

    at Timer.listOnTimeout (timers.js:214:5)

 

Is there a config I need to do first?  I see other's in the world with this issue on older BeagleBone's and the responses vary considerably.

 

This is the code:

const b = require('bonescript');


const inputPin  = "A3";
const outputPin = "P9_14";


console.log('Hit ^C to stop');
b.pinMode(outputPin, b.ANALOG_OUTPUT);
setTimeout(loop, 200);  // work-around to wait for PWM permissions


function loop() {
    var value = b.analogRead(inputPin);
    process.stdout.write(inputPin + '-->' + outputPin + ': ' + (value*100).toFixed(1) + '%   \r');
    b.analogWrite(outputPin, value);
    setTimeout(loop, 10);
}

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • Sean_Miller
    Sean_Miller over 7 years ago in reply to Sean_Miller +4
    YYYYYEEEEEAAA!!!!!!!! blinkLED.js works now!!! I always tell the boy...if you can blink an LED, you can change the world. The door is open! See ya', Sean
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to clem57 +2 suggested
    I saw these two references tonight in my hunt. My thoughts were "this surely is handled in by the bonescript and Python libraries on the fly, right?" "Otherwise, it would be in the comments in the header…
  • mayermakes
    mayermakes over 7 years ago in reply to clem57 +2 suggested
    The only thing I could find out about this issue is that the device tree files for the BB-AI are missing, there is currently no suitable file provided for the BB-AI all the BBB black files just brick the…
Parents
  • clem57
    0 clem57 over 7 years ago

    Yes since the number of pins is less than possible interfaces...

    https://www.bing.com/videos/search?q=how+to+setup+pins+beagle+bone&docid=608009253376952439&mid=30773886A1337BD47A863077…

     

    Or a better read https://vadl.github.io/beagleboneblack/2016/07/29/setting-up-bbb-gpio .

    Enjoying the BB-AI Sean_Miller ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 7 years ago in reply to clem57

    I saw these two references tonight in my hunt.  My thoughts were "this surely is handled in by the bonescript and Python libraries on the fly, right?"  "Otherwise, it would be in the comments in the header, right?"  I guess not.

     

    For the video, I didn't have the directories he showed for the capes and trees.

     

    I tried the redirect to export tricks, but still received the same error of having no pinmux.

     

    I'll run it harder through the paces tomorrow evening.  I found the tutorials just aren't out there like you find for Raspberry Pi and Arduino IDE driven microcontrollers.

     

    But, so, far, I love the idea of computations happening at the speed of the frame with the tidl libraries, love the Cloud 9 interface (1st time using it), and love being able to use it as an adhoc device while its connected to the internet.

     

    Just got to get an LED to blink and stop it from calling my black cat a ping-pong-ball.  image

     

    -Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Sean_Miller
    0 Sean_Miller over 7 years ago in reply to clem57

    I saw these two references tonight in my hunt.  My thoughts were "this surely is handled in by the bonescript and Python libraries on the fly, right?"  "Otherwise, it would be in the comments in the header, right?"  I guess not.

     

    For the video, I didn't have the directories he showed for the capes and trees.

     

    I tried the redirect to export tricks, but still received the same error of having no pinmux.

     

    I'll run it harder through the paces tomorrow evening.  I found the tutorials just aren't out there like you find for Raspberry Pi and Arduino IDE driven microcontrollers.

     

    But, so, far, I love the idea of computations happening at the speed of the frame with the tidl libraries, love the Cloud 9 interface (1st time using it), and love being able to use it as an adhoc device while its connected to the internet.

     

    Just got to get an LED to blink and stop it from calling my black cat a ping-pong-ball.  image

     

    -Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • clem57
    0 clem57 over 7 years ago in reply to Sean_Miller

    Just got to get an LED to blink and stop it from calling my black cat a ping-pong-ball.  image

     

    LMAO