BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Accessing GPIO and PWM on BeagleBone AI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 36 replies
  • Answers 21 answers
  • Subscribers 110 subscribers
  • Views 10138 views
  • Users 0 members are here
  • beaglebone ai
Related

Accessing GPIO and PWM on BeagleBone AI

Sean_Miller
Sean_Miller over 7 years ago

I'm running through the BeagleBone examples for the AI, but the ones that attempt to read or write to pins throw errors in both Python and bonescript.

 

Here is the output from analoginout.js:

 

Hit ^C to stop

info: No pinmux for P9_14

fs.js:733

  var r = binding.read(fd, buffer, offset, length, position);

                 ^

Error: ETIMEDOUT: connection timed out, read

    at Error (native)

    at Object.fs.readSync (fs.js:733:19)

    at tryReadSync (fs.js:488:20)

    at Object.fs.readFileSync (fs.js:528:19)

    at Object.readAIN (/usr/local/lib/node_modules/bonescript/src/hw_mainline.js:287:30)

    at Object.f.analogRead (/usr/local/lib/node_modules/bonescript/src/index.js:330:19)

    at Timeout.loop [as _onTimeout] (/var/lib/cloud9/BeagleBone/AI/analogInOut.js:23:19)

    at ontimeout (timers.js:386:11)

    at tryOnTimeout (timers.js:250:5)

    at Timer.listOnTimeout (timers.js:214:5)

 

Is there a config I need to do first?  I see other's in the world with this issue on older BeagleBone's and the responses vary considerably.

 

This is the code:

const b = require('bonescript');


const inputPin  = "A3";
const outputPin = "P9_14";


console.log('Hit ^C to stop');
b.pinMode(outputPin, b.ANALOG_OUTPUT);
setTimeout(loop, 200);  // work-around to wait for PWM permissions


function loop() {
    var value = b.analogRead(inputPin);
    process.stdout.write(inputPin + '-->' + outputPin + ': ' + (value*100).toFixed(1) + '%   \r');
    b.analogWrite(outputPin, value);
    setTimeout(loop, 10);
}

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • Sean_Miller
    Sean_Miller over 7 years ago in reply to Sean_Miller +4
    YYYYYEEEEEAAA!!!!!!!! blinkLED.js works now!!! I always tell the boy...if you can blink an LED, you can change the world. The door is open! See ya', Sean
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to clem57 +2 suggested
    I saw these two references tonight in my hunt. My thoughts were "this surely is handled in by the bonescript and Python libraries on the fly, right?" "Otherwise, it would be in the comments in the header…
  • mayermakes
    mayermakes over 7 years ago in reply to clem57 +2 suggested
    The only thing I could find out about this issue is that the device tree files for the BB-AI are missing, there is currently no suitable file provided for the BB-AI all the BBB black files just brick the…
Parents
  • Sean_Miller
    0 Sean_Miller over 7 years ago

    Jason Kridner has released a beta for the BBAI GPIO libraries for node.js:

     

     

    https://groups.google.com/forum/embed/?place=forum%2Fbeagleboard&showsearch=true&showpopout=true&showtabs=false&hideforu…

     

    I'm try to get something going tomorrow.

     

    He also released an update that was to fix the tidl examples, but that one went backwards on me and now I can't get it to execute without error.  It's been posted to his support forum.

     

    -Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 7 years ago in reply to Sean_Miller

    YYYYYEEEEEAAA!!!!!!!!  blinkLED.js works now!!!

     

    I always tell the boy...if you can blink an LED, you can change the world.

     

    The door is open!

     

    See ya',

    Sean

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Sean_Miller
    0 Sean_Miller over 7 years ago in reply to Sean_Miller

    YYYYYEEEEEAAA!!!!!!!!  blinkLED.js works now!!!

     

    I always tell the boy...if you can blink an LED, you can change the world.

     

    The door is open!

     

    See ya',

    Sean

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mp2100
    0 mp2100 over 7 years ago in reply to Sean_Miller

    This is great to know.  Progress is being made.  (even if it's marked as "unsafe-perm")