BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beagle Bone Black Serial UART Speed is Slow
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 107 subscribers
  • Views 1421 views
  • Users 0 members are here
  • bbb
Related

Beagle Bone Black Serial UART Speed is Slow

kpokigo99
kpokigo99 over 6 years ago

I am using the BBB and setting up UARTS one the I/O pins.

Example UART4, P9 pins 11 and 13.

I am set for 9600 baud

Im looking at teh bit patter on an oscilloscope and notice the serial speed comes out of the port at a rate slower than 9600 baud (about 7-8% slower)

That means that rate is outside of the acceptable speed tolerance of about 5% for the serial 9600 standard.

I cannot properly communicate with serial devices that use 9600 baud.

Any idea on the cause of this and if there is some sort of calibration that can be done to improve the accuracy of the UART.

I am using Debian operating system

To run the tests I am using minicom

 

 

Ken

  • Sign in to reply
  • Cancel

Top Replies

  • gdstew
    gdstew over 6 years ago +1 suggested
    If the UART baud rate counter and the timer that supplies the UART clocks (4) are set correctly the baud rate should be within 0.16% at 9600 baud as specified by the TI AM335x Technical Reference Manual…
Parents
  • gdstew
    0 gdstew over 6 years ago

    If the UART baud rate counter and the timer that supplies the UART clocks (4) are set correctly the baud rate should be within

    0.16% at 9600 baud as specified by the TI AM335x Technical Reference Manual. I did some quick calculations on the values

    given in the manual and they are correct. It would seem(?) that one of the two is not being set to the correct count value. As

    far as I know it should be the Debian that sets these counter/timer values based on the baud rate requested by minicom. Since

    these timers are all internal the only way to verify they are correct would be to read the timer count and UART divisor registers

    after minicom has been started.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 6 years ago

    If the UART baud rate counter and the timer that supplies the UART clocks (4) are set correctly the baud rate should be within

    0.16% at 9600 baud as specified by the TI AM335x Technical Reference Manual. I did some quick calculations on the values

    given in the manual and they are correct. It would seem(?) that one of the two is not being set to the correct count value. As

    far as I know it should be the Debian that sets these counter/timer values based on the baud rate requested by minicom. Since

    these timers are all internal the only way to verify they are correct would be to read the timer count and UART divisor registers

    after minicom has been started.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer