BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Ben Heck's Beaglebone Black Geocache
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 107 subscribers
  • Views 1917 views
  • Users 0 members are here
  • tbhs
  • geocache
  • bbb
  • element14 presents
  • beagle_bone_black
  • beagle_board
Related

Ben Heck's Beaglebone Black Geocache

adamsoileau1
adamsoileau1 over 5 years ago

A few years back Ben created a BeagleBone Geocache that saved pictures and messages when discovered. Currently, I have my hands on it and am curious what you would like to see added or changed on the build. I have some experience with Raspberry Pis, but I would like to know if anyone has worked BeagleBones before and what the benefit may be for using one over a Raspberry Pi -- because a Pi usually my go-to single board computer. I have a few ideas like implementing solar cells to improve the battery life and maybe more clues for unlocking the device, but I would like to know what the community thinks of the project and what they would like to see included!

 

Original Episode: Episode 197: Ben Heck's BeagleBone Black Geocache Episode

  • Sign in to reply
  • Cancel

Top Replies

  • mp2100
    mp2100 over 5 years ago +3 suggested
    Adam, scanning quickly through Ben's geocache video, I assume he selected the BBB for a couple of reasons. Using the built-in eMMC memory, it boots up fast, and shuts down fast, compared to a Raspberry…
  • cstanton
    cstanton over 5 years ago +1
    The BeagleBone Black has three main features going for it: - It's pretty much fully open source - You have two microcontrollers that run at 200MHz onboard for real-time handling of things like vision sensors…
  • adamsoileau1
    adamsoileau1 over 5 years ago in reply to cstanton +1
    Thank you for the information! I definitely need to grab one and try it out. Now, I am certainly interested
Parents
  • mp2100
    0 mp2100 over 5 years ago

    Adam, scanning quickly through Ben's geocache video, I assume he selected the BBB for a couple of reasons.  Using the built-in eMMC memory, it boots up fast, and shuts down fast, compared to a Raspberry Pi.  He was optimizing the battery life.  Especially in the "old days", the BBB operating system was Angstrom, and it was fast.  I assume Ben used the lite version of debian (called the IoT version).  The Pi could have been substituted for the BBB.  Another advantage is the BBB power draw, it can reliably be powered by a USB 2.0 connection (5 v at 0.5 amps).  The BBB isn't as fast as a Pi 2 or Pi3.  It was fast enough for Ben's objectives.

     

    The Pi is definitely easier to learn because of its popularity, there are examples for everything you can think of.  I use both SBCs.  Among the reasons I like the BBB is has true analog inputs for sensor readings, and it has the PRU processors for real-time tasks.  Those reasons probably don't help with geocaching though.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • adamsoileau1
    0 adamsoileau1 over 5 years ago in reply to mp2100

    Awesome! Thank you for the input! I'm probably going to pick up a BBB and investigate a little more. I have not used one before, and I am curious to know if the Pi4 boots faster than the BBB with the newest operating system. It has been a while since I used anything older than a Pi3B -- I think the Pi2 was released before Ben made the project, but I am assuming the Pi4 boots faster than the older models; however, I am definitely not sure. I would not be surprised if the BBB boots faster than the Pi2, so that would make sense as to why he chose it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • adamsoileau1
    0 adamsoileau1 over 5 years ago in reply to mp2100

    Awesome! Thank you for the input! I'm probably going to pick up a BBB and investigate a little more. I have not used one before, and I am curious to know if the Pi4 boots faster than the BBB with the newest operating system. It has been a while since I used anything older than a Pi3B -- I think the Pi2 was released before Ben made the project, but I am assuming the Pi4 boots faster than the older models; however, I am definitely not sure. I would not be surprised if the BBB boots faster than the Pi2, so that would make sense as to why he chose it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mp2100
    0 mp2100 over 5 years ago in reply to adamsoileau1

    Huh. Now someone has the bbb booting in 3 seconds. Well, from thevideo it’s a bb green.


    https://www.linkedin.com/feed/update/urn:li:activity:6788102767182434304