BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum What hinders your BeagleBone project?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 106 subscribers
  • Views 5456 views
  • Users 0 members are here
  • projects
  • BeagleBone
  • beagleboard
  • introduction
  • BeagleBone Black
Related

What hinders your BeagleBone project?

cstanton
cstanton over 4 years ago

You could call this a series of discussions... 

When I was first introduced to BeagleBone, the BeagleBone Black was just released, and I managed to kill it. 5 volts on a 3.3v logical input without being aware thanks to a devicetree not being updated for an LCD display, but I had no idea, I'd only just been given the hardware and I was entirely new to it. Completely killed the kit. Then there was the difficulty of working with assembly for the PRUSS... it was a long list of interruptions.

So what tends to stop you from developing with a BeagleBone? Do you find that you encounter a problem part way through the project? Is it some knowledge you're lacking or is it the software? Is it how the hardware behaves or doesn't how you expect it to? Is it the operating system when you want to work bare bones or bare metal with the hardware?

Would you benefit from help with Linux? Or is it something else?

We're looking at expanding our content and what we ask from BeagleBoard to help introduce their products and guidance on their products, and I'm interested in what you need help with, so reply and let us know, regardless of knowledge level.

  • Sign in to reply
  • Cancel

Top Replies

  • mp2100
    mp2100 over 4 years ago +3
    I really like the beaglebone, same as Jan, my favorite SBC. I own many of them, several colors, bbb, bbg, bbbw, bb-ai, pocket beagle, even a beagleboard xm. The bbb is great for IoT and tinkering with…
  • Jan Cumps
    Jan Cumps over 4 years ago +1
    In my case, the consistency of the project - to keep things up to date after relaease. BB is my preferred SBC. I work more on a Pi these days but I started with BB and it has a favourite spot in my heart…
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to BigG +1
    For me, the rollover from µC to SBC (except for size) is when I'm building gateway/edge devices have database, or processes with a long lifecycle that are candidates for the likes of node-RED calculation…
Parents
  • shabaz
    shabaz over 4 years ago

    There was a period where so much code and blogs were broken because device paths changed, and not everyone updates blogs or code, so nothing seemed to work.

    Also, there just wasn't any C library for I/O (at least, not for fast I/O), so I had to write my own, and having to delve into the register configurations (non-trivial, it was different for the various banks of pins) and then repeating for different functions like I2C etc., got really hard to maintain, and I don't know what the recommended speedy library is today that is usable like (say) mbed or Arduino with DigitalRead/DigitalWrite etc., so that it could be easy to pick up. The Pi has ready-to-use libraries in C, and they are reasonably fast. I'd say that holds me back from using the BBB a bit nowadays - Pi is just easier to quickly get into, despite the BBB having better hardware in some ways (and less features in others, e.g. 5 GHz WLAN absence, less memory. etc). Still, I really like the BBB, it's got better audio features for instance, and hope that if there were well-documented good libraries (I'm sure there are, I just don't know about them) for I/O (for C and for Python) then I'd use it more.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 4 years ago

    There was a period where so much code and blogs were broken because device paths changed, and not everyone updates blogs or code, so nothing seemed to work.

    Also, there just wasn't any C library for I/O (at least, not for fast I/O), so I had to write my own, and having to delve into the register configurations (non-trivial, it was different for the various banks of pins) and then repeating for different functions like I2C etc., got really hard to maintain, and I don't know what the recommended speedy library is today that is usable like (say) mbed or Arduino with DigitalRead/DigitalWrite etc., so that it could be easy to pick up. The Pi has ready-to-use libraries in C, and they are reasonably fast. I'd say that holds me back from using the BBB a bit nowadays - Pi is just easier to quickly get into, despite the BBB having better hardware in some ways (and less features in others, e.g. 5 GHz WLAN absence, less memory. etc). Still, I really like the BBB, it's got better audio features for instance, and hope that if there were well-documented good libraries (I'm sure there are, I just don't know about them) for I/O (for C and for Python) then I'd use it more.