BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Another board - BeagleV-Ahead
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 105 subscribers
  • Views 2974 views
  • Users 0 members are here
  • risc-v
  • beagleboard
Related

Another board - BeagleV-Ahead

Fred27
Fred27 over 3 years ago

Hot on the heel of the BeaglePlay, it seems there's another new BeagleBoard offering - the BeagleV-Ahead.

https://beagleboard.org/beaglev-ahead
https://forum.beagleboard.org/t/beaglev-ahead-new-risc-v-computer-from-beagleboard-org-is-broadly-available-now-around-150/35317

Personally, I feel that whilst it's great that they're producing new boards, it would be even better if the existing ones were "finished" (i.e. documentation and example code) before things move on to the latest shiny thing.

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 3 years ago +1
    Hi Fred, I've converted this to a forum thread from blog post as it looked more like a thread. I also started a similar one here : Welcome to the BeagleV Ahead! The RISC based single board computer.…
  • Fred27
    Fred27 over 3 years ago in reply to cstanton +1
    I'm keeping an eye out. I regularly check to see if the BeaglePlay documentation has been updated yet. I was doing so when I spotted this. If you need one reviewed then I'd be happy to oblige. I will…
  • cstanton
    cstanton over 3 years ago in reply to Fred27 +1
    Fred27 said: I will be as honest as I was with the BeaglePlay one though. I would expect nothing less
  • Fred27
    Fred27 over 3 years ago

    It looks very much like a RISC-V version of the BeagleBone Black. The things that jumps out at me are:

    • It runs Ubuntu rather than the Debian on other boards. I wonder why this is. Must be something to do with the RISC-V I suppose.
    • It has a mikroBUS shuttle rather than a standard mikroBUSconnector, Yet another standard!
    • It has a micro USB 3.0 connector. These always look odd.

    I also found out from the unboxing video that it's called the Beagle "Vee" but the processor is a RISC "Five". I always wondered how RISC-V was pronounced (i.e. letter or number). Now I know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago

    Hi Fred, I've converted this to a forum thread from blog post as it looked more like a thread.

    I also started a similar one here :  Welcome to the BeagleV Ahead! The RISC based single board computer. - glad to see you're also keeping an eye on beagleboard :)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 3 years ago in reply to cstanton

    I'm keeping an eye out. I regularly check to see if the BeaglePlay documentation has been updated yet. I was doing so when I spotted this.

    If you need one reviewed then I'd be happy to oblige. I will be as honest as I was with the BeaglePlay one though. Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to Fred27
    Fred27 said:
    I will be as honest as I was with the BeaglePlay one though. 

    I would expect nothing less Slight smile 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago
    Fred27 said:
    better if the existing ones were "finished" (i.e. documentation and example code)

    Business as usual. 
    image

    The link to the processor on the product home page goes to a taobao error page. They aren't even trying.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    On the document page, they talk about TI AM6254 instead of the RISK-V

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    I just tried to fix it, but it's in GitLab, so you'd have to create a branch and submit a merge request, even for small changes, which means it's not going to get done much, I gave up. I'm surprised the documentation isn't a wiki.

    Also, I'm still waiting on BeagleConnect Freedom documentation. I don't even think a lot of documentation is needed, just enough for the community to run with things. But with absolutely no information, I'm stuck. Everywhere I looked it was "to do". Hope it's better with the Beagle-V, but I still want to use the BCF as mentioned too..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to shabaz

    Maybe it's worth reaching out to them directly on discord?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to cstanton

    Hi Christopher, 

    Thanks for that. I had left them a couple of messages on the BeagleBoard forum, but neither message resulted in anything much. Discord is a great idea. I'll reach out tonight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iker46
    iker46 over 3 years ago

    I completely agree with you, Fred. It has been such a pain to test the BeaglePlay and meet the deadline. It is supposed to be plug&play and it is really far from that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>