BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum This Beagle's on Fire
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 105 subscribers
  • Views 3800 views
  • Users 0 members are here
  • beaglev-fire
  • beaglev
  • beagleboard
Related

This Beagle's on Fire

cstanton
cstanton over 3 years ago

image

https://docs.beagleboard.org/latest/boards/beaglev/fire/ 

Feature

Description

Processor

MPFS025T-FCVG484E

Memory

2GB (1Gb x 16)- 1866MHz 3733Mbps, LPDDR4

Storage

Kingston 16GB eMMC

Wireless

1x M.2 Key E, support 2.4GHz/5GHz WiFi module

Ethernet

  • PHY: Realtek RTL8211F-VD-CG Gigabit Ethernet phy

  • Connector: integrated magnetics RJ-45

USB C

  • Connectivity: Flash/programming support

  • Power: Input: 5V @ <To-Do>

Other connectors

  • 1x SYZYGY High speed connector

  • microSD card slot

  • CSI connector compatible with BeagleBone AI-64, BeagleV-Ahead, Raspberry Pi Zero / CM4 (22-pin)

This product information should be treat as 'preliminary' and 'draft' - I'm definitely hoping for documentation Slight smile I wasn't aware microchip made RISC processors though, perhaps I shouldn't be surprised?

  • Sign in to reply
  • Cancel

Top Replies

  • misaz
    misaz over 3 years ago +4
    It is not RISC procesor. It is FPGA combined with RISC-V procesor(s). Similar FPGA (but without CPU part; just FPGA) we RoadTested few years ago: /products/roadtest/rv/roadtest_reviews/1632/microchi…
  • Fred27
    Fred27 over 3 years ago +3
    This certainly looks interesting, but it worries me that they're churning out new boards whilst the documentation for existing boards (e.g. BeaglePlay, Beagle Freedom Connect) is still mostly "TO DO".…
  • cstanton
    cstanton over 3 years ago in reply to kmikemoo +2
    I shorted out my original BeagleBone Black because of a poor default device tree for the official LCD screen, does that count?
Parents
  • misaz
    0 misaz over 3 years ago

    It is not RISC procesor. It is FPGA combined with RISC-V procesor(s). Similar FPGA (but without CPU part; just FPGA) we RoadTested few years ago:

    /products/roadtest/rv/roadtest_reviews/1632/microchip_polarfire_1

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • misaz
    0 misaz over 3 years ago

    It is not RISC procesor. It is FPGA combined with RISC-V procesor(s). Similar FPGA (but without CPU part; just FPGA) we RoadTested few years ago:

    /products/roadtest/rv/roadtest_reviews/1632/microchip_polarfire_1

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • cstanton
    0 cstanton over 3 years ago in reply to misaz

    Thanks misaz I appreciate the detail, I had not entirely picked up on that!