BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum This Beagle's on Fire
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 105 subscribers
  • Views 3800 views
  • Users 0 members are here
  • beaglev-fire
  • beaglev
  • beagleboard
Related

This Beagle's on Fire

cstanton
cstanton over 3 years ago

image

https://docs.beagleboard.org/latest/boards/beaglev/fire/ 

Feature

Description

Processor

MPFS025T-FCVG484E

Memory

2GB (1Gb x 16)- 1866MHz 3733Mbps, LPDDR4

Storage

Kingston 16GB eMMC

Wireless

1x M.2 Key E, support 2.4GHz/5GHz WiFi module

Ethernet

  • PHY: Realtek RTL8211F-VD-CG Gigabit Ethernet phy

  • Connector: integrated magnetics RJ-45

USB C

  • Connectivity: Flash/programming support

  • Power: Input: 5V @ <To-Do>

Other connectors

  • 1x SYZYGY High speed connector

  • microSD card slot

  • CSI connector compatible with BeagleBone AI-64, BeagleV-Ahead, Raspberry Pi Zero / CM4 (22-pin)

This product information should be treat as 'preliminary' and 'draft' - I'm definitely hoping for documentation Slight smile I wasn't aware microchip made RISC processors though, perhaps I shouldn't be surprised?

  • Sign in to reply
  • Cancel

Top Replies

  • misaz
    misaz over 3 years ago +4
    It is not RISC procesor. It is FPGA combined with RISC-V procesor(s). Similar FPGA (but without CPU part; just FPGA) we RoadTested few years ago: /products/roadtest/rv/roadtest_reviews/1632/microchi…
  • Fred27
    Fred27 over 3 years ago +3
    This certainly looks interesting, but it worries me that they're churning out new boards whilst the documentation for existing boards (e.g. BeaglePlay, Beagle Freedom Connect) is still mostly "TO DO".…
  • cstanton
    cstanton over 3 years ago in reply to kmikemoo +2
    I shorted out my original BeagleBone Black because of a poor default device tree for the official LCD screen, does that count?
Parents
  • Fred27
    0 Fred27 over 3 years ago

    This certainly looks interesting, but it worries me that they're churning out new boards whilst the documentation for existing boards (e.g. BeaglePlay, Beagle Freedom Connect) is still mostly "TO DO". I'm sure they're having fun moving onto the next new shiny toy, but it doesn't make it easy for end users.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 3 years ago in reply to Fred27

    I agree wholeheartedly and we are passing on that sentiment.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cstanton
    0 cstanton over 3 years ago in reply to Fred27

    I agree wholeheartedly and we are passing on that sentiment.