BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Can a BBB run Debian 11.7 GUI?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 107 subscribers
  • Views 1628 views
  • Users 0 members are here
Related

Can a BBB run Debian 11.7 GUI?

landolfi
landolfi over 2 years ago

I inherited an Element14 Beaglebone Black from my grandson and tried to install the latest Debian 11.7 GUI software image on it from https://www.beagleboard.org/distros/am335x-11-7-2023-09-02-4gb-emmc-xfce-flasher.

The GUI loads the first time I boot after flashing, but subsequent boots go to a command prompt, and when I try to install anything it says "no space left on device", leading me to think the only way to run a GUI is off SD even though I got the image directly from the BBB software images. Any other ideas?

I don't have a specific application for this, just wanted to use the UI to play around with it. I've also noticed from previous times I had a UI running, my 802.11n Edimax USB wifi module and browser are incredibly resource intensive and slow even with the router only 20 feet away. Would an older, non-GUI OS solve the slow wifi performance?

Thanks,
Bob

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +2
    Hi Bob, You're correct, the BBB needs a micro SD card for any reasonable image with GUI, i.e. desktop. The build-in storage (eMMC) is quite small. The BBB is a very underpowered platform nowadays, so…
  • cstanton
    cstanton over 2 years ago in reply to shabaz +2
    shabaz said: (those will require a micro SD card) Or USB, or even with the Pi 5 an nvme with the appropriate hat! And perhaps even network boot. I cannot remember if the BBB supported pxe booting.
  • bidrohini
    bidrohini over 2 years ago +1
    Flash the Debian 11.7 XFCE image to an SD card instead of using the eMMC, or switch to a lighter distribution. Consider a non-GUI OS to free up resources and improve Wi-Fi performance.
Parents
  • bidrohini
    0 bidrohini over 2 years ago

    Flash the Debian 11.7 XFCE image to an SD card instead of using the eMMC, or switch to a lighter distribution. Consider a non-GUI OS to free up resources and improve Wi-Fi performance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bidrohini
    0 bidrohini over 2 years ago

    Flash the Debian 11.7 XFCE image to an SD card instead of using the eMMC, or switch to a lighter distribution. Consider a non-GUI OS to free up resources and improve Wi-Fi performance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • landolfi
    0 landolfi over 2 years ago in reply to bidrohini

    Thanks to all! This all began because the factory eMMC image wouldn't drive the wireless module. I had previously tried LXQT 9.1 on SD with no significant performance improvement. I'll try going back to the oldest GUI on SD and if that doesn't work I'll settle for a non-GUI.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mp2100
    0 mp2100 over 2 years ago in reply to landolfi

    Yes. I love the bbb, but Even 5 years ago the bbb was slow with xwindows gui. You could try and flash really old angstrom images onto it but that would be not very secure by today’s standards.