BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone Blue Bricked
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 108 subscribers
  • Views 3942 views
  • Users 0 members are here
  • debian
  • beaglebone#
  • beaglebone blue
Related

Beaglebone Blue Bricked

jomoenginer
jomoenginer over 8 years ago

So, I loaded the latest Debian image for the Beaglebone boards, Debian 9.5 2018-10-07 4GB SD LXQT, and was using this for a short bit, but for some reason after trying to run a QT compiled program via remote ssh the BBBlue froze and will not boot any more.  I powered off the board and when it powers on only the Green and Red LEDS from the status bank stay constantly on and the Battery LEDs flash a bit but then 2 stay on constantly; CHG and the one labeled 75.

I have removed all of the EduMIP connections from the board as well as a n LCD that was connected but still nothing happens.  This board does not have the FTDI connections like the Black so I do not have a way to get a console to it to see if it is locking up somewhere.  

 

I've tried removing the SD card as well as use a known good one but still no luck. 

 

This board was running fine for sometime now so I am not sure what happened.  It was not until I loaded the new image that I ran into an issue.

 

Anyone else run into this issue with the Blue?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 8 years ago +4
    I got it working with an MSP432, Jon I'll write down the instructions. It's easy.
  • Jan Cumps
    Jan Cumps over 8 years ago +3
    I have a Green (from Seeed) - so not the same one as you. Have you tried pushing the User button with the working SD Card inserted, and then providing power?
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jomoenginer +3
    Maybe jkridner knows how to revive a bricked Blue?
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    I have a Green (from Seeed) - so not the same one as you. Have you tried pushing the User button with the working SD Card inserted, and then providing power?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 8 years ago

    I have a Green (from Seeed) - so not the same one as you. Have you tried pushing the User button with the working SD Card inserted, and then providing power?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jomoenginer
    jomoenginer over 8 years ago in reply to Jan Cumps

    Yeah, the Blue has an "SD" button but nothing changes if I power the board while pressing any of the buttons on the board including the SD button.  I appears to be dead.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jomoenginer

    Maybe jkridner knows how to revive a bricked Blue?

    • Cancel
    • Vote Up +3 Vote Down