BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone Blue Bricked
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 108 subscribers
  • Views 3940 views
  • Users 0 members are here
  • debian
  • beaglebone#
  • beaglebone blue
Related

Beaglebone Blue Bricked

jomoenginer
jomoenginer over 8 years ago

So, I loaded the latest Debian image for the Beaglebone boards, Debian 9.5 2018-10-07 4GB SD LXQT, and was using this for a short bit, but for some reason after trying to run a QT compiled program via remote ssh the BBBlue froze and will not boot any more.  I powered off the board and when it powers on only the Green and Red LEDS from the status bank stay constantly on and the Battery LEDs flash a bit but then 2 stay on constantly; CHG and the one labeled 75.

I have removed all of the EduMIP connections from the board as well as a n LCD that was connected but still nothing happens.  This board does not have the FTDI connections like the Black so I do not have a way to get a console to it to see if it is locking up somewhere.  

 

I've tried removing the SD card as well as use a known good one but still no luck. 

 

This board was running fine for sometime now so I am not sure what happened.  It was not until I loaded the new image that I ran into an issue.

 

Anyone else run into this issue with the Blue?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 8 years ago +4
    I got it working with an MSP432, Jon I'll write down the instructions. It's easy.
  • Jan Cumps
    Jan Cumps over 8 years ago +3
    I have a Green (from Seeed) - so not the same one as you. Have you tried pushing the User button with the working SD Card inserted, and then providing power?
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jomoenginer +3
    Maybe jkridner knows how to revive a bricked Blue?
  • Jan Cumps
    Jan Cumps over 8 years ago

    I have a Green (from Seeed) - so not the same one as you. Have you tried pushing the User button with the working SD Card inserted, and then providing power?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to Jan Cumps

    Yeah, the Blue has an "SD" button but nothing changes if I power the board while pressing any of the buttons on the board including the SD button.  I appears to be dead.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jomoenginer

    Maybe jkridner knows how to revive a bricked Blue?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago

    That's disappointing if the design doesn't have UART console pins : (

    I don't have a BB-Blue, but was wondering, does it make any difference if a battery is also connected, as well as the 12V supply? With the original BBB design, if it was modified for battery operation, then the battery needed to be present even if it wasn't charged. Probably the BB-Blue design is different but it could be worth a try. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to shabaz

    There are a couple of UARTs mapped to JST connections on the Blue.  I'll have to see if I rig a FTDI to JSt connection to one of these to see if there is any console output.

     

    As far as power, I've tried with and without the battery connected while the 12v supply was connected.  I also, tried running with just the battery as well as with just the USB connected.  Each has the same result with the Blue not booting. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jomoenginer

    if you happen to have a Bus Pirate, it allows to act as a USB / UART passtrough (attention: 3.3 V signals on the TX/RX pins, not RS232 compatible.

     

    If I recall well, you can also turn an MSP432 LaunchPad in a USB to Uart converter by tapping off the pins between debugger and controller section.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago

    I got it working with an MSP432, Jon

    image

     

    I'll write down the instructions. It's easy.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to Jan Cumps

    A Bus Pirate would be cool, but I have a few FTDI to USB cables so they should suffice with regards to connecting to  a UART on the Blue.  I am just not sure if the console on the Blue is being sent to a UART or not.  I'll have to try and see.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to Jan Cumps

    Yeah!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    Locate the debug header. I used this website as inspiration.

    Ultimate Serial Port

     

    image

     

    You need:

    MSP432 LaunchPad , red or black) and BB

    2 USB cables, one for each. Don't plug in yet.

    3 female to female jumpers (I only have male to female and used a breadboard as interconnect.

    On your MSP432, remove the RXD and TXD jumpers in the middle. Don't worry about the other 4, they can be mounted or removed.

    image

    Connect TX to TX, RX to RX. (yes, I thought I needed to swap but it is what it is - edit:because the PCB of the launchpad labels the microcontroller side signals). See schematic. Tap the signals from the debugger side of the LaunchPad

     

    Then connect the MSP432 USB. Check in the Device monitor what port number is assigned to the UART.

    Open Putty, create a serial connection.

    Here are the settings (use your com port)

    image

    Connect.

     

    Nothing shows. That's normal

     

    Now plug in your BeagleBoard. Your putty session is an active UART session into the debug port.

     

    Good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>