BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Kernel configurations reset by make command
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 107 subscribers
  • Views 795 views
  • Users 0 members are here
Related

Kernel configurations reset by make command

elem2018
elem2018 over 7 years ago

Hi There,

 

my environment:

BBB, ti-processor-sdk-linux-am335x-evm-05.01.00.11

 

After running

$(MAKE) -C $(LINUXKERNEL_INSTALL_DIR) ARCH=arm CROSS_COMPILE=$(CROSS_COMPILE)  tisdk_am335x-evm_defconfig

I get .config file in the linux kernel root path

 

Now I changed CONFIG_BRCMFMAC=m to CONFIG_BRCMFMAC=y  in this .config file to get inbuild driver.

 

After that I built the dtb file

$(MAKE) -j $(MAKE_JOBS) -C $(LINUXKERNEL_INSTALL_DIR) ARCH=arm CROSS_COMPILE=$(CROSS_COMPILE)  am335x-boneblack.dtb

 

Now strange thing happened:

CONFIG_BRCMFMAC=y in the .config file is set back to CONFIG_BRCMFMAC=m,   not what I wanted CONFIG_BRCMFMAC=y !

It seems that the make command reset the .config file.

 

Question:

How can I make sure that CONFIG_BRCMFMAC=y stays permanently, not reset by the make command?  I tried to do it in the tisdk_am335x-evm_defconfig file, but the same results.

 

Regards

Xi

  • Sign in to reply
  • Cancel
Parents
  • elem2018
    elem2018 over 7 years ago

    Hi,

     

    excatly speaking it is not reset, but ovewritten.  Now I find out that the FMAC driver can't be set as built-in, running menuconfig I can only choose either FMAC as module or no FMAC. In the appropriate Kconfig file, I see the FMAC is defined as tristate,

    so it is strange why only two states are allowed.  The Linux kernel versoin 4.14.67.  Thanks in advance for any hint

     

    Regards

    Xi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • elem2018
    elem2018 over 7 years ago

    Hi,

     

    excatly speaking it is not reset, but ovewritten.  Now I find out that the FMAC driver can't be set as built-in, running menuconfig I can only choose either FMAC as module or no FMAC. In the appropriate Kconfig file, I see the FMAC is defined as tristate,

    so it is strange why only two states are allowed.  The Linux kernel versoin 4.14.67.  Thanks in advance for any hint

     

    Regards

    Xi