RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog Rooting Android for the RIoTBoard
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: radiatortwo
  • Date Created: 24 May 2014 1:38 PM Date Created
  • Views 3916 views
  • Likes 1 like
  • Comments 10 comments
  • android
  • riotboard
  • root
Related
Recommended

Rooting Android for the RIoTBoard

radiatortwo
radiatortwo
24 May 2014

I´m not an Android developer. I´m using my RIoTBoard mainly with a Debian Linux distribution.

but because I am rooting all of my Android devices, I thought why not root the RIoTBoard as well. Just for fun.

It´s still an Android development board however and someone might need it.

 

And boy was that a journey. But I made it and here is how I did it.

(This was tested with the Downloadable Image you get here at Element14 and also with the image compiled with development configuration with build-type "eng")

 

What you need before you can start:

I´m assuming since you´re using the RIoTBoard as a development platform, that you have the Android SDK installed and adb is configured.

If not. Well you don´t need to download the whole SDK. When using Windows you can use the "15 seconds adb installer" from a thread at XDA Developers. (Google it)

It also has the needed drivers integrated. Just choose yes when asked to install it. Also I suggest to install adb and fastboot globally when asked.

Also don´t forget to activate USB debugging inside the Android Developer Options. (Look here at part 2 and 3 on how to do that. How to Install Netflix Streaming on the RIoTBoard)

 

Next thing needed is the zip file attached to this blog post.

Inside the zip file are the scripts, the su binary and a SuperSu.apk. I tried using SuperUser but i only got it working with this version of SuperSu.

Also i integrated a terminal app to test root in the end.

Extract all the files into a folder.

 

Also you´ll need a connection to the UART serial port with putty or similar.

 

Now let´s start this.

Open a cmd window inside the folder you extracted the files to and execute the following commands.

 

adb push su /data/local/tmp
adb push SuperSu.apk /data/local/tmp
adb push 99SuperSUDaemon /data/local/tmp
adb push install-recovery.sh /data/local/tmp
adb install terminal.apk

 

Installing the terminal app is optional. But with that you can test if root is working.

 

Next switch to your UART connection terminal and execute the following commands.

(You have to be root to execute the commands. So look if you are connected as root@riot_6solo)

 

mount -w -o remount /dev/block/mmcblk0p5 /system

mkdir /system/etc/init.d
mkdir /system/bin/.ext

cp /data/local/tmp/su /system/bin/.ext/.su
cp /data/local/tmp/su /system/xbin/daemonsu
cp /data/local/tmp/su /system/xbin/su
cp /data/local/tmp/SuperSu.apk /system/app/SuperSu.apk
cp /data/local/tmp/99SuperSUDaemon /system/etc/init.d/99SuperSUDaemon
cp /data/local/tmp/install-recovery.sh /system/etc/install-recovery.sh
echo 1 > /system/etc/.installed_su_daemon

chmod 0777 /system/bin/.ext
chmod 06755 /system/bin/.ext/.su
chmod 06755 /system/xbin/su
chmod 0755 /system/xbin/daemonsu
chmod 0755 /system/etc/install-recovery.sh
chmod 0755 /system/etc/init.d/99SuperSUDaemon
chmod 0644 /system/app/SuperSu.apk
chmod 0644 /system/etc/.installed_su_daemon

 

What does all this stuff do?

Well it remounts the system partition so you can write to it.

After that it creates two folders and copies all the files needed into the right folders.

The su binary will be copied 3 times. One as execution file, one to run as a daemon, and one as some sort of backup inside the bin folder if the app won´t search for it in the xbin folder.

The two script files are only needed to execute the SuperSu daemon from the su binary.

And in the end the permissions are set, so the scripts and files are accessible in Android.

 

Now you need to restart the board. You can just type the "reboot" command to do this.

 

When Android starts again, open the terminal emulator from the apps.

Then just type the command "su" and press enter.

 

You should get a SuperSu question to grant the terminal app access to root.

Tap on Grant and there you go.

You are root inside Android.

 

image

Attachments:
RIoTBoard_root.zip
  • Sign in to reply

Top Comments

  • radiatortwo
    radiatortwo over 12 years ago in reply to toonamo +2
    Make sure you remounted the system partition with write permissions before changing the permissions of the files. mount -w -o remount /dev/block/mmcblk0p5 /system The permissions should look like this…
  • mrpipes3
    mrpipes3 over 8 years ago

    I keep getting mount operation not permitted.  Do I need to log in as root somehow?  Very new!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mrpipes3
    mrpipes3 over 8 years ago in reply to radiatortwo

    Can you use GooglePlay with the image provided by Element14? admin@

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • radiatortwo
    radiatortwo over 11 years ago in reply to sjcchuma

    There should be 2 drivers. One for the device and one for the ADB Interface.
    If you have no ADB Interface try to install it manually.

     

    The problem here is that the drivers for the device and the interface can replace each other without errors.
    But won´t work correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sjcchuma
    sjcchuma over 11 years ago in reply to radiatortwo

    I follow the exact steps describe above, yes enable USB debugging mode in Developer. As for driver, it detected as Google Nexus 7. Should I use "Android composite ADB Interface" instead? I will try when I get home.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • radiatortwo
    radiatortwo over 11 years ago in reply to sjcchuma

    You have to activate the debugging in Android.
    Go to settings then device Info and tap on the Build Number entry until it says, that you´re now a developer.
    Then go back and into developer options and activate USB Debugging.

     

    Also make sure the adb driver for the android device is installed correctly.

     

    Then you have to allow the debugging on the device when you execute adb devices and it will show up in the list.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>