RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Python IDLE and terminal...
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 26 subscribers
  • Views 1493 views
  • Users 0 members are here
Related

Python IDLE and terminal...

mubase
mubase over 12 years ago

Hi again.

OK. I'm getting to grips with Riotboard & Ubuntu. Still haven't solved the HDMI to VGA problem but I'm going to try a powered converter box.

I want to run IDLE but when I do I get an error about the DISPLAY environment variable..

I have heard about being able to run programs using X11 and tunneling with SSH on a host computer.. Does anyone know if this could be done with RIoTboard?? If they have or know if it's possible .......

Cheers. image

Steve.

  • Sign in to reply
  • Cancel

Top Replies

  • radiatortwo
    radiatortwo over 12 years ago in reply to mubase +1
    Putty is a client that connects over the SSH protocol to the unix systems console. It´s like a remote access to the terminal. So yes the username and password you are asked for are those from the Riotboard…
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    the 3.0.35 based distro from from e14 had a password "linaro".
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    the 3.0.35 based distro  from from e14 had a password "linaro".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mubase
    mubase over 12 years ago in reply to e14 Contributor

    Found a very nice beginners example of what can be done with Riotboard, Python & GPIOs here...

    its all in Chinese and I wish I understood Chinese but the first program sets up a module to access the USER_LED and a second program controls the LED state  on a screen button press. image

    RioTboard-体验RioTBoard记录W3-使用Python对LED编程-爱板网论坛 - 手机版 - 电子工程师学习交流园地

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to mubase

    Steve if you work at it you can set up an X display and forwarding in Putty and then you'll get all the Xwindows goodness as well form the comfort of your laptop.. Checkout Cygwin like Selsinork stated earlier on the thread the system is great for this and other Windows to 'Nix stuff such as RPI BBB etc

     

     

    Good luck ..Be nice to see a review of the board ...Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Problemchild
    Problemchild over 12 years ago in reply to mubase

    Steve if you work at it you can set up an X display and forwarding in Putty and then you'll get all the Xwindows goodness as well form the comfort of your laptop.. Checkout Cygwin like Selsinork stated earlier on the thread the system is great for this and other Windows to 'Nix stuff such as RPI BBB etc

     

     

    Good luck ..Be nice to see a review of the board ...Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mubase
    mubase over 12 years ago in reply to Problemchild

    Hi John Thanks for the info. . I've got Xwindows working. Its fantastic! A board running in tandem with my laptop and I have run some of the example X11 applications like the roving eyes an XMore but the most important for me at the moment is the IDLE python editor which I can now run. imageimage

    The link to the site mentioned above gives an example of what can be done with the Python TKinter library and the Riotboard LEDs.

    I've got it running.

    I've included a screenshot of the putty window & the X11 TKinter control panel 

    Now I can use python with the IDLE editor I've got some serious learning to do.

    I want to find out about programming the RIoTboard audio in Python. image

     

    I'd love to do a review but note: I not a seasoned pro in the embedded game. This is my first single board computer. I've had plenty experience with Arduino and AVR and some STM32 programming, all in C/C++. I was considering getting an R-PI but then I saw Riotboard...image

    I'll do a bit more learning and then submit a review .

    Cheerio 4 now.

    Steve.