RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum 1280x720 on RIOTboard!!!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 25 subscribers
  • Views 1105 views
  • Users 0 members are here
Related

1280x720 on RIOTboard!!!

e14 Contributor
e14 Contributor over 12 years ago

So the Android package gives humongous black bars on my Sony Bravia LCD.  I try to flash to ubuntu...  Turns outIt gives 1280x720 and nothing else.  (And it has no black bars.)  That's because I have a scorching case of the 1280x720 blues, again!  My Raspberry Pi NEVER gave me this problem.  Ever.

  • Sign in to reply
  • Cancel
Parents
  • radiatortwo
    radiatortwo over 12 years ago

    The resolution is set in the boot variables of u-boot.

    Heres a thread with that: Screen Resolution with preinstalled Android

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    I've also seen anecdotal tales that leaving the video= piece out altogether, or removing the resolution might allow it to use EDID, however it seems rather variable as there are some boards using i.MX6 where EDID doesn't work properly or hasn't been connected... So forcing the resolution on the commandline has become the norm.

     

    letting the system use EDID seems to be much more workable with 3.15 kernel, but that doesn't help for android...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    I've also seen anecdotal tales that leaving the video= piece out altogether, or removing the resolution might allow it to use EDID, however it seems rather variable as there are some boards using i.MX6 where EDID doesn't work properly or hasn't been connected... So forcing the resolution on the commandline has become the norm.

     

    letting the system use EDID seems to be much more workable with 3.15 kernel, but that doesn't help for android...