RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum LCD8000-97C on RIoT ?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 24 subscribers
  • Views 1026 views
  • Users 0 members are here
Related

LCD8000-97C on RIoT ?

e14 Contributor
e14 Contributor over 12 years ago

bluescreen do you know if the LCD8000-97CLCD8000-97C that's supposed to work with sabre-lite / MarS will work with the RIoT board as well ?  Only a guess, but the RIoT appears to be somewhat based on the MarS and have the same LVDS connector, so it could be possible ?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1 verified
    selsinork, Yes, the LCD8000-97C should work with the RIoT board. However, the default boot mode does not use the LVDS interface. In order to enable the LVDS interface used with the LCD8000-97C you will…
  • bluescreen
    0 bluescreen over 12 years ago

    Hi selsinork.

     

    Let me find out for you.


    Sagar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    selsinork,

     

    Yes, the LCD8000-97C should work with the RIoT board.  However, the default boot mode does not use the LVDS interface.  In order to enable the LVDS interface used with the LCD8000-97C you will need to use the modify the uboot boot args.  Additionally the cable is slightly different that used on the MarS board.  There is a nice clean mini HMDI connector on both ends.

     

    The boot args should be set as follows:

    U-Boot >> setenv bootargs console=ttymxc1,115200 init=/init nosmp video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off vmalloc=400M androidboot.console=ttymxc1 androidboot.hardware=freescale

    U-Boot >> saveenv

     

    To access U-Boot you will need console access to the board at boot.  On a prototype version of the board I was able to use the debug serial port with an RS232 adapter.  I've have done this yet on the official release version.  The debug connector (J18, next to the OTG USB port) is a slightly different pinout.

     

    I will try to dig into the details a bit more and provide instructions for accessing the u-boot prompt.

     

    -Clark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vandana
    0 vandana over 12 years ago

    You can use the UART8000-U a USB - serial (TTL) cable for debugging.

     

    It will be available on Newark, Farnell and element14 very soon!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to vandana

    I can confirm that the LCD8000 LVDS display works on the Riot, both Ubuntu and Andriod