RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum LCD8000-97C on RIoT ?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 24 subscribers
  • Views 1029 views
  • Users 0 members are here
Related

LCD8000-97C on RIoT ?

e14 Contributor
e14 Contributor over 12 years ago

bluescreen do you know if the LCD8000-97CLCD8000-97C that's supposed to work with sabre-lite / MarS will work with the RIoT board as well ?  Only a guess, but the RIoT appears to be somewhat based on the MarS and have the same LVDS connector, so it could be possible ?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1 verified
    selsinork, Yes, the LCD8000-97C should work with the RIoT board. However, the default boot mode does not use the LVDS interface. In order to enable the LVDS interface used with the LCD8000-97C you will…
Parents
  • vandana
    0 vandana over 12 years ago

    You can use the UART8000-U a USB - serial (TTL) cable for debugging.

     

    It will be available on Newark, Farnell and element14 very soon!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vandana
    0 vandana over 12 years ago

    You can use the UART8000-U a USB - serial (TTL) cable for debugging.

     

    It will be available on Newark, Farnell and element14 very soon!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to vandana

    I can confirm that the LCD8000 LVDS display works on the Riot, both Ubuntu and Andriod