RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum riotboard camera module
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 25 subscribers
  • Views 3171 views
  • Users 0 members are here
Related

riotboard camera module

e14 Contributor
e14 Contributor over 12 years ago

I would like to connect a CMOS camera module to the Riotboards MIPI camera interface.

Which cameras are avilable for the Riotboard? Can someone advice me a specific camera?

 

Cheers

  • Sign in to reply
  • Cancel
Parents
  • tusharp
    0 tusharp over 12 years ago

    The "e-CAM50IMX6" camera has Mipi/CSI-2 interface which is supported by riotboard hardware (J8).

    Have a look at "DM-CAM130" and "CAM8100-UCAM8100-U" from element14/Embest.

    The drivers supporting riotboard will be available in few weeks.

     

    Are you looking at any specific application to use this camera with?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tusharp

    Hey i´m new on all this board development and i was looking for a camera module so i take a look to the one you suggested, the e-CAM50IMX6, and just happens that i´m confused about the MIPI CSI-2 interface. The e-CAM50IMX6 supposedly is configured to provide MIPI-CSI-2 interface only, it has a 24 pin FFC connector that goes to another interface card for the sabre lite board which has dual row 30 pin connector .

     

    So like you say if it has MIPI CSI-2 interface it should fit on riots mipi cam interface. But

    my confusion is that roit´s mipi csi-2 interface has single row 20 pin connector. As far as i know the CSI-2 is a protocol but the connectors just don´t match.

    Do you know how can i plugged in to the riot board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to e14 Contributor

    but the connectors just don´t match

    The connectors are definitely a challenge.

     

    In the meantime have a look at "DM-CAM130" and  CAM8100-UCAM8100-U , specifically CAM8100-U.

    These modules will be supported on Riotboard .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to tusharp

    Is that DM-CAM130 the same as STM32F4DIS-CAM - STMICROELECTRONICS - MODULE, STM32F4, 1.3MP CAMERA | Farnell UK

     

    Any thoughts on higher resolution cameras?  Something comparable to the RPi camera would be nice...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to e14 Contributor

    Yes, the DM-CAM130  is based on "STM32F4".

    The hardware has 1280*1024 resolution.

     

    Currently only the above cams are going to be supported.

    High res cam may will come down the line sometime in future.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • McuOnEclipse
    0 McuOnEclipse over 12 years ago in reply to tusharp

    Hello,

    I have ordered the CAM8100-U module, and I can confirm that the module is automatically detected and supported by the RIoT board. However, the images/pictures from this module are having a lot of artifacts and are of bad quality (see attached).

    Anyone else using that camera mdule with the RIoT board?

     

    Erichimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to McuOnEclipse

    I have taken pics  in daylight as well as evening, never saw anything like this .

    some improper  post processing is causing this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to tusharp

    android has some good post processing stuff.

    let me know if you are using any specific apks with camera or specific scenarios which causes this, so that  i can emulate  the same here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tusharp
    0 tusharp over 12 years ago in reply to tusharp

    android has some good post processing stuff.

    let me know if you are using any specific apks with camera or specific scenarios which causes this, so that  i can emulate  the same here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • McuOnEclipse
    0 McuOnEclipse over 12 years ago in reply to tusharp

    I have used the default RIoT board Android Image/apks, and have not made any modifications.

    More pictures and details in

    http://mcuoneclipse.com/2014/08/16/review-of-the-cam8100-u-usb-camera-module-with-the-riot-board/

    I was first thinking that the connector might cause problems. Checked everything carefully, and this did not improve anything.

     

    Erich

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to McuOnEclipse

    I was first thinking that the connector might cause problems

       doesn't seem like a connector problem.

     

      shared this issue with android team. will update once fixed.