RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Problem in installing eMMC with Linux from Windows 7 64bit
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 25 subscribers
  • Views 1584 views
  • Users 0 members are here
  • riotboard
  • linux
Related

Problem in installing eMMC with Linux from Windows 7 64bit

bose
bose over 12 years ago

Hello,

 

I have just received my RIoT board and wish to change the existing Android OS to Ubuntu.

I downloaded updater tool for Linux Image: http://downloads.element14.com/linux/Linux.zip?ICID=knode-riotboard-quick&COM=RIoTboard

 

However the updater tool would not start up.

The OS on my laptop is Windows 7 64bit.

 

Here are the steps I followed:

1. Set the boot jumpers to Serial Download as stated in the RIoT board User Manual

2. Extract the Linux.zip to a folder

3. Copy the files from 'image_SVN2487' directory to 'tools\Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\files' directory.

4. Power up the board using 5V DC jack with 3A power adapter

5. Connect the USB-OTG cable to PC and it recognised as USB HID Input device

6. Run the Updater MfgTool2.exe - However this fails with the below Error

image

I have tried using Admin Mode but does not work and shows the same error.

 

I wish to know if any one has faced this problem or has a solution for this.

Kindly point out if there are any mistakes in my configuration steps.

 

Warm Regards,

Abhijit

  • Sign in to reply
  • Cancel
Parents
  • bose
    0 bose over 12 years ago

    Hi,

     

    Thanks to you guys,

     

    Ubuntu installation is working on the RIoT board now.

     

    There are two additional learning that I would like to share.

    1. Putty Based terminal connected to the Serial Debug all times helps to check the progress and booting of the boards. From: Impressions on the RIoTboard and changing its Operating System in Windows

    2. While changing the boot configuration switch the board must be turned off.

     

    Thanks again for your help.

     

    Warm Regards,

    Abhijit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bose
    0 bose over 12 years ago

    Hi,

     

    Thanks to you guys,

     

    Ubuntu installation is working on the RIoT board now.

     

    There are two additional learning that I would like to share.

    1. Putty Based terminal connected to the Serial Debug all times helps to check the progress and booting of the boards. From: Impressions on the RIoTboard and changing its Operating System in Windows

    2. While changing the boot configuration switch the board must be turned off.

     

    Thanks again for your help.

     

    Warm Regards,

    Abhijit