RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum spdif audio programming
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 24 subscribers
  • Views 667 views
  • Users 0 members are here
Related

spdif audio programming

kylemills
kylemills over 12 years ago

i was able to setup the riotboard on Linux after some attempts.

i discovered there is a spdif interface, i want to do some sound programming.

i am new to embedded but have worked on linux, so any pointers will be good.

 

regards

kyle

  • Sign in to reply
  • Cancel

Top Replies

  • tusharp
    tusharp over 12 years ago in reply to kylemills +1 verified
    there is freescale document AN3663 on sgtl5000. its a high performance low power codec and highly supported by freescale .
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    While the i.MX6 is capable of SPDIF, unfortunately it's not been usefully wired up on the RIoTboard. Without sensible access to the hardware side of the SPDIF, there really isn't a lot you can do with it.

     

    The only obviously accessible SPDIF signals would be:

     

    SPDIF_IN on KEY_COL3, but that's already used by HDMI

     

    SPDIF_IN on EIM_D21

    SPDIF_OUT on EIM_D22

    both of which are used for USB OTG power and would probably require removal of U20.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    While the i.MX6 is capable of SPDIF, unfortunately it's not been usefully wired up on the RIoTboard. Without sensible access to the hardware side of the SPDIF, there really isn't a lot you can do with it.

     

    The only obviously accessible SPDIF signals would be:

     

    SPDIF_IN on KEY_COL3, but that's already used by HDMI

     

    SPDIF_IN on EIM_D21

    SPDIF_OUT on EIM_D22

    both of which are used for USB OTG power and would probably require removal of U20.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • kylemills
    0 kylemills over 12 years ago in reply to e14 Contributor

    If SPDIF doesn't work, any other interface i can use image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 12 years ago in reply to kylemills

    there is freescale document AN3663 on sgtl5000.

    its a high performance low power codec and highly supported by freescale .

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer