RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Linux freezes when connected to HDMI
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 1 answer
  • Subscribers 25 subscribers
  • Views 5417 views
  • Users 0 members are here
  • hdmi
  • riotboard
Related

Linux freezes when connected to HDMI

e14 Contributor
e14 Contributor over 12 years ago

I have loaded the Linux image SVN2652 on Riotboard, but it only boots if HDMI is not connected.

If I connect the HDMI after Linux starts running it also freezes.

The kernel is: Linux version 3.10.17_1.0.0_RIoTboard+g9ba99b4 (luofc@embest-tech) (gcc version 4.8.1 (GCC) ) #1 SMP PREEMPT Thu Jun 19 09:46:07 CST 2014.

I have tried it on two other boards with the same result. If I stop the boot it displays the Freescale logo, so the hardware seems to work.

Could it be a driver problem?

Is there a fix for this?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • tusharp
    0 tusharp over 12 years ago

    hi cristian,

     

    I guess you have downloaded from here : https://www.dropbox.com/sh/nuhzba8uqpijenb/AAAt8l9g6u6T6-DOqJHozyKca/fsl-image-fb-riotboard.sdcard?dl=1

     

    If I connect the HDMI after Linux starts running it also freezes.

    The HDMI screen freezes or Riotboard booting ??

     

    it only boots if HDMI is not connected.

    The HDMI GUI support is not yet enabled in kernel.

    on display devices it will show a terminal with Yocto signature as shown below.

     

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to tusharp

    Hello Tushar

     

    Greetings

     

    From your post I understand that the kernel does not have HDMI support enabled. Could you confirm if BSP Linux Yocto v3.10.17 available at RIoTboard BSP Images and Tools Download - Android and Linux has the same issue too. The booting freezes at "starting kernel" when the HDMI cable is connected.

     

    Regards

    Karthik

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tusharp
    0 tusharp over 11 years ago in reply to e14 Contributor

    The BSP in Download center is SVN2652(deprecated), it has no GUI support, (hdmi is a later thing).

    This BSP (tutorial) is SVN3000 &  has GUI support for HDMI & LVDS .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tusharp
    0 tusharp over 11 years ago in reply to e14 Contributor

    The BSP in Download center is SVN2652(deprecated), it has no GUI support, (hdmi is a later thing).

    This BSP (tutorial) is SVN3000 &  has GUI support for HDMI & LVDS .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to tusharp

    Hey.

     

    I have the same problem as stated above.

    Riotboard, Yocto Image from E14 homepage, Linux 3.10.17 yocto BSP  image_SVN2652.zip

     

     

    uart tells me:

     

    -----------

    CPU: Freescale i.MX6SOLO rev1.1 at 792 MHz
    CPU: Temperature 43 C, calibration data: 0x5845075f
    Reset cause: POR
    Board: MX6SOLO RIoTboard
    I2C: ready
    DRAM: 1 GiB
    MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
    No panel detected: default to HDMI
    Display: HDMI (640x480)
    In: serial
    Out: serial
    Err: serial
    mmc2(part 0) is current device
    Net: FEC [PRIME]
    Warning: failed to set MAC address

     

    Normal Boot
    Hit any key to stop autoboot: 0
    mmc2(part 0) is current device
    reading boot.scr
    ** Unable to read file boot.scr **
    reading uImage
    5275824 bytes read in 275 ms (18.3 MiB/s)
    Booting from mmc ...
    reading imx6solo_RIoTboard.dtb
    43553 bytes read in 21 ms (2 MiB/s)
    ## Booting kernel from Legacy Image at 12000000 ...
    Image Name: Linux-3.10.17_1.0.0_RIoTboard+g9
    Image Type: ARM Linux Kernel Image (uncompressed)
    Data Size: 5275760 Bytes = 5 MiB
    Load Address: 10008000
    Entry Point: 10008000
    Verifying Checksum ... OK
    ## Flattened Device Tree blob at 18000000
    Booting using the fdt blob at 0x18000000
    Loading Kernel Image ... OK
    OK
    Using Device Tree in place at 18000000, end 1800da20

     

    Starting kernel ...

     

    Booting Linux on physical CPU 0x0
    Linux version 3.10.17_1.0.0_RIoTboard+g9ba99b4 (luofc@embest-tech) (gcc version 4.8.1 (GCC) ) #1 SMP PREEMPT Thu Jun 19 09:46:07 CST 2014

    ...

    ...

    Starting Linux NFC daemon
    Starting OProfileUI server
    Running local boot scripts (/etc/rc.local).
    Stopping Bootlog daemon: bootlogd.

     

    Poky (Yocto Project Reference Distro) 1.5.1 riotboard /dev/ttymxc1

     

    riotboard login: root
    root@riotboard:~#

     

    -------------------

     

    Board boots without any errors into riotboard User root.

    As soon as HDMI is connected Linux hangs up...

     

    When I stop by in uBoot and  stop by the HDMI Monitor has the chance to display a standard freescale bootscreen (freescale Logo and script plus Some uBoot Info: U.Boot 2013.04-04988-gd2e8066-dirty (Jul 04 2014 - 09:18:53)

     

     

    Continuing to boot fails at

     

    Starting kernel...

     

    It's funny that although connected the Riotboard tells me the no HDMI display is connected.

     

    the Riotboard sends some messages when connecting USB pheripherals as well as HDMI Monitor (EDID related and that sort of thing....) But this messages I cannot reproduce at the moment....

     

    Any solution known to why Yocto won't start?

    I had   trouble with HDMI since the start which makes me believe the board may be broken.

    Under Ubunto and Android I wasn't able to setup anything larger than 640x480, which is the default resolution on HDMI but at least I had graphichs displayed in these two systems.

     

    Christian

     

     

    PS/EDIT: I used MFG tool to flash from Windows as my PC at work doesn't support Linux yet (legal thingy). I cannot flash SVN3000 (yet) from windows