Freescale i.MX6 Development Platforms
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • Freescale i.MX6 Development Platforms
  • More
  • Cancel
Freescale i.MX6 Development Platforms
Forum Yocto and IMX 6 Element14 devlopment kit
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freescale i.MX6 Development Platforms to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 5 subscribers
  • Views 1884 views
  • Users 0 members are here
  • i.mx6quad
  • yocto
  • i.mx6
  • sabre_lite
Related

Yocto and IMX 6 Element14 devlopment kit

e14 Contributor
e14 Contributor over 13 years ago

Good morning,

 

     I just received my IMX 6 Element 14 devlopment Kit and I try to put some free linux on it. My goal is to use the 2D and 3D graphical card's acceleration. So I try first to build the sabre_lite yocto image as in the thread ( https://community.freescale.com/docs/DOC-93844 ). Well it build well on a Fedora 16. And with the original q_bootscripts of the timesys image it start booting on my kit. I have to change the partition of the SD Card but it works. So I was then very glad, evrything was smooth and work well. But ... Then I try to plug a keyboard on the kit, and I ve got some error ( kernel panic ) during the boot and the boot stop, perhaps udev can't handle the keyboard during the boot ?  I've try to get the network working but the kernel stop too.

If plug after the boot the keyboard works well and there's no kernel panics. So it's just during the initial boot.

 

So are there people who succeded to boot the yocto image with this element14 kit ? Or the prefered free are just lbit and linearo ?

 

My next step will probably be to update the u-boot and to try the lbit / linearo image.

But it will be very helpfull to know if there was some people which succeded with yocto( and how they have done it ). Yocto seem's to be the freescale prefered linux distribution, and well it's seem very cool.

 

Thanks,

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello,

     

         I used the dylan branch, and it works ( stable, cool, and so on ... ). The danny branch do not work.

     

              Sincerely,

     

     

     

    To get the BSP you need to have `repo` installed and use it as:

     

    Install the `repo` utility:

     

    $: mkdir ~/bin

    $: curl https://dl-ssl.google.com/dl/googlesource/git-repo/repo > ~/bin/repo

    $: chmod a+x ~/bin/repo

     

    Download the BSP source:

     

    $: PATH=${PATH}:~/bin

    $: mkdir fsl-community-bsp

    $: cd fsl-community-bsp

    $: repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b dylan

    $: repo sync

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    . The danny branch do not work.

     

    imageimageimage

     

    Thank you katre and Yves

     

    Compiling dylan ....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    . The danny branch do not work.

     

    imageimageimage

     

    Thank you katre and Yves

     

    Compiling dylan ....