Freescale i.MX6 Development Platforms
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • Freescale i.MX6 Development Platforms
  • More
  • Cancel
Freescale i.MX6 Development Platforms
Forum Uses of the SABRE Light i.MX6 Platform Development Kit?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freescale i.MX6 Development Platforms to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 4 subscribers
  • Views 575 views
  • Users 0 members are here
  • freescale
  • imx6
  • single_board_computer
  • development_kit
  • sabre_lite
Related

Uses of the SABRE Light i.MX6 Platform Development Kit?

Anonymous-167986
Anonymous-167986 over 13 years ago

This probably sounds like a very noobish question (mainly because I am a noob), but are there any uses of the SABRE Light i.MX6 Platform Development Kit other than pretty much just using it as a mini computer?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I'd say you're spot on.  You do use it as a tiny computer.   Take that in context though, use it in places where you don't have the space, power, cooling needed for a full size computer.  Or where you need the sort of IO capabilities that a full sized PC rarely provides

     

    There's an 'automotive' version on the chip (and that's what's on my Sabre-Lite) so you can see this sort of thing appearing in cars, perhaps running the dashboard display, or the headrest movie players for the kids in the back. Whether you'd use a SL for that or a custom designed board with the iMX6 SoC is a different matter.

     

    The SL is as it's full title sugests a platform development kit the idea being to use it to prototype and prove an application before going to the expense of designing that custom board.

     

    So you can use the SL for almost all of the things you can do with a big PC, but also for lots of things that you can't.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer