Freescale i.MX6 Development Platforms
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • Freescale i.MX6 Development Platforms
  • More
  • Cancel
Freescale i.MX6 Development Platforms
Documents Freescale i.MX 6 Development Platforms Software Download Center
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freescale i.MX6 Development Platforms to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: atomar
  • Date Created: 5 Dec 2013 6:43 AM Date Created
  • Last Updated Last Updated: 20 Aug 2014 5:37 PM
  • Views 6814 views
  • Likes 1 like
  • Comments 20 comments
Related
Recommended

Freescale i.MX 6 Development Platforms Software Download Center

image

Software Download


RIoTboard, SABRE Lite & MarS board are evaluation platforms featuring the powerful i.MX 6 Quad-Core, Dual-Core and Solo multimedia application processors from Freescale Semiconductor. These evaluation platforms are provided with Linux and Android system images and source code.

 

 

You can download all the latest Linux & Android system images and the source code for all three I.MX 6 boards from here. All the listed images support the LCD8000-97C module, a portable 9.7” LVDS display module designed for I.MX 6 boards.


RIoTboard (with LCD8000-97C support)

Linux Image


image

Android Image

image

Android Tools

 


image
SABRE Lite (with LCD8000-97C support)

Linux Image


image

Linux Source Code

image

Linux Tools

image

Android Image

image

Android Source Code

image

Android Tools

 


image
Mars Board (with LCD8000-97C support)

Linux Image

image

Linux Source Code

image

Android Image

image

Android Source Code

image

Micrium Demo Image

image

Tool - MFG Tool

image
Tool - USB Driver
image
Tool - USB Serial Driverimage

http://www.pinterest.com/pin/create/extension/

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    The above download links are not working! Can you please fix this!
  • shivangi
    shivangi over 4 years ago

    Hello all,

    Above Linux Image downloading links are not working.

    Kindly fix it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wangyunpeng1992
    wangyunpeng1992 over 9 years ago

    how to chang the default value of uboot

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • imrank340@gmail.com
    imrank340@gmail.com over 10 years ago

    Hi Forum members,

     

    I recently got a MarSBoard iMX6 Dual core board I am trying to set the board as following:

     

    1/ Try to boot from SD setting Boot Mode SW 1= OFF and SW2=ON

    2/ On SD  micro card; using MAINLINE DENX u-boot compiled, created u-boot.img  and rest of the files

    3/ On SD from MAINLINE kernel.scm.git repository downloaded kernel and built uImag and zImage

    4/ Try to boot iMX6 board from the SD but NO avail board seems to be not booting from the SD.

     

    5/ I have two partitions on my micro SD card

           1) BOOT with W95 32 bit

           2) rootfs  with 83 Linux Ext4 partition.

     

    I wonder someone can guild or put me in the right direction to get this board up and running?

    Thank you,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hello engineers:

             The OpenCL 1.1 and OpenGL 2.0 will be used for image-processing (such as sobel,

     

     

    canny, gaussion-filter ) on SabreLite board.

    According to the description in the 13.1.1.6 Menu Configuration Options in the paper

     

     

    (i.MX 6 Linux Reference Manual)(document number: IMX6LXRM ,Version:Rev

     

     

    L3.10.53_1.1.0-ga, 01/2015), I can't find the configuration about GPU driver.

         Could you tell me how to configure relative GPU-related options in the timeSys's

     

     

    BSP and SabreLite.

         Best Wishes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    I tried booting the sabre_lite board Linux image and it gets booted and the image loads but finally the following comes. Could somebody tell what’s wrong with the same or how should I fix it?

     

    VFS: Cannot open root device "(null)" or unknown-block(0,0)

    Please append a correct "root=" boot option; here are the available partitions:

    1f00            1024 mtdblock0  (driver?)

    1f01            1024 mtdblock1  (driver?)

    b300         3872256 mmcblk0  driver: mmcblk

      b301         3868160 mmcblk0p1 00000000-0000-0000-0000-000000000000

    Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

    [<8004a828>] (unwind_backtrace+0x0/0xf8) from [<8050b41c>] (panic+0x74/0x18c)

    [<8050b41c>] (panic+0x74/0x18c) from [<80008ce8>] (mount_block_root+0x170/0x224)

    [<80008ce8>] (mount_block_root+0x170/0x224) from [<80008e84>] (mount_root+0xe8/0x108)

    [<80008e84>] (mount_root+0xe8/0x108) from [<80008fc4>] (prepare_namespace+0x120/0x178)

    [<80008fc4>] (prepare_namespace+0x120/0x178) from [<800089b0>] (kernel_init+0x108/0x13c)

    [<800089b0>] (kernel_init+0x108/0x13c) from [<80044a24>] (kernel_thread_exit+0x0/0x8)

    CPU0: stopping

    [<8004a828>] (unwind_backtrace+0x0/0xf8) from [<8003e324>] (do_IPI+0x150/0x17c)

    [<8003e324>] (do_IPI+0x150/0x17c) from [<8004398c>] (__irq_svc+0x4c/0xe8)

    Exception stack(0x80a91f68 to 0x80a91fb0)

    1f60:                   80afe100 20000093 00000001 00000000 80a90000 80af6ca4

    1f80: 80513810 80aa4e7c 1000406a 412fc09a 00000000 00000000 00000000 80a91fb0

    1fa0: 800525a8 80044a84 40000013 ffffffff

    [<8004398c>] (__irq_svc+0x4c/0xe8) from [<80044a84>] (default_idle+0x24/0x28)

    [<80044a84>] (default_idle+0x24/0x28) from [<80044c7c>] (cpu_idle+0xbc/0xfc)

    [<80044c7c>] (cpu_idle+0xbc/0xfc) from [<80008868>] (start_kernel+0x248/0x288)

    [<80008868>] (start_kernel+0x248/0x288) from [<10008040>] (0x10008040)

    CPU1: stopping

    [<8004a828>] (unwind_backtrace+0x0/0xf8) from [<8003e324>] (do_IPI+0x150/0x17c)

    [<8003e324>] (do_IPI+0x150/0x17c) from [<8004398c>] (__irq_svc+0x4c/0xe8)

    Exception stack(0xbffadf90 to 0xbffadfd8)

    df80:                                     80afe100 60000193 00000001 00000000

    timer 3: cpufreq_frequency_table_target error

    dfa0: bffac000 80af6ca4 80513810 80aa4e7c 1000406a 412fc09a 00000000 00000000

    dfc0: 00000000 bffadfd8 800525a8 80044a84 40000113 ffffffff

    [<8004398c>] (__irq_svc+0x4c/0xe8) from [<80044a84>] (default_idle+0x24/0x28)

    [<80044a84>] (default_idle+0x24/0x28) from [<80044c7c>] (cpu_idle+0xbc/0xfc)

    [<80044c7c>] (cpu_idle+0xbc/0xfc) from [<10508254>] (0x10508254)

    CPU3: stopping

    [<8004a828>] (unwind_backtrace+0x0/0xf8) from [<8003e324>] (do_IPI+0x150/0x17c)

    [<8003e324>] (do_IPI+0x150/0x17c) from [<8004398c>] (__irq_svc+0x4c/0xe8)

    Exception stack(0xbff01f90 to 0xbff01fd8)

    1f80:                                     80afe100 60000093 00000001 00000000

    1fa0: bff00000 80af6ca4 80513810 80aa4e7c 1000406a 412fc09a 00000000 00000000

    1fc0: 00000000 bff01fd8 800525a8 80044a84 40000013 ffffffff

    [<8004398c>] (__irq_svc+0x4c/0xe8) from [<80044a84>] (default_idle+0x24/0x28)

    [<80044a84>] (default_idle+0x24/0x28) from [<80044c7c>] (cpu_idle+0xbc/0xfc)

    [<80044c7c>] (cpu_idle+0xbc/0xfc) from [<10508254>] (0x10508254)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to atomar

    Hello. Where i can find correct Android Image?

    Now Android image size 8.7 mb, I think this impossible - correct android image with size less 10 mb...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Patch for LCD8000-97C for sabre light is broken:

     

    Binary files linux-3.0.old/drivers/input/touchscreen/generic_ts_rel/lib/chip.x and linux-3.0.new/drivers/input/touchscreen/generic_ts_rel/lib/chip.x differ

    Binary files linux-3.0.old/drivers/input/touchscreen/generic_ts_rel/lib/ct360.x and linux-3.0.new/drivers/input/touchscreen/generic_ts_rel/lib/ct360.x differ

    Binary files linux-3.0.old/drivers/input/touchscreen/generic_ts_rel/lib/ct365.x and linux-3.0.new/drivers/input/touchscreen/generic_ts_rel/lib/ct365.x differ

    Binary files linux-3.0.old/drivers/input/touchscreen/generic_ts_rel/lib/enhance.x and linux-3.0.new/drivers/input/touchscreen/generic_ts_rel/lib/enhance.x differ

     

    Does anybody have such files to build the kernel with touchscreen support?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • simon@weltrend.com.tw
    simon@weltrend.com.tw over 12 years ago in reply to atomar

    Hi,

    The link of SABRE lite Android Image & Android tools, It seems not fix yet..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • simon@weltrend.com.tw
    simon@weltrend.com.tw over 12 years ago

    Hi,

    The above download link of Android image & Android Tools (SABRE Lite) ,It's seems some problem of file size , It's only 8.7MB of image_SVM2236.zip.

    I using the MfgTool : (mfgtools-rel-12.04.01_er_mx6q_updater) on tools_SVN2236 floder, It also can not download image to Sabere lite board.

    Can fix the download link of SABRE lite !!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • atomar
    atomar over 12 years ago in reply to e14 Contributor

    Hi Stefan,

     

    Download links has been fixed. Thanks

     

    Ankur Tomar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>