Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Documents element14 Year in Review 2016: SBC Comparison Chart
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: CharlesGantt
  • Date Created: 21 Dec 2016 9:19 AM Date Created
  • Last Updated Last Updated: 10 Jan 2017 9:51 AM
  • Views 2311 views
  • Likes 11 likes
  • Comments 7 comments
Related
Recommended

element14 Year in Review 2016: SBC Comparison Chart

image

      Top Single Board Computers & µController Boards of 2016

Also read: Product of the Year Awards
                                                                                                 

imageimageimageimage
BoardRaspberry Pi 3 Model BBeagleBone BlackBeaglebone Black WirelessBeaglebone Black Industrial
Feature
CPU / MCUArm Cortex-A53AM335x 1GHz ARM Cortex-A8AM335x 1GHz ARM Cortex-A8AM335x 1GHz ARM Cortex-A8
Quad Core 1.2GHzSingle Core 1GHzSingle Core 1GHzSingle Core 1GHz
RAM1024MB512MB512MB512MB
GPUBroadcom VideoCore IV @ 250 MHz SGX530 Graphics EngineSGX530 Graphics EngineSGX530 Graphics Engine
GPIO Ports40-Pin Populated2x   46-Pin Populated 72 GPIO in total2x   46-Pin Populated 72 GPIO in total2x 46-Pin Populated 72 GPIO in total
USB Ports4x Type A1X USB Client, 1X  USB Host 1X USB Client, 1X  USB Host 1X USB Client, 1X USB Host
EthernetYes 10/100Yes 10/100NoneYes 10/100
WiFiWiFi 802.11b/g/nNoneWiLink   8 WL1835MOD 802.11b/g/nNone
Bluetooth YesNoneYesNone
Internal StorageNone4GB Embedded eMMC Flash4GB Embedded eMMC Flash4GB Embedded eMMC Flash
Expandable   StorageMicro SDHCMicro SDHCMicro SDHCMicro SDHC
CVBS Video4-Pole 3.5mm JackVia Cape Add-on BoardVia Cape Add-on BoardVia Cape Add-on Board
Video InputMIPI Camera InterfaceVia Cape Add-on BoardVia Cape Add-on BoardVia Cape Add-on Board
HDMIYesYesYesYes
Audio OutputVia HDMI and 3.5mm Audio JackVia HDMI and Cape Add-on BoardVia HDMI and Cape Add-on BoardVia HDMI and Cape Add-on Board
Audio InputAudio Input Through I2C interfaceVia Cape Add-on BoardVia Cape Add-on BoardVia Cape Add-on Board
Serial Port YesUART0 access via 6-pin 3.3V TTL HeaderUART0 access via 6-pin 3.3V TTL HeaderUART0 access via 6-pin 3.3V TTL Header
Power Source5V 3A Via Micro-USB Cable5V 2A Via Onboard 5.5mm Barrel Jack5V 2A Via Onboard 5.5mm Barrel Jack5V 2A Via Onboard 5.5mm Barrel Jack
Temperature Range0°C to 70°C0°C to 70°C0°C to 70°C0°C to 70°C
OS CompatibilityRaspbian, AndroidDebian, Android, Ubuntu, Cloude9 IDE, LabviewDebian, Android, Ubuntu, Cloude9 IDE, LabviewDebian, Android, Ubuntu, Cloude9 IDE, Labview
Buy Now Raspberry Pi 3 Model BRaspberry Pi 3 Model B
Beaglebone Black Rev. CBeaglebone Black Rev. C Beaglebone Black WirelessBeaglebone Black Wireless Beaglebone Black IndustrialBeaglebone Black Industrial

                                                                                                       

 

imageimageimageimage
BoardBBC micro:bitCodeBugWaRP 7RIoTboard
Feature
CPU / MCUNordic nRF51822 – 32-bit ARM Cortex-M0Microchip PIC18F25k50i.MX 7Solo applications processor Freescale i.MX 6Solo
NXP/Freescale   KL26Z  48 MHz ARM Cortex-M0+ (Arm   Cortex-A7/Cortex –M4)(ARM Cortex-A9 1GHz)
RAM16k2048   bytes512MB  LPDDR31GB
GPUNoneNoneMali   V500 NEON MPE / OpenGL ES 2.0
GPIO Ports3 + 23-Pin Edge Connector4Requires Expansion board40-Pin Populated
USB Ports1115
EthernetNoneNoneNoneYes 10/100
WiFiNoneNoneMurata LBEE5KL1DX-TEMP-DS-SD 802.11b/g/nNone
BluetoothYesNoneYesNone
Internal Storage256k256k HEF8GB   eMMC 5.0 4GB eMMC
Expandable   StorageNoneNoneNoneMicro SDHC
CVBS VideoNoneNoneMIPI Display Interface
Video InputNoneNoneMIPI Camera InterfaceMIPI Camera Interface
HDMINoneNoneNoneYes
Audio OutputNoneNone3.5mm Audio Jack3.5mm Audio Jack
Audio InputNoneNoneVia 3.5mm Audio   Jack3.5mm Audio Jack
Serial PortVia 23-Pin Edge ConnectorNoneVia unpopulated headersVia GPIO
Power Source5V 1A Via Micro-USB Cable3.3V  / 5V Via USB5V 1A Via USB5V 2A Via 5.5mm Power Jack
Temperature Range0°C to 70°C0°C to 70°C0°C to 70°C0°C to 70°C
OS CompatibilityMicroPython, Blockly, JavaScriptBlockly, Python, JavaScriptBSP: Linux 4.1Linux, Android
Buy Now BBC micro:bitBBC micro:bit CodebugCodebugWaRP 7WaRP 7 RIoT BoardRIoT Board

                                                                                                    

 

imageimageimageimage
BoardIntel Edison IoT ModuleIntel Edison Kit for ArduinoIntel Genuino / Arduino 101Intel Joule 570x Developer Kit
Feature
CPU / MCUIntel Atom 32-BitIntel Atom 32-BitIntel Curie Intel Atom T5700 64-bit
Dual Core 500 MHzDual Core 500 MHz Quad Core 1.7GHz
RAM1GB1GB24k4GB LPDDR4
GPUNoneNoneNoneIntel HD Graphics
GPIO Ports26 Unpopulated26   Populated, Arduino Compatible1480-pin populated
USB PortsNone311
EthernetNoneNoneNoneNone
WiFi802.11 b,g,n802.11 b,g,nNone802.11 b,g,n
BluetoothYesYesYesYes
Internal Storage4GB eMMC4GB eMMC196k16GB eMMC
Expandable   StorageNoneMicro SDNoneNone
CVBS VideoNoneNoneNoneMIPI DSI
Video InputNoneNoneNoneMIPI CSI
HDMINoneNoneNoneYes
Audio OutputNoneNoneNoneVia HDMI
Audio InputNoneNoneNoneNone
Serial PortYesYesYesYes
Power Source3.3V 1A7-15V 2A Via 5.5mm Power Jack5V 500mAh Via 5.5mm Power Jack / USB3.3V 2A
Temperature Range0°C to 40°C0°C to 40°C0°C to 40°C0°C   to 70°C
OS CompatibilityYocto Linux v1.6 / Arduino IDEYocto Linux v1.6 / Arduino IDEArduino IDECustom Linux Kernel / Windows 10 IoT Core
Buy NowIntel Edison IoT ModuleIntel Edison IoT ModuleIntel Edison Kit for ArduinoIntel Edison Kit for ArduinoIntel Genuino / Arduino 101Intel Genuino / Arduino 101Intel Joule 570X Developer KitIntel Joule 570X Developer Kit
  • single board computers
  • intel
  • sbc
  • raspberry pi
  • microcontroller
  • edison
  • beaglebone black wireless
  • year in review
  • BeagleBone Black
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 9 years ago +4
    The voltage of the I/O would be very useful. The Edison has a 1.8v I/O so it means it requires an interface for most operations. Codebug also has provision for an on-board battery. Thanks mark
  • balearicdynamics
    balearicdynamics over 9 years ago +3
    Great chart! Useful for now and in future. I see that the Arduino UNO has not been mentioned... Finally! A first small step ahead Enrico
  • e14 Contributor
    e14 Contributor over 9 years ago +2
    This is a great comparison table, I wonder if it would benefit from having a rating for expected user skill or experience level, giving people an indication what device would be suitable for them.
  • koudelad
    koudelad over 9 years ago in reply to e14 Contributor

    Agree... I also vote for adding some approximate CPU and video performance. I don't mean a specific benchmark score, but a quick relative comparison among the boards, to have an idea what a typical application could or couldn't be.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago

    This is a great comparison table, I wonder if it would benefit from having a rating for expected user skill or experience level, giving people an indication what device would be suitable for them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago

    BBC micro:bit accepts 3V on the battery connector.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • starrider
    starrider over 9 years ago

    There are a lot of "2016 devboards" missing, supposably the ones that you do not sell, that's understandable.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago

    Great chart! Useful for now and in future.

    I see that the Arduino UNO has not been mentioned... Finally! A first small step ahead image

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago

    The voltage of the I/O would be very useful.

    The Edison has a 1.8v I/O so it means it requires an interface for most operations.

     

    Codebug also has provision for an on-board battery.

     

    Thanks

    mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michelmerlin
    michelmerlin over 9 years ago

    Thanks for this table rich with information. However it would be more useful if completed with explanations and comments.

    Meanwhile I thank you all again for your work, and I wish you a happy New Year

    Versailles, Tue 27 Dec 2016 23:57:55 +0100