STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Problem with "official" LCD software example on STM32F4 Discovery Expansion Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 8 subscribers
  • Views 4717 views
  • Users 0 members are here
  • discovery
  • stm32f4-lcd
  • stm32
  • stm32f4dis-bb
  • stm32f4dis_software_examples
  • stm32f4discovery
Related

Problem with "official" LCD software example on STM32F4 Discovery Expansion Board

e14 Contributor
e14 Contributor over 13 years ago

Hi,

 

I've just started to use my STM32F4 discovery expansion board (discovery board, base board, LCD and camera) and as a first shot I want to try out the software examples found here:

 

http://www.element14.com/community/docs/DOC-51670/l/stm32f4dis-bb-discover-more-software-examples

 

I've tried to run the LCD example called "LCD_35T" located in the folder "STM32F4xx_LCD_Example" but ran into some problems...

 

I'm using IAR Embedded Workbench for ARM as my IDE and have performed the following steps:

 

  • Open the project file located in "LCD_35T/EWARM" folder
  • Rebuild all --> Results in a successful build without errors/warnings
  • Download and debug --> Code is flashed and debugger started (using ST-LINK)
  • Running program (Go) --> Expecting LCD to show color bars according to the example but the screen is just white...


Does anyone have an idea what I'm doing wrong?

 

Thanks in advance for all response!

  • Sign in to reply
  • Cancel

Top Replies

  • Kilohercas
    Kilohercas over 13 years ago +1
    do you have LCD with same controller/pinout ? Right code with wrong init ( set registers for refresh rate, color type, bus type and so on) will produce white screen Check if RESET is high. Disable opt…
  • Kilohercas
    Kilohercas over 13 years ago in reply to e14 Contributor +1
    IF LCD reset Line is LOW, you never get LCD working. some one mentioned bad contacts, also make RESET High after power up at if not by default code, than yourself. #define LCD_RST_PIN (GPIO_Pin_3) #define…
  • ChuckMcM
    ChuckMcM over 13 years ago +1
    So I too was having issues with the code provided by Embest so I wrote some of my own. You can pull a copy from Github here: https://github.com/ChuckM/bb-lcd This puts up a simple display on the LCD with…
Parents
  • philip-1992
    0 philip-1992 over 13 years ago

    In addition with this query is it possible to use another type of touch screen instead the one which comes with the STM32F4 Discovery expansion board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • philip-1992
    0 philip-1992 over 13 years ago

    In addition with this query is it possible to use another type of touch screen instead the one which comes with the STM32F4 Discovery expansion board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Kilohercas
    0 Kilohercas over 13 years ago in reply to philip-1992

    I don't know exactly what kind interface is used in this demo-board.

    if SPI, yes, but you will need to develop custom code  it is possible that registers are different in  controller)

    if it's connects to ADC ( reads Resistor divider voltage, like other may use ) it should work,