STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Problem with "official" LCD software example on STM32F4 Discovery Expansion Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 8 subscribers
  • Views 4729 views
  • Users 0 members are here
  • discovery
  • stm32f4-lcd
  • stm32
  • stm32f4dis-bb
  • stm32f4dis_software_examples
  • stm32f4discovery
Related

Problem with "official" LCD software example on STM32F4 Discovery Expansion Board

e14 Contributor
e14 Contributor over 13 years ago

Hi,

 

I've just started to use my STM32F4 discovery expansion board (discovery board, base board, LCD and camera) and as a first shot I want to try out the software examples found here:

 

http://www.element14.com/community/docs/DOC-51670/l/stm32f4dis-bb-discover-more-software-examples

 

I've tried to run the LCD example called "LCD_35T" located in the folder "STM32F4xx_LCD_Example" but ran into some problems...

 

I'm using IAR Embedded Workbench for ARM as my IDE and have performed the following steps:

 

  • Open the project file located in "LCD_35T/EWARM" folder
  • Rebuild all --> Results in a successful build without errors/warnings
  • Download and debug --> Code is flashed and debugger started (using ST-LINK)
  • Running program (Go) --> Expecting LCD to show color bars according to the example but the screen is just white...


Does anyone have an idea what I'm doing wrong?

 

Thanks in advance for all response!

  • Sign in to reply
  • Cancel

Top Replies

  • Kilohercas
    Kilohercas over 13 years ago +1
    do you have LCD with same controller/pinout ? Right code with wrong init ( set registers for refresh rate, color type, bus type and so on) will produce white screen Check if RESET is high. Disable opt…
  • Kilohercas
    Kilohercas over 13 years ago in reply to e14 Contributor +1
    IF LCD reset Line is LOW, you never get LCD working. some one mentioned bad contacts, also make RESET High after power up at if not by default code, than yourself. #define LCD_RST_PIN (GPIO_Pin_3) #define…
  • ChuckMcM
    ChuckMcM over 13 years ago +1
    So I too was having issues with the code provided by Embest so I wrote some of my own. You can pull a copy from Github here: https://github.com/ChuckM/bb-lcd This puts up a simple display on the LCD with…
  • Kilohercas
    0 Kilohercas over 13 years ago

    do you have LCD with same controller/pinout ?
    Right code with wrong init ( set registers for refresh rate, color type, bus type and so on) will produce white screen

    Check if RESET is high.
    Disable optimization

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Kilohercas

    Hi,

     

    First of all, thanks for your reply, Linas!

     

    I have the STM32F4DIS-LCD which I believe is the one considered for this project so i don't think it should be any problems with the controller/pinout.

    I checked that RESET is not high and turned off all optimization but I still have the same behavior from the LCD.

     

    Let me know if you have any additional thoughts to this problem.

     

    Thanks again!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago in reply to e14 Contributor

    IF LCD reset Line is LOW, you never get LCD working. some one mentioned bad contacts, also make RESET High after power up at if not by default code, than yourself.

    #define LCD_RST_PIN                     (GPIO_Pin_3)

    #define LCD_RST_PORT                 (GPIOD)


    (and you can't use that for your one usage, just for lcd )

     

    Set this pin yourself high before init, and delete same code from lcd init, i don't know why it's not High, it must be. , where is no point to look any further if you have lcd in reset at all time.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Kilohercas

    Hi again,

     

    Never mind, I also had bad contact! Reconnected everything after you mentioned that, and now it all works just fine image

     

    Sorry for taking your time with such a silly problem, but I really appreciate your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago

    In addition with this query is it possible to use another type of touch screen instead the one which comes with the STM32F4 Discovery expansion board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago in reply to philip-1992

    I don't know exactly what kind interface is used in this demo-board.

    if SPI, yes, but you will need to develop custom code  it is possible that registers are different in  controller)

    if it's connects to ADC ( reads Resistor divider voltage, like other may use ) it should work,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ChuckMcM
    0 ChuckMcM over 13 years ago

    So I too was having issues with the code provided by Embest so I wrote some of my own. You can pull a copy from Github here:

    https://github.com/ChuckM/bb-lcd This puts up a simple display on the LCD with a running timer (counting up seconds and milliseconds)

    A screenshot of what it looks like when it is running is here: https://github.com/ChuckM/bb-lcd/blob/master/screen-shot.png

     

    I've noticed a couple of things, first that the viewing angle on this display is quite poor, the second is that since the LCD isn't actually memory

    mapped it would be really really hard to get it to update without flickering. If you run the demo it animates moving the RED/GREEN/BLUE/MULTI

    blocks around every 10 seconds.

     

    Also a shout out to the AdaFruit folks for their GFX library, it let me get something up and running quickly where it was more than just draw a

    line or draw a box. Originally the demo drew a clock face and animated the hands but that was really hard to watch with the flickering.

     

    --Chuck

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago in reply to ChuckMcM

    if you want fast updates, you must use write to internal ram function. Idea is simple, you send special commands to define area , and start send raw data. It's like paint bmp function. i can get up to ~400fps with this modification on SSD1963 480*272 lcd.

     

    void LCD_WriteBMP(uint16_t Xpos, uint16_t Ypos, uint16_t Height, uint16_t Width, uint8_t *bitmap)

    {

      u32 index;

      u32 size = Height * Width;

      u16 *bitmap_ptr = (u16 *)bitmap;

      bitmap_ptr+=Height * Width-1;

      LCD_WriteCom(0x0036);

      LCD_WriteRAM(0x0040);

     

      LCD_StartPixelLineAddress(Xpos,Ypos,Xpos+Height-1,Ypos+Width);

      for(index=0;index<(size);index++)

      {

        LCD_RAM = *bitmap_ptr--;

      }

      LCD_WriteCom(0x0036);

      LCD_WriteRAM(0x0000);

    }

     

    Problem is, you need to have frame buffer in sram if you want to refresh all screen.But you can optimize all paint functions by adding write directly to internal ram function.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ChuckMcM
    0 ChuckMcM over 13 years ago in reply to Kilohercas

    Sorry about being late to reply, in this particular case the Embest board uses the SSD2119 (not the 1963) however there is a similar sort of mode where you can set up the address counter internally and then repeatedly write to the 'Data' address and have it autoincrement. However, in this particular case the board is implemented poorly, it does not take full advantage of the STM32F4 FSMC controller, and doesn't wire up either the WAIT line or explicit RD/WR lines, (in part because the chip used doesn't have all FSMC pins due to the low pin count). Bottom line is that writing the frame cannot recognize a 'slow' write (as you get durring a DRAM refresh in the controller chip) so the software sets up delays in the DATA hold to insure that all the writes "work" (but even then you can over run the chip if you aren't careful.) The display works more reliably if you wire it up to the SPI port. That has its own limitations of course but at least you can then wire up the 'sync' pin to know when it is displaying and trying to do beam following (well display following as there is no "beam" :-).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I would like to try the examples but do not have the usual IDE's.  I'm currently downloading one now, a massive, 274MB that is going to take ~ 4 hours!  Could some kind soul post a working hex file to test the display so I know it is working before returning it to Farnell when really it is my software at fault. image

     

    Thanks Chuck for your link, I git cloned your repro ... but it is incomplete, Where is make.include, the readme mentions uart.c etc.

     

    A hex file would be great.  Farnell your people must have tested this stuff for suitability before selling it, surely you have some test files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>