STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Using a different LCD screen
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 6 subscribers
  • Views 942 views
  • Users 0 members are here
Related

Using a different LCD screen

philip-1992
philip-1992 over 13 years ago

Hi all,

 

I am in a phase of my project where I need to use a different LCD. I am currently using SSD2119 and I am considering in buying the ILI9325. Has anyone worked with these 2 screens? If I have started a project on SSD2119 is it possible to use the same project for the ILI9325? Or I need to change the FSMC timings?

 

Thankyou all.

  • Sign in to reply
  • Cancel
Parents
  • philip-1992
    0 philip-1992 over 13 years ago

    I have found this type of LCD: http://www.ebay.com/itm/3-2-QVGA-240x320-262k-TFT-LCD-module-with-touch-panel-/170874318466 it says that the LCD driver is SSD1289 (point 3 in the description part of the item) whilst my current LCD uses the SSD2119. Will the code be compatible? Or I need different libraries for the two screens?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • philip-1992
    0 philip-1992 over 13 years ago

    I have found this type of LCD: http://www.ebay.com/itm/3-2-QVGA-240x320-262k-TFT-LCD-module-with-touch-panel-/170874318466 it says that the LCD driver is SSD1289 (point 3 in the description part of the item) whilst my current LCD uses the SSD2119. Will the code be compatible? Or I need different libraries for the two screens?