STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Using a different LCD screen
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 6 subscribers
  • Views 943 views
  • Users 0 members are here
Related

Using a different LCD screen

philip-1992
philip-1992 over 13 years ago

Hi all,

 

I am in a phase of my project where I need to use a different LCD. I am currently using SSD2119 and I am considering in buying the ILI9325. Has anyone worked with these 2 screens? If I have started a project on SSD2119 is it possible to use the same project for the ILI9325? Or I need to change the FSMC timings?

 

Thankyou all.

  • Sign in to reply
  • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago

    you need to change init function, and all other functions (maybe some functions use same commands, like LCD_Clear is same, i mean use same registers )

     

    What i do, is i use same names and same prototypes for same functions, so same code will run on different lcd, but i must change lcd.c and lcd.h files. I believe if you find library from ST that works with you new lcd, code in main will work the same (if resolution is the same)

     

    Go to stm32f4 examples, open adc sample project, \IAR Embedded Workbench\arm\examples\ST\STM32F4xx\STM32F4xx_DSP_StdPeriph_Lib\Utilities\STM32_EVAL\STM324x7I_EVAL (open iar arm, go for example projects, and find this one)
    inside files will be for your controller, and functions should have same name.
    Good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago in reply to Kilohercas

    Hmm, Ok will try what you have told me once the new LCD is bought. Thanks again Linas image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • philip-1992
    0 philip-1992 over 13 years ago

    I have found this type of LCD: http://www.ebay.com/itm/3-2-QVGA-240x320-262k-TFT-LCD-module-with-touch-panel-/170874318466 it says that the LCD driver is SSD1289 (point 3 in the description part of the item) whilst my current LCD uses the SSD2119. Will the code be compatible? Or I need different libraries for the two screens?