STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum Discover Wi-Fi Download Package
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 7 subscribers
  • Views 2711 views
  • Users 0 members are here
Related

Discover Wi-Fi Download Package

e14 Contributor
e14 Contributor over 12 years ago

Buongiorno,

ho recentemente acquistato il Kit Discover Wi-Fi, ma sembra che manchi un pacchetto di installazione tra i SW messi a disposizione secondo quando comunicatomi da Murata.

Il file in questione è " SNIC-8200-03-37191.exe" (o simile), che secondo Murata deve essere incluso nei file messi a disposizione all'atto del download.

E' possibile avere il suddetto eseguibile al fine di poter utilizzare sia la modalità SPI e soprattutto l'EZ Web Wizzard, contenuto nel pacchetto di installazione?


<<

Hi,

I recently bought the kit Discover Wi-Fi, but it's lacking an installation package from the SW made available when the second reported by Murata.

The file in question is "SNIC-8200-03-37191.exe" (or similar), which according to Murata must be included in the files made available at time of download.

it' possible to have the above-mentioned executable to be able to use both SPI and modality especially the "EZ Web Wizzard software", contained in the installation package?

>>

 

Grazie

Cordiali saluti.

 

Giuseppe.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

     

    I just downloaded the software pack again here from Element14 and both the Web Wizard parts seems to be included now and also the patches for the WICED SDK which is really great. Now I'm just awaiting the WICED 3.0 SDK and I hope that Murata and Element14 will supply patches for that one as well later one.

     

    Thanks Element14 for updating the package.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

     

    I just downloaded the software pack again here from Element14 and both the Web Wizard parts seems to be included now and also the patches for the WICED SDK which is really great. Now I'm just awaiting the WICED 3.0 SDK and I hope that Murata and Element14 will supply patches for that one as well later one.

     

    Thanks Element14 for updating the package.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Andreas,

    How are you getting the WICED 3.0 SDK package?

     

    Dave.