STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum 32F429IDISCOVERY atop of STM32F4DISCOVERY Base Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 5 subscribers
  • Views 945 views
  • Users 0 members are here
  • stm32f4
  • 32f429idiscovery
Related

32F429IDISCOVERY atop of STM32F4DISCOVERY Base Board

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

Is it possible to attach 32F429IDISCOVERY atop of STM32F4DISCOVERY Base Board?

 

Thanks.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello,

    that is a really interesting question ... I also have two such boards here arround.

    After a little research I found the schematics of the boards of concearn here:

     

    32F429IDISCOVERY

    http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259090

     

    STM32F4DIS-EXT (including those of the base board)

    http://www.st.com/web/catalog/tools/FM146/CL1984/SC720/SS1462/PF255417

     

    STM32F4DISCOVERY

    http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF252419

     

    The connectors P1 and P2 are of interest and comparing them of the first and last

    board, they seem not to be compatible image

     

    For example

    P1 at the 32F429I has Pin1 and Pin2 5V ... the 32F4 provides ground there

    P2 at the 32F429I has Pin1 and Pin2 3V ... the 32F4 provides ground there also

     

    even more:

    the base board at CON2 (connecting to P2 of 32F4) expects Pin3 and Pin4 to be 5V, Pin5 and Pin6 to be 3V

     

    So it seems not to match.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for detailed answer!

    So only one way remains is to wait on BB exactly for 32F429IDISCOVERY.