STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum LCD35RT Example Program with stm32f407 with base board with LCD connected
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 5 subscribers
  • Views 720 views
  • Users 0 members are here
Related

LCD35RT Example Program with stm32f407 with base board with LCD connected

e14 Contributor
e14 Contributor over 12 years ago

Hello

(I am just beginning so don't know a lot!)

I have just got into programming this chip and require some help I have tried for hours trying to get examples to work and fail.

I have downloaded the example LCD_35T which I can get working with the text and the three bars. but you cannot edit this program as it is a read only and I cant seem to change it.

I am hoping someone could send me a example of a program that would work so I can add to it. I am just doing the blinky projects turning leds on and configuring inputs and outputs and analoge inputs.

I just want to be able to printf to the LCD to help me fault find and maybe show the status of my inputs.

If anyone could help I would be grateful thanks!!

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 12 years ago

    Is there a debugging terminal built into your board (there is in many ST designs). If not then think about buying an STLLInk debugging interface.

    Arm Cortex chips have  a nice debugging interface built in and you should only consider printf debugging as an absolute last resort.

     

    I don't understand why you can't edit the LCD_35T code - it seems to be open source and readily available.

     

    Which tool chain are you using ?

     

    (I would recommend the free version of the Keil tools for beginners - it works, it properly supports debugging tools and knoes about a LOT of different chips.)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago

    Is there a debugging terminal built into your board (there is in many ST designs). If not then think about buying an STLLInk debugging interface.

    Arm Cortex chips have  a nice debugging interface built in and you should only consider printf debugging as an absolute last resort.

     

    I don't understand why you can't edit the LCD_35T code - it seems to be open source and readily available.

     

    Which tool chain are you using ?

     

    (I would recommend the free version of the Keil tools for beginners - it works, it properly supports debugging tools and knoes about a LOT of different chips.)

     

    MK