STM32F4DISCOVERY Expansion Boards
  • Products & Partners
  • Dev Tools
  • STM32F4DISCOVERY Expansion Boards
  • More
  • Cancel
STM32F4DISCOVERY Expansion Boards
Forum STM32F4DIS-BB Stm32CubeMX project template
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STM32F4DISCOVERY Expansion Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 8 subscribers
  • Views 3102 views
  • Users 0 members are here
  • expansion
  • ethernet
  • stm32f4discovery
Related

STM32F4DIS-BB Stm32CubeMX project template

nikola1010
nikola1010 over 10 years ago

Hi all,

 

I got  STM32F4DIS-BBSTM32F4DIS-BB but I am unable to make ethernet demo with CubeMX

Could someone please create template project with CubeMX that works.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +1
    You dont need to buy KEIL. Follow these steps to get it to work. Get Atollic TrueStudio their free version is now with no size limit. Create the template with CubeMX. CubeMX creates EVERYTHING you need…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    You dont need to buy KEIL.

    Follow these steps to get it to work.

    Get Atollic TrueStudio their free version is now with no size limit.

    Create the template with CubeMX. CubeMX creates EVERYTHING you need to run the Ethernet with LWIP, however it will create a project using the registers for a different PHY, so it wont work out of the box, you need to change two register addresses:

     

    #define PHY_READ_TO                     ((uint32_t)0x0004FFFF)

    #define PHY_WRITE_TO                    ((uint32_t)0x0004FFFF)

     

    You can do this in the config screen of CubeMX or directly in the file stm32f4xx_hal_conf.h once you have created the code.

    Once the code is ready, import it to True studio, compile and run.

     

    CubeMX is a pretty neat tool, but you can't expect to do everything for you image, that should get you started

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    You dont need to buy KEIL.

    Follow these steps to get it to work.

    Get Atollic TrueStudio their free version is now with no size limit.

    Create the template with CubeMX. CubeMX creates EVERYTHING you need to run the Ethernet with LWIP, however it will create a project using the registers for a different PHY, so it wont work out of the box, you need to change two register addresses:

     

    #define PHY_READ_TO                     ((uint32_t)0x0004FFFF)

    #define PHY_WRITE_TO                    ((uint32_t)0x0004FFFF)

     

    You can do this in the config screen of CubeMX or directly in the file stm32f4xx_hal_conf.h once you have created the code.

    Once the code is ready, import it to True studio, compile and run.

     

    CubeMX is a pretty neat tool, but you can't expect to do everything for you image, that should get you started