Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Blog EAGLE ULPs Every User Should Know
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: DaveYoung
  • Date Created: 19 Jan 2015 5:39 PM Date Created
  • Views 33660 views
  • Likes 5 likes
  • Comments 10 comments
  • eagle
  • autodesk eagle
  • ulp
  • pcb
  • cad
  • eagle ulp
  • dyoung
Related
Recommended

EAGLE ULPs Every User Should Know

DaveYoung
DaveYoung
19 Jan 2015

A ULP (User Language Program) is a feature designed into EAGLE to allow users to generate their own processes to automate tasks that would otherwise be tedious and time consuming. While most users know that this functionality exists, very few want to write their own script. A casual user would have to dump far more time learning the system and designing/testing their code than just completing the task at hand.image

 

Many EAGLE users don't know that there are many ULPs that have been written by the pros at CadSoft waiting to be discovered.  These are tried and true ways to get things done quickly without having to bother writing the ULP from scratch. So give the intern an interesting project to take on and start using tools! Note that this article is written based on EAGLE v7.1.


Mountsmd.ulp: Create a Component Placement List (CPL) for pick-and-place programming.

A heavily-used ULP, this takes what would be a very tedious task and automates it reliably. Any contract manufacturer will need to know where each component needs to be mounted and its rotation so they can program their pick-and-place machine. This ULP outputs 2 files: one describing top side SMD parts, and the other describing bottom side SMD parts. Note it doesn’t call out through-hole parts (but Mount.ulp does). You will also want to import the data into a spreadsheet and label each column. It is best to generate this anytime gerbers are generated to be sure it is accurate.

How to Use:

In the layout editor, click the ‘ULP’ button and select Mountsmd.ulp. Enter a path and filename, and a semicolon-separated-values document is created.

 

Ref Desx (mm)y (mm)RotationValuePackage
C512.2314.56010uC0805
D116.0114.54180LED0603DIODE0603
Q15.3220.95180AO6604TSOP-6
Q25.3215.87180AO6604TSOP-6
Q35.3210.79180AO6604TSOP-6
Q624.259.3990AO6604TSOP-6
Q724.2514.4790AO6604TSOP-6
Q824.2519.5590AO6604TSOP-6
Q911.724.70NTGS3443TSOP-6
R47.96.91010kR0603
R11110.221.7600R0603
R11318.7514.0790330R0603
U117.9618.97180MCP1702SOT23
U213.910.5270G2X[0/1]1---PW14PW14


BOM.ULP: Generate a BOM based on component data

EAGLE is capable of maintaining manufacturer and part number for each part so the schematic can be the controlled document for manufacturing information. The BOM.ulp is there to output this data in a format that manufacturing can easily read.

How to Use:

In the schematic editor, click the ‘ULP’ button and select ‘bom.ulp’. Review for accuracy, and then save it in the desired format.

image

 

billy-eicher-parks-and-rec-w724.jpgNormalize-text.ulp: Force all of the text on silkscreen layers to be of unified size and thickness.

Even among my component library there is wide variation on silkscreen text size. Reading the text reminds me of Craig Middlebrooks on the TV show ‘Parks and Recreation.’ It takes a lot of clicking to manually change the size, and I always miss one. Instead, this ULP takes care of it in one click. Although make sure you do this before placing the silkscreen text as they will need to be repositioned!

How to Use:

Determine the desired silkscreen text size and thickness. In the layout editor, click the ‘ULP’ button and select ‘normalize-text.ulp’. Enter your desired text size and thickness, and hit OK.

image

 

Exp-Lbr.ulp: Build a component library from a design.

As a consultant, I am always careful to keep each client’s design files separate. When a client wants the EAGLE library to be included when I send them documentation it would be inappropriate an unwieldy to give them libraries that may include components designed for other clients. This ULP is great for saving a library to accompany design documentation so another engineer can easily modify a component’s details without having to create it from scratch. I’ve used it before with great success!

How to Use:

This ULP has a nice shortcut found in File>Export>libraries

image

 

Statistic-brd.ulp:  Details some standard stats about the board.

I’ve added this to my standard PCB review process. It takes about 30 seconds, but going through all of the board stats can have something stick out like a sore thumb. I’ve found myself saying, ‘I don’t remember creating a hole of that size’ or ‘There shouldn’t be a trace that fat in there’ which uncovered an error.

How to Use:

In the layout editor, click the ‘ULP’ button and select Statistic-brd.ulp. Click through the resulting data.

image

 

This short list of ULPs has saved me hours of work, but I still don’t trust them any more than I would a downloaded component library. Always be sure to double check anything they do, and never run a ULP after your review process has started. It’s never fun when an automated feature causes more errors than it saves!

  • Sign in to reply

Top Comments

  • Joop14
    Joop14 over 11 years ago +1
    diff-sch-lbr.ulp: look for differences between schematic and the libraries. Checks also for missing libraries. Something that Cadsoft should have implemented many years ago. It's crazy that Eagle only…
  • AnnaDennym
    AnnaDennym over 4 years ago

    Hello! A personal application is a necessary step that is required when entering a university. You need to do your best to make your personal statement unique and error-free. Our ucas personal statement checker will help you with this, which will analyze your personal statement, identify plagiarism, help you paraphrase it and eliminate all grammatical, spelling and punctuation errors!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • paul_walker
    paul_walker over 4 years ago

    Sometimes even experienced copywriters can use the handy revise paragraph online free, which will help you check the text of any size and complexity, as well as allow you to use a wide range of tools to improve the text. Try it and you will be satisfied with the result today without paying even a cent for the services of the service.

    Link: https://www.completesentencechecker.com/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DiLin
    DiLin over 4 years ago

    Catch a tool that will help you correct dialogue punctuations free! I use it both for checking complex textual and literary works, and for checking simple abstracts and amateur articles. The tool works on the basis of algorithms that find errors and identify them. I'm happy with it, as it helped me not only improve the quality of the text, but also saved me a lot of time!

    https://www.dialoguepunctuation.com/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • EmilyForb
    EmilyForb over 4 years ago

    Hi all! If you are having problems with writing and checking texts for errors, then use this tool. Fix my essay generators free on this site and am very happy with the result. Very high quality, fast and most importantly free this site will facilitate your writing and check your text for errors. The site is very easy and easy to use. Use and enjoy!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Nickmark42
    Nickmark42 over 4 years ago

    is there any ULP, which can remove very small gaps between two lines. I am facing this issue, when i am trying to import DXF file. There are lots of lines, where this small gaps(0.0001% of gaps) occurs automatically. Due, to this problem, I am unable to close the contour. I am able to to remove gaps by manual method.But, I want to do it using ULPs automatically.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>