Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) device with same signal legs, how?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 755 views
  • Users 0 members are here
Related

device with same signal legs, how?

e14 Contributor
e14 Contributor over 16 years ago

Hi,

 

I have a part, a FET in a SOT223-5EV-VREGSOT223-5EV-VREG package, it has the three regular DSG

legs + a large drain for cooling. The drain therefor has two pads, how

can I connect them so they carry the same signal?

 

Tried the connection function in the device editor, but it won't allow

me to connect to two pins to the same signal.

 

Any ideas?

 

Thanks,

 

Arthur

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    artelse wrote on Wed, 07 July 2010 07:50

    I have a part, a FET in a SOT223-5EV-VREGSOT223-5EV-VREG package, it has the three regular DSG

     

    legs + a large drain for cooling. The drain therefor has two pads, how

     

    can I connect them so they carry the same signal?

     

    You can short the two pads together with a polygon, or make only one pad

    and simulate the other yourself and connect them, but either way you will

    get massive DRC errors.  There is no good answer for this in Eagle

    unfortunately.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    artelse wrote

    I have a part, a FET in a SOT223-5EV-VREGSOT223-5EV-VREG package, it has the three regular DSG

    legs + a large drain for cooling. The drain therefor has two pads, how

    can I connect them so they carry the same signal?

    >

    "Olin Lathrop"  replied

    You can short the two pads together with a polygon, or make only one pad

    and simulate the other yourself and connect them, but either way you will

    get massive DRC errors.  There is no good answer for this in Eagle

    unfortunately.

     

    Not quite true

    You can add a connected polygon copper pad for the tab without DRC errors.

    For a SOT-223 package with only 3 pads.

    Add the Tab pad in the board editor using the polygon tool.

    Determine the name of the drain net and name the polygon the same.

    Route from the drain pad to the polygon outline  .

    Ratsnest to fill polygon and recalculate airwires

     

    Warren

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    On 2010-07-09 08:49:28 +0200, Warren Brayshaw said:

     

    artelse wrote

    >>> I have a part, a FET in a SOT223-5EV-VREGSOT223-5EV-VREG package, it has the three regular DSG

    >>> legs + a large drain for cooling. The drain therefor has two pads, how

    >>> can I connect them so they carry the same signal?

    >>

    "Olin Lathrop"  replied

    >> You can short the two pads together with a polygon, or make only one pad

    >> and simulate the other yourself and connect them, but either way you will

    >> get massive DRC errors.  There is no good answer for this in Eagle

    >> unfortunately.

     

    Not quite true

    You can add a connected polygon copper pad for the tab without DRC errors.

    For a SOT-223 package with only 3 pads.

    Add the Tab pad in the board editor using the polygon tool.

    Determine the name of the drain net and name the polygon the same.

    Route from the drain pad to the polygon outline  .

    Ratsnest to fill polygon and recalculate airwires

     

    Warren

     

    Thanks for the response, I thought I missed something, but it's just

    not as easy as one might expect. The @ rule and the polygon trick of

    Warren will solve my problem, although not in the most elegant way.

     

    Arthur

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Gary Gofstein schrieb:

     

    yup. it's a big problem with EAGLE. I often do the same as Warren

    suggests, and just leave that Heatsink out of the part's footprint.

    lately, I've been adding a Heatsink pin to the part and just connecting

    it up. It looked ugly in the schem at first, but I got used to it.

     

    JFYI: For devices with multipe pads per node, I always use (ugly)

    symbols that represent the pad count 1:1. It's better to have an

    explicitly correct schematic and board than to have a nice looking

    schematic only, IMHO.

     

    The downside of this method is that you need multiple devices for

    different packages of basically the same part (if they differ in pad

    count). So far, we'll have to live with that. Many suggestions have been

    made about how to eventually solve this, but we are still hoping for

    something to get real...

     

    For thermal pads, I simply put the stop and cream masks in the package

    definition, and use a polygon in the board - which is there for heat

    spreading, anyway. So in this case, the connection at the thermal pad

    doesn't show up in the schematic - this doesn't matter to me since it

    normally is also connected elsewhere to the device, or obvious...

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Gary Gofstein schrieb:

     

    yup. it's a big problem with EAGLE. I often do the same as Warren

    suggests, and just leave that Heatsink out of the part's footprint.

    lately, I've been adding a Heatsink pin to the part and just connecting

    it up. It looked ugly in the schem at first, but I got used to it.

     

    JFYI: For devices with multipe pads per node, I always use (ugly)

    symbols that represent the pad count 1:1. It's better to have an

    explicitly correct schematic and board than to have a nice looking

    schematic only, IMHO.

     

    The downside of this method is that you need multiple devices for

    different packages of basically the same part (if they differ in pad

    count). So far, we'll have to live with that. Many suggestions have been

    made about how to eventually solve this, but we are still hoping for

    something to get real...

     

    For thermal pads, I simply put the stop and cream masks in the package

    definition, and use a polygon in the board - which is there for heat

    spreading, anyway. So in this case, the connection at the thermal pad

    doesn't show up in the schematic - this doesn't matter to me since it

    normally is also connected elsewhere to the device, or obvious...

     

    Tilmann