Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) device with same signal legs, how?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 751 views
  • Users 0 members are here
Related

device with same signal legs, how?

e14 Contributor
e14 Contributor over 16 years ago

Hi,

 

I have a part, a FET in a SOT223-5EV-VREGSOT223-5EV-VREG package, it has the three regular DSG

legs + a large drain for cooling. The drain therefor has two pads, how

can I connect them so they carry the same signal?

 

Tried the connection function in the device editor, but it won't allow

me to connect to two pins to the same signal.

 

Any ideas?

 

Thanks,

 

Arthur

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    artelse wrote on Wed, 07 July 2010 07:50

    I have a part, a FET in a SOT223-5EV-VREGSOT223-5EV-VREG package, it has the three regular DSG

     

    legs + a large drain for cooling. The drain therefor has two pads, how

     

    can I connect them so they carry the same signal?

     

    You can short the two pads together with a polygon, or make only one pad

    and simulate the other yourself and connect them, but either way you will

    get massive DRC errors.  There is no good answer for this in Eagle

    unfortunately.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    artelse wrote

    I have a part, a FET in a SOT223-5EV-VREGSOT223-5EV-VREG package, it has the three regular DSG

    legs + a large drain for cooling. The drain therefor has two pads, how

    can I connect them so they carry the same signal?

    >

    "Olin Lathrop"  replied

    You can short the two pads together with a polygon, or make only one pad

    and simulate the other yourself and connect them, but either way you will

    get massive DRC errors.  There is no good answer for this in Eagle

    unfortunately.

     

    Not quite true

    You can add a connected polygon copper pad for the tab without DRC errors.

    For a SOT-223 package with only 3 pads.

    Add the Tab pad in the board editor using the polygon tool.

    Determine the name of the drain net and name the polygon the same.

    Route from the drain pad to the polygon outline  .

    Ratsnest to fill polygon and recalculate airwires

     

    Warren

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    warrenbrayshaw wrote on Fri, 09 July 2010 02:49

    Quote:

    You can short the two pads together with a polygon, or make only

    one pad and simulate the other yourself and connect them, but either

    way you will get massive DRC errors.  There is no good answer for this

    in Eagle unfortunately.

     

    Not quite true You can add a connected polygon copper pad for the tab

    without DRC errors.  For a SOT-223 package with only 3 pads.  Add the Tab

    pad in the board editor using the polygon tool.

     

    But now you're manually messing with it in the board editor, which you'd

    have to do seperately each time you use the device.  I guess there is still

    no good answer in Eagle.

     

    If you know of a way to pre-define devices like this that then don't cause

    DRC errors, I'd really like to know about it.  Right now I live with the

    DRC errors, which makes DRC rather less useful than it could be.  Not a

    good answer either.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    warrenbrayshaw wrote on Fri, 09 July 2010 02:49

    Quote:

    You can short the two pads together with a polygon, or make only

    one pad and simulate the other yourself and connect them, but either

    way you will get massive DRC errors.  There is no good answer for this

    in Eagle unfortunately.

     

    Not quite true You can add a connected polygon copper pad for the tab

    without DRC errors.  For a SOT-223 package with only 3 pads.  Add the Tab

    pad in the board editor using the polygon tool.

     

    But now you're manually messing with it in the board editor, which you'd

    have to do seperately each time you use the device.  I guess there is still

    no good answer in Eagle.

     

    If you know of a way to pre-define devices like this that then don't cause

    DRC errors, I'd really like to know about it.  Right now I live with the

    DRC errors, which makes DRC rather less useful than it could be.  Not a

    good answer either.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.