Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Circular PCB with circular notches
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 1399 views
  • Users 0 members are here
Related

Circular PCB with circular notches

e14 Contributor
e14 Contributor over 15 years ago

what is the best way to micro-rotate the circular notches around the

circumference of the pcb?

 

Thanks,

Don

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    The idea would be to group an arc plus two short straight segments together

    and rotate the entire object by maybe a degree or so.  I then want to copy

    and paste five of these objects around the circumference.

     

    Thanks,

    Don

     

     

    "Don Golding" <dgolding@sbcglobal.net> wrote in message

    news:i5bot3$4m1$1@cheetah.cadsoft.de...

    what is the best way to micro-rotate the circular notches around the

    circumference of the pcb?

    >

    Thanks,

    Don

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    The idea would be to group an arc plus two short straight segments together

    and rotate the entire object by maybe a degree or so.  I then want to copy

    and paste five of these objects around the circumference.

     

    Thanks,

    Don

     

     

    "Don Golding" <dgolding@sbcglobal.net> wrote in message

    news:i5bot3$4m1$1@cheetah.cadsoft.de...

    what is the best way to micro-rotate the circular notches around the

    circumference of the pcb?

    >

    Thanks,

    Don

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Don Golding wrote:

    >The idea would be to group an arc plus two short straight segments together

    >and rotate the entire object by maybe a degree or so.  I then want to copy

    >and paste five of these objects around the circumference.

     

    That's the easy part 8-)

     

    just draw your arc + attached segments and group them.

    Then enter  'rot r72' on the command line, press

     

    assuming that the center of rotation (center of board) is the point of

    origin.

     

    repeat 4 times, done

     

     

    but as said before, that is the easy part. As eagle will not calculate

    line intersections, or does no snap-to-end-off-line when drawing,

    there is no easy way to get a closed outline when adding the arcs for

    the board outline.

     

    So either construct the board outline in a CAD program and import them

    via dfx (see appropriate ULP), or draw one notch and one attached

    outline arc using precalculated coordinates, then complete the outline

    per copying as described above.

     

    And see the help text for the wire command (especially the radius and

    curve options) and the chapter 'command syntax' (about coordinate

    modifiers).

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

     

    "Don Golding" wrote >

    what is the best way to micro-rotate the circular notches around the

    circumference of the pcb?

     

    >The idea would be to group an arc plus two short straight segments together

    and rotate the entire object by maybe a degree or so.  I then want to copy

    and paste five of these objects around the circumference.

     

    Don

    Although not what you have said, are notches 2 and 3 in the attached image

    what you wish to achieve?

     

    Warren

     

     

    begin 666 notched_circle.jpg

    M_]C_X `02D9)1@`!`0$!+ $L``#_VP!#``@&!@<&!0@'!P<)"0@*#!0-# L+

    M#!D2$P\4'1H?'AT:'!P@)"XG("(L(QP<*#<I# Q-#0T'R<Y/3@R/"XS-#_

    MVP!#`0D)"0P+#!@-#1@R(1PA,C(R,C(R,C(R,C(R,C(R,C(R,C(R,C(R,C(R

    M,C(R,C(R,C(R,C(R,C(R,C(R,C(R,C+_P `1" #[`0`#`2(``A$!`Q$!_\0`

    M'P```04!`0$!`0$```````````$"`P0%!@<("0H+_\0`M1 ``@$#`P($`P4%

    M! 0```%]`0(#``01!1(A,4$&$U%A!R)Q%#!D:$((TQP152T? D,V)R@@D*

    M%A7J#A(6&AXB)BI3E)66EYB9FJCI6FIZBIJKSM6VM[BYNL#Q,7&

    MQ\C)RM+3U-76U]C9VN'BX3EYN?HZ>KQ\O/T]?;W/GZ_\0`'P$``P$!`0$!

    M`0$!`0````````$"`P0%!@<("0H+_\0`M1$``@$"! 0#! <%! 0``0)W``$"

    M`Q$$!2$Q!A)!40=A<1,B,H$(%$*1H;'!"2,S4O 58G+1"A8D-.$E\1<8&1HF

    M)R@IC4V-S@Y.D-$149'2$E4U155E=865IC9&5F9VAI:G-T=79W>'EZ@H.$

    MA8:'B(FDI.4E9:7F)F:HJ.DI::GJFJLK.TM;:WN+FZPL/$Q<;'R,G*TM/4

    MU=;7V-G:XN/DY>;GZ.GJ\O/T]?;W/GZ_]H`# ,!``(1`Q$`/P#WBBB@ HH

    MHH **** "BBB@ HHHH **R]2\0Z9I5PMK<3R/=L@D%K:P27$^S)&\QQJSA,C

    M&[&,X&<D53_M'Q+>_P#'GH,%A&?D,FIWB^8A_OB*$.KJ,C@RH201\HPQ`.@H

    MKG_[!U:Z^;4/%%]\_$L%A#%;PLO3"DJ\R9'4B7=DDJ5X`/\`A"?#LG_'[I_]

    MIXY_:LTE]Y?KL\]GV9XSMQG`SG H T-3UW1]$\KUM5L;#SL^7]KN$BWXQG

    M&XC.,CIZBC3-=T?6_-_LG5;&_P#)QYGV2X279G.,[2<9P>OH:SY;71_"%FSZ
    M-HEC;W5Y+';QP6D*0&XD)(7<57.U06=B`Q5%=L'!%:&F:9]A\VXN)OM.H7&#
    M<7)7;NQG:BKD[(UR=JY.,DDLS,S $FI:MINC6ZW&J:A:6,#.$62ZF6)2V"<`
    ML0,X!./8U8@GANK>XMY8YH)4#QR1L&5U(R""."".<U7U+38=3MUCD:22-Q

    M)!<1$"2"0 @.A((S@D$$$$$JP*D@\WI_AWPWJEY?PZMX7T-]7MY0;J3[!'BX

    MWC<)UW MM?+#DG#K(NYMNX@'845S_P#PB%E!\VG7VJZ=(O$7V>_D:.$?W4@D

    M0A<<!=F%'W0" 0?8?$NG?-9ZO!JL8Y,.IQ%(Q/&!-"H5%'!P86).1D`C:

    M=!17/_\`"17EC\NLZ#?6^.//L$-]"S=0%$8\[IU1*H((R?E;%C?V>IV<=Y

    M87<%W:R9V302"1&P2#AAP<$$?A0!8HHHH **** "BBB@`HHHH **** "BBB@

    M`HHHH **** "BHYYX;6WEN+B6.&")"\DDC!510,DDG@`#G-8?VO4?$/_`""Y

    M_L.DMRNI(5::?'>%'1D\LG&)&SN .U<,DE %S4M=MM/N%LHTDO=3=!(FGVK(

    M9V3)!<AF4*@P?F8@9PH)8@&G_96L:OSK-_\`8[<_\N.E3.F?]^XPLC<@,-@B

    MQDJV\5J:;I5CI%NT%A;1P([F20KRTKD`%W8\NYP,LQ)/<FKE`%/3=*L=(MV@

    ML+:.!'<R2%>6E<@`N['EW.!EF))[DU<HHH **** .?\`$W[J\.7K\6]MJJ

    M:_\`=\V&:!..IS)-&O'3=DX`)'05'/!#=6\MO<11S02H4DCD4,KJ1@@@\$$<

    M8K#\S6="_<1V$^M6`XA>X3[7&.R/YKKJ,']YOWG*@JQ#2$`Z"N?T[]_P".

    M=>N8_FABM.R=NF)D,TKCV2>(YZ?-C.00#[=KVJ_P"CV^D3Z-&>);N]EA>1

    M`>\,<;2S<$9<J%)4XD`UL6-C;Z=9QVMK'Y<*9(!8L22269F.2S$DDL2222

    M2230!8HKC_"OB?6-7\7*-%U:SL;;R?LGEK:2OGS8V<Y=@N[H.BC)'/6N

    MPH *Q[[PSIUY>27T8GLK]\%KNQF:%W8`!#(%.V7;C@2!U'(Q@D'8HH Y_P"U

    M:[HO%];_`-KV*_\`+U:(%N8U]9(>DF "2T9#,2 L-;%C?V>IV<=Y87<%W:R9

    MV302"1&P2#AAP<$$?A5BL>T!)+R34=,G_LW4Y,>;<0Q*PN0``JSJ1\48'.

    M5<#(5UW'(!L45CV.N9O(]-U>.#3]5DR8H!/YB7"@$DPN54O@`[AM#+CD;2K-

    ML4 %%%% !1110 4444 %%%% !1110 57OKZWTZSDNKJ3RX4P"0I8DD@*JJ,E

    MF)(`4 DD@ $FB^OK?3K.2ZNI/A3`)"EB22 JJHR68D@!0"22 `2:S[&QNV

    M\CU758_F3)M,L&%H"""S$9#3$$@L,A02BD@N\@!'!87VJW$5YK(CCMXW$U

    MMIJKGRW!RK3.&(D=<!@%`5&)YDHXW** "BBB@`HHHH`**** "BBB@`HHHH

    M`Y?0_#=YIGCOQ7KDTD#6NK_8_LZ(Q+KY411MP(P,D\8)_"NHHHH`****`"BB

    MB@"O?6-OJ-G):W4?F0O@D!BI!!!5E88*L" 0P(((!!!%9<%Y?:1<16NLW$=S

    M;S.([;4%B\OYR<+', <!VXPZ[59B5VH=@?<J.>"&ZMY;>XBCF@E0I)'(H974

    MC!!!X((XQ0!)16'!/-H5Q%8WTLDVGRN([2\E8LT;$X6&9CR23@)(?O<*WS[6

    MEW* "BBB@ HHHH **** "BBN?US_`(G5Y_PC4?,$D0DU4]"+5Q(H13_>D9"O

    M`X19.48H2 %G_P`5)>&E;2>56L$'WM@`PN#_`'E#9$8QM^7S`6S&4Z"B

    MB@`HHHH`***`"BBB@`HHHH`**`"BBB@`HHHH`***`"BBB@`HHHH`KWUC

    M;ZC9R6MU'YD+X) 8J000596&"K @$,""" 0016?I-]<)>3Z1J4F[@:WF90

    MIO(,^]P/EW*S;'"]P&VHLB6Q67KNFS:A9))9-&FIV;FXL))2=BS;&4!P`<

    MHRNRMQG#$KA@" #4HJGI>I0ZM8=PK(@O&\<@`:.1'*.AP2,JRLN02#C()&

    M#5R@`HHHH **** *>JZE#I&EW%_.LCI"F1'$`7E;HJ("1N=F(51W) [U7T+3

    M9M/LGDO6C?4[QQ<7\D1.QIMBJ0@(&$5455XSA06RQ)-/4/\`B9^+;#3#\]K8

    MQ'4+E.WF%MEN&!X9<B=\`9#PQG(XW=!0`4444 %%%% !1110`4444 %%%% !

    M1110`4444 %%%% !1110`4444 %%%% !1110!S]Q_P`2Q''=Q8:O+Y=T3R

    M(5TV'5]N"=I$29,"2(@/$W570D':ZL

    M`RGL0#VJOX<U*;5O#]G=W2QI>%#'=QQ@A8[A"4F09)X6177.2#C()'- &I11

    M10`445S_`(T_?^%[K3%YFU;&FQ@<L/..QG"_Q;$+R$?W8VY R0`'@[_2=#_M

    MAN9-9E;4-QX)C? @##H&6!84('&5)R22QZ"BB@`HHHH`****`"BBB@`HHHH`

    M***`"BBB@`HHHH`**`"BBB@`HHHH`***`"BBB@`KG[?_`(EWCF[MAQ#J

    MUH+U%7G]]"5BE9B>F4>U``X_=L<`\MT%<_XK_P!&BTK5SS'IFH1SR@\`1NKP

    M.[-_"J,TA)XQ&<X!R #H**** "N?U?_`$KQ?X<LON^1]IU?UW>7&(-F.V?

    MM>[/QC'S9'05S]M\^(>I[_`)O(TJT\K=SY?F2W._;Z;O+CSCKL7/W10!T%

    M%%% !1110 4444 %%%% !1110 4444 %%%% !1110 4444 %%%% !1110 44

    M44 %%%% !6?KNF?VWX>U/2?.\G[=:2VWF[=VS>A7=C(SC.<9%:%%`&?H6I_V

    MWX>TS5O)\G[=:17/E;MVS>@;;G SC.,X%:%<_P"#/E\/O$.(X=0OH(D'2.-+

    MN5$11V5555 '```'`KH`"N?T#]YX@\52O\`-(FH10YY*QBT@<(#_=#22,!

    MTR['J36K?1ZC)Y?V"ZM8,9W^?;-+GIC&'7'?U_"N8T*#6SK'B<1:CIZN-302

    MEK%V#-]DM^5'G#:-NT8.>03GG EM]C6-.5W-G\0_P#04TO_

    M`,%LG_QC[/XA_Z"FE_"V3_`./T<S[?E_F5[&'_`#\7_DW^1K45D_9_$/\`

    MT%-+_P#!;)_\?HS(?@II?_@MD_P#C]',WY?YA[&'_/Q?^3?Y&M163]G\

    M0_\`04TO_P`%LG_QC[/XA_Z"FE_"V3_P"/T<S[?E_F'L8?\_%_Y-_D:U%9

    M/V?Q#_T%-\%LG`,?HS(?^@II?\`X9/_C]',WY?YA[&'_/Q?\`DW1

    MK45D_9_$/_04TO\`\%LG_P`?HS(?\`H*:7_P""V3_X_1S/M78>QA_P`_

    M%_Y-_D:U%9/V?Q#_`-!32_\`P6R?_'Z/L_B'_H*:7_X+9/\`X_1S/M78>Q

    MA_S\7_DW1K57O;R.P@6:56*M-%"`HYS(ZH/PRPS[51S(?@II?_@MD_\`

    MC]<OK6JZO=6$7V.ZM=2@%W;'SK73RL>[STV@2/<!7887.""&=1$ZGMCH

    MPV#56HESJUU??\[6]#OJYVQN]6U'S!;:UI9DCQYD3Z7DD><XW(TP9<XR,@

    M9'(XJY]G\0_]!32__!;)_P#'ZI3OJE79C#J#Y932?I_Y$UJ*R?L_B'_H

    M*:7_`."V3_X_1]G\0_\`04TO_P`%LG_QGS/M7^9/L8?\_%_P"3?Y&M163]

    MG\0_]!32_P#P6R?_`!C[/XA_P"@II?_`(+9/_C]',WY?YA[&'_`#\7_DW^

    M1K45D_9_$/\`T%-+_P#!;)_\?HS(?@II?_@MD_P#C]',WY?YA[&'_/Q?

    M3?Y&M163]G\0_\`04TO_P`%LG_QC[/XA_Z"FE_^"V3_P"/T<S[?E_F'L8?

    M\_%_Y-_D:U%9/V?Q#_T%-\%LG`,?HS(?^@II?\`X9/_C]',^WY?YA[

    M&'_/Q?\`DW1K45D_9_$/_04TO\`\%LG_P`?HS^(?\`H*:7_P""V3_X_1S/

    MM78>QA_P`_%_Y-_D5?#GR:KXH@7Y88M5'EQCA4WVMO(V!VR[NQ]69CU)KH

    MXW0H-;.L>)Q%J.GJXU-!6L78,WV2WY4><-HV[1@YY!.><#KXA((4$SJ\H4

    M;V1=JD]R`2<#VR?K33;Z$3A&.TD_2_ZI#ZY_0_W'B7Q/;2?-=PWJ+US"]O

    M'$K9]W@E&.ORYQ@@GH*Y'_1_B'>;\OVW2H/L_??Y$LWF_3;]HAZXSOXS@X

    M9F=!1110`4444 %%%% !1110`445G76J[+A[2SMI;R[7`946.(D9&0\#JI

    MC+X8$12;2WA"4W:)HUERZNTTSV^E0?31L4E?S@D,+#JKOR=W!^558CC<

    M%!!IO]E7%_\`-J]SYD9_Y<K?0@>CG[TO4@YPC#J@-:<44<$0PQK'%&H5$0

    M850.``!T%+51I:G3W]Y_A_F_P`/5F9_8GVSYM9N/M__`$[[-EL/V63NZ _

    M.7P1E=M'B/\`Y!D/_7_9_P#I3%6M63XC_P"09#_U_P!G_P"E,53**478TH59

    M3KT^9]5Z;]MBW?:99ZCY9N8<R1Y\N5&*21YQG:ZD,N<8.",C@\54\_5--XNH

    MO[0M1_RWMUVS*/5X^CX`R2G))PL=:U%4X]48QK-+EEJNS_3M_5RO9W]KJ$)E

    MM)UE56V.!]Y&[JP/L,CG!'<58JC>:7'=S"XCGGM;I5VB>W?#8]&4@JXY;&
    MY3C<2,$YJO\`VC=Z;QK"Q&#M>VR/L'<8G)B`'\19E4DE<@$YFOB*]DI_PO

    MNZ_\'\_(UJ9%+'/"DT,BR12&1T.58'D$$=13ZHP:MHPHHHH **** "BBB@

    M`HHHH Y_PS]OO$=ZG-O<ZJWE/\`WO*AA@?CJ,20RSUVY&003T%<_X?PT

    MERO,-Y=W=[ W]&:XDEC;';*.IP>1G! .1704 %<_K/C>*O#5XG,DTMQI[

    M]!&\+3DC_:W6L8!Z8+<9((Z"L/QA!--X3OWM8I)KNU1;VVA12QDF@831I@<D

    M%XU!`Y()`(/-`&Y14<$\-U;Q7%O+'-!@>.2-@RNI&001P01SFI`"BBB@`H

    MHJC>ZM:V4PMR6FO&7<EK`N^5@> <#[JY&-[84'J12;2WA"4W:N7JSKK6;>

    M"X>T@26]O$QNMK4!F3(R-Y)"ID*B\C5-2YNI?[/M3_RPMVW3,/1

    MY.B9!P0G((RLE:%K:V]E;I;VEO%!`F=L<2!%7)R<`<=232NWL:\M.G\6K[+;

    MYOK\OO1G_8-1U#G4KO[/#_SZV$CG_>FX<\@$;0F.0=PK0M;6WLK=>TMXH(

    M$SMCB0(JY.3@#CJ2:FHH44M2)U927+LNRV_KS>OF%%%%49A63XC_`.09#_U_

    MV?\`Z4Q5K5D^(_\`D&0_]?\`9_\`I3%4S^%F^%_CP]5^9K44451@%%%%`&7+

    MHL:3/<Z=,UA<NQ=S$,Q2L>29(S\K$G&6&'(&-PIO]M_8_EUFW^P?]/&_?;'_

    M`:X&WJ!\X3).%W5K45/;8W5;FTJ*_Y_?\`YI^5@HK)_LJXL/FTBY\N,?\`

    ME<9>$CT0_>BZ #&44=$)J6UU97N$L[V[%?-G9#)(I$V!R8F'WP,'L&`P65

    M<C)S=&)T;KF@[K\?N_RNC1HHHJC$***`"LOQ+J4VC>%=7U2W6-I[RFN(UD

    M!*ED0L <$'&1ZBM2N?\`$O\`I=YH6E#E;G4$GF"??2. &<./1?-2!"2,?O,<

    M%E- &II.FPZ-HUCI=NTC065O';QM(06HH4$X &<#T%7** "BBB@#FO#MU;

    MZ)I=WI-]<16J:/84,SA$6U9LVQ!;!A"L6X]7B<98@DVY;G4]741Z9YFG6Y

    M/SWEU;?O'7H1%&Q!5AS\TBX!`^1P<B\=)T]M6&JM9PMJ`B6);AERZH-V`">G

    MWVZ=<\U<J=;FEZ:C9*[_`"_KO'4Y_\`L/6X/WEMXMOI9A]U+TMI(3Z[EBC

    MB<\=,.O.,Y&098?$UFFZVU#_`$35(^)!<RR-_MQ*HW2QG!(8T!W!65E7;K

    MG]<_<>)?#%S'\LTMW-9.W7,V\DKCW>"(YZ_C."06[]"8\J?O3^O4M8U3

    M4_EEC_LVS;ADW[KEQW&Y#MBZ=5D@\%&'%ZSL73X3%:0+$K-O<C[SMW9B>6

    M8X&6.2>YJQ1244M2YU927M%V7]:_,***HR"BBB@ HHHH *R?$?_(,A_P"O

    M^S_]8JUJR?$?_(,A_Z_[/\`]8JF?PLWPO\>'JOS-:BBBJ,`HHHH **** "

    MH;JUM[VW>WN[>>!\;HY4#JV#D9!XZ@&IJ!IM.Z,-=)U'3AIMU"6X@;):

    MQU"9G4DA0"DQ#.F,$X.\')X7J=KK-O/<):3I97CYVVUT K/@9.P@E7P.3L

    M8R,X/%:-<]XX19_"LUG(H,=[<6UDY(Y19IXXBZ^CJ'><,`<'&CEM\)NZ

    MRJ?Q5?S6_P`^_P`]7W)9]2U+4;B6VT%;01PN8YM0N@SQI(#RD<:D&4@@JQWH

    M%)QEF5T5BCQ79N)9IM)U2.'@@MI.0#NRLTDBLW& AV`D\NN.=N""&UMXK>

    MWBCA@B0)''&H544#```X``XQ4E6<Z*ECJ=GJ/F"VFS)'CS(G4I)'G.-R, RY

    MQD9 R.1Q7->'_/UGQSKN2_-8V>-)TT_O4X=URVUOE.90J;QU\G';)Z6^TR

    MSU'RS<PYDCSY<J,4DCSC.UU(9<XP<$9'!XJ/1='LO#^BV>DZ?$(K6UB$<:@`

    M$XZL< 98G))[DD]Z2OU-)SWA?T??7[E\R_1113,PHHHH ***R_$,^H6NBS

    MW.FJ7EA'F21I%YDKQC[XB'3S<9@@@L`",'(&.3=F[%J_U*QTNW^T:A>VUG

    M!G'F7$JQKG!.,D@=`3%9MG!-JJ0:S=1206]NCK8VTJD/\`/@&>13]QRH*J

    MN RJ[[N7)-I^DZ2YMM4B$5_<%?-AU"5A,Y#+]Y'ZI#'A,+\QP`#6M25^I4

    MU!:1U"BO-_$OAWPGHL5;_1_$CUO7[N5K6VN51[F5V4#RXY-H:*&-0#NS^[

    M'.<X![#PKIJ:5X7TZQUK4?[1U*&(+/=8^<\#)Y; PNX\MC)Y)ID&Q1110`

    M4444`%%%% !63XC_`.09#_U_V?\`Z4Q5K5D(_\`D&0_]?\`9_\`I3%4S%F

    M%_CP]59K44451@%%%%`!1110`4444`%9^MZ9_;&CSV2S>1,VV2"?;N\F9&

    M#QR;<C=M=5;:>#C!X)KB_$6GVVAV6M:EXAUSQ/=/<O<7-N^DM=QBSA5!MC"Q

    M,8EXR'D"ACDMT-=1X.GU>Z\':5<:[:3:E;J\TEHP:-
    J05^4DKM)
    _+G

    M.WC%`%S3-3^W>;;W$/V;4? N8MNVYSM=6P-\;8.UL#.""%965="L_5-#TS

    M6A#]OM%ED@8-#,"4EB.Y6^1U(9<E%S@C..:RYKZZT77=TB:6_74&DV1S(Q

    M>WBC`+R&4 @HN40!QN9I!E^N);:Z&D81DOBU\_\`/_.QTE%%%49A1110`444

    M4 %%%% '/M_Q36HR3'G2=1NTW =;6XDH,.L<CD$X&1([,=P=C'T%1SP0W5

    MO+;W$4<T$J%)(Y%#ZD8((/!!'&QX)YM"N(K&EDFT5Q':7DK%FC8G"PS,

    M>22<!)#][A6^?:TH!GMX'QXEO=?A\2:S#?W:"(L%M7$40)(BCWPL40$YP#R>

    M6R>:Z2QMY;2SC@FO9[V1<YGG"!WR2>0BJO'3@#IZ\U8HH **** "BBB@`HHH

    MH R?$?_`"#(?OS_\`2FM:LGQ'_R#(?\`K_L__2F*IG\+-\+_`!X>J_,U

    MJ**HP"BBB@`HHHH`*** .3_P"$=\36CZLNF>*XU@OKB2XB-_8M=2VA=0-L

    M;><J[%()52A S@Y[['AS0+'PMX?L]%TU9!:6J%4\QMS,22S,3ZEB3Q@<\ #B

    MM2J]]?6G6<EU=2>7"F 2%+$DD!551DLQ) "@$DD``DT`5]8UFST.S2XNW:

    M65>WA4@//,YPD:9(!8GU( Y)( )%?0=)N#[9>:C<_:=2OI?-E;@K"@^Y!&

    M=H)C0$X)`RS.V 7(HL;&XO;R/5=5C\N9,FTLRP86@((+,1D-,02"PR%!**2"

    M[R;%`!1110`4444`%%%%`!1110`5'/!#=6\MO<11S02H4DCD4,KJ1@@@\$$<

    M8J2B@#G_`#KSPWS>W/VK1%^47#@F:S7L9G)/F1]C)@,@`+[P7D7<@GANK>*X

    MMY8YH)4#QR1L&5U(R""."".<U)6'/I5]I]Q>:%&?,<O+IMR^RWD=CEI%<(

    MSQN3AC@%6.[-U^QUX:S#26VH(A>2QNE\N=5!`+!3]] QV^8A

    M9"0<,:U`"BBB@`HHHH`R?$?_(,A_Z_[/\`]*8JUJR?$?\`R#(?^O\`L_\`

    MTIBJ9_"S?"_QX>J_,UJ***HP"BBB@ HHHH ***Y__A(7UC]UX96"]7^/4)2W

    MV2,'C,!B=@<_(A ^5@SH<9 -#4]9L]\J.9_,N[C(M;.,@S7+#&0BDC.,C)

    M.%4<L54$BO8Z9>37D>HZU-!-=19-M! I$-KN!!(+',DF"5\PA?EX54W.&L:9

    MI:;YLKW,]Y>38$UW<[?,D"YVK\JJJJN3A5 &2QQN9B="@`HHHH`***`"BB

    MB@`HHHH`***`"BBB@`HHHH`IZEI=IJUNL-VDA".'C>5XI(VP1E'0AE."02

    M",AB.A(K_XJ1OH_:#_KG!>_Z##R?F6U5_C8UT%% &7INOV.I7#68:2

    MVU!$R6-TOESJH(!8*?OH&.WS$(2#AC6I5/4M)TW6;=;?5-/M+Z!7#K'=0K

    M*H;!&0&!&<$C/N:R_P#A&KBTYTKQ#JMJH^80W$HO(W?U<S!I=IX!59$X'&TD

    MM0!T%%<_]I\66GRRZ=I6HQIRTUO=/;R2CJ0D+HRANP#38)&25!X/$JS_\`

    M(2T'7+'=_J_]#U[_7_CV,NW''WMN<\9P< '05D(_\`D&0_]?\`9_\`I3%5

    M7_A-O#L?_'[J']F9^Y_:L,ECYGKL\]4WXXSMSC(SC(K-UWQIX5N=/B2#Q+HT

    MKB\M7I?Q,0JSQLQX;H%!)/8`FIG\+-\+_'AZK\SLJY_P#X3OP?_P!#7H?_

    M`(,8?_BJ/^$STAN8DU6>,\K-;Z/=RQR#LR.D15U/4,I((Y!(JC Z"BN?_M[5

    MKKY=/\+WWS\Q3W\T5O"R]<L`SS)D= 8MV2 P7D@S*=1XN;VQT>$\,E@#=3

    M<<AEEE547)X*F%N <-DC: =!7/\`_"4I?<>'[&?6%/ NH&5+12>A,S$!USD,

    M8A(5VD$9P"?\(=I=S\VL>?K<AY;^TW\V,GLP@ $,!QN5 <9R268GH .?\`

    M[!O-6?Q#>;">?[-M"8[8#^[(?OS\%E.XK&XQF(&N@HHH **** "BBB@ HH

    MHH **** "BBB@ HHHH **** "BBB@ HHHH **** "BBB@ K.UJUFN["*.!-[

    MK=VTA&0/E2='8\^BJ3^%:-%)JZL73FX34UTU"BBBF0%%%% !1110`4444 %%

    1%% !1110`4444 %%%% '_]D`

    `

    end