Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) wiring diagram
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 189 subscribers
  • Views 2199 views
  • Users 0 members are here
Related

wiring diagram

e14 Contributor
e14 Contributor over 15 years ago

Hello all,

 

Has anyone been able to get Eagle to work for wiring diagrams.  When I

try and create some schematic only components (wire housings, ferrules,

etc..) I get error messages that there is no PCB footprint.  OF COARSE,

this is for the wiring I plan to associated with the board I have created.

 

We are getting to crunch time and I need to get this moving.  Maybe I

just need to have the SolidWorks team work on this for me.

 

Thanks

Ryan

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    > I get error messages that there is no PCB footprint.  OF COARSE,

    this is for the wiring I plan to associated with the board I have created.

     

    I sometimes use SET CHECK_CONNECTS OFF; might be suitable.  From the

    menu select Options | Misc (tab) | Check Connects

     

    From the help:

    "The ADD command checks whether a pin has been connected to every pad

    (with CONNECT). This check can be switched off. Nevertheless, no board

    can be generated from a schematic if a device is found which does not

    have a package."

     

    Regards,

    Neil

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kcadsoft
    kcadsoft over 15 years ago in reply to e14 Contributor

    On 08/31/10 23:26, Neil Allison wrote:

    >> I get error messages that there is no PCB footprint.  OF COARSE,

    >> this is for the wiring I plan to associated with the board I have

    >> created.

     

    I sometimes use SET CHECK_CONNECTS OFF; might be suitable.  From the

    menu select Options | Misc (tab) | Check Connects

     

    From the help:

    "The ADD command checks whether a pin has been connected to every pad

    (with CONNECT). This check can be switched off. Nevertheless, no board

    can be generated from a schematic if a device is found which does not

    have a package."

     

    Actually this should read

     

      "The ADD command checks whether every pin has been connected to a pad..."

     

    I've changed that in the online help for the next version.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to kcadsoft

    Klaus Schmidinger wrote:

     

    >On 08/31/10 23:26, Neil Allison wrote:

    >>> I get error messages that there is no PCB footprint.  OF COARSE,

    >>> this is for the wiring I plan to associated with the board I have

    >>> created.

     

    would it be possible to add a new pin direction 'no_pad' or something

    to the effect that symbol-only devices are possible?

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 9/1/2010 10:43 PM, Lorenz wrote:

    Klaus Schmidinger wrote:

    >

    >> On 08/31/10 23:26, Neil Allison wrote:

    >>>> I get error messages that there is no PCB footprint.  OF COARSE,

    >>>> this is for the wiring I plan to associated with the board I have

    >>>> created.

    >

    would it be possible to add a new pin direction 'no_pad' or something

    to the effect that symbol-only devices are possible?

     

    just reiterating my support for symbol only devices.

     

    But I think it better to have it at the package level than at the pin

    level... there may be advantages to having it at the pin level, such as

    a pot mounted on a board, the 3 terminals are part of the package and

    the case can be shown grounded on the schematic without incurring a

    footprint pad. This could also be done in the current system with a

    special footprint, since there will need to be a ground connection

    somewhere. Maybe someone can think of a better reason to make it a pin

    direction rather than a package level option 'off_board' ??

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 9/1/2010 10:43 PM, Lorenz wrote:

    Klaus Schmidinger wrote:

    >

    >> On 08/31/10 23:26, Neil Allison wrote:

    >>>> I get error messages that there is no PCB footprint.  OF COARSE,

    >>>> this is for the wiring I plan to associated with the board I have

    >>>> created.

    >

    would it be possible to add a new pin direction 'no_pad' or something

    to the effect that symbol-only devices are possible?

     

    just reiterating my support for symbol only devices.

     

    But I think it better to have it at the package level than at the pin

    level... there may be advantages to having it at the pin level, such as

    a pot mounted on a board, the 3 terminals are part of the package and

    the case can be shown grounded on the schematic without incurring a

    footprint pad. This could also be done in the current system with a

    special footprint, since there will need to be a ground connection

    somewhere. Maybe someone can think of a better reason to make it a pin

    direction rather than a package level option 'off_board' ??